66 #ifndef ti_drivers_sd_SDSPI__include 67 #define ti_drivers_sd_SDSPI__include 70 #include <ti/drivers/dpl/SemaphoreP.h> SD_CardType cardType
Definition: SDSPI.h:119
Serial Peripheral Interface (SPI) Driver Interface.
uint16_t spiCsGpioIndex
Definition: SDSPI.h:107
uint_least8_t spiIndex
Definition: SDSPI.h:106
SPI_Handle spiHandle
Definition: SDSPI.h:118
The definition of a SD function table that contains the required set of functions to control a specif...
Definition: SD.h:284
SDSPI Hardware attributes.
Definition: SDSPI.h:104
bool isOpen
Definition: SDSPI.h:120
Secure Digital (SD) Driver.
SemaphoreP_Handle lockSem
Definition: SDSPI.h:117
SDSPI Object.
Definition: SDSPI.h:115
SPI Global configuration.
Definition: SPI.h:744
SD_CardType
SD Card type inserted.
Definition: SD.h:197
const SD_FxnTable SDSPI_fxnTable