255 #ifndef ti_drivers_lcd_LCDDogm1286__include 256 #define ti_drivers_lcd_LCDDogm1286__include 259 #include <ti/drivers/dpl/SemaphoreP.h> 266 #define LCD_PIXELS 8192 268 #define LCD_BYTES 1024 274 #define LCD_X_MAX (LCD_COLS - 1) 280 #define LCD_Y_MAX (LCD_ROWS - 1) 284 #define LCD_PAGE_ROWS 8 286 #define LCD_CHAR_WIDTH 6 288 #define LCD_FONT_WIDTH 5 514 extern void LCD_close(LCD_Handle handle);
591 unsigned int bufIndex,
593 unsigned int uiValue,
594 unsigned char ucFormat,
595 unsigned char ucLine);
611 extern void LCD_update(LCD_Handle handle,
unsigned int bufIndex);
650 unsigned int bufIndex,
651 unsigned char ucXFrom,
738 unsigned int bufIndex,
739 unsigned char ucXFrom,
770 unsigned int bufIndex,
771 unsigned char ucXFrom,
772 unsigned char ucYFrom,
774 unsigned char ucYTo);
809 unsigned int bufIndex,
810 unsigned char ucXFrom,
845 unsigned int bufIndex,
887 unsigned int bufIndex,
889 LCD_Align iAlignment,
922 unsigned int bufIndex,
963 unsigned int bufIndex,
965 LCD_Align iAlignment,
1005 unsigned int bufIndex,
1007 unsigned char ucDecimals,
1050 unsigned int bufIndex,
1052 unsigned char ucDecimals,
1053 LCD_Align iAlignment,
1083 unsigned int bufIndex,
1084 unsigned char ucXFrom,
1085 unsigned char ucYFrom,
1086 unsigned char ucXTo,
1087 unsigned char ucYTo);
1116 unsigned int bufIndex,
1117 unsigned char ucXFrom,
1118 unsigned char ucYFrom,
1119 unsigned char ucXTo,
1120 unsigned char ucYTo);
1146 unsigned int bufIndex,
1147 unsigned char ucXFrom,
1148 unsigned char ucXTo,
1175 unsigned int bufIndex,
1176 unsigned char ucXFrom,
1177 unsigned char ucXTo,
1204 unsigned int bufIndex,
1206 unsigned char ucYFrom,
1207 unsigned char ucYTo);
1233 unsigned int bufIndex,
1235 unsigned char ucYFrom,
1236 unsigned char ucYTo);
1264 unsigned int bufIndex,
1265 unsigned char ucXFrom,
1266 unsigned char ucXTo,
1295 unsigned int bufIndex,
1297 unsigned char ucYFrom,
1298 unsigned char ucYTo);
1320 extern void LCD_bufferSetPx(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucY);
1341 extern void LCD_bufferClearPx(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucY);
1362 extern void LCD_bufferCopy(LCD_Handle handle,
unsigned int fromBufIndex,
unsigned int toBufIndex);
1378 extern void LCD_setContrast(LCD_Handle handle,
unsigned char ucContrast);
char displayStartLine
Definition: LCDDogm1286.h:377
LCD_Command const * LCD_initCmd
Definition: LCDDogm1286.h:448
ADC_Params params
Definition: Driver_Init.h:11
void LCD_bufferInvertPage(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPage)
This function inverts a range of columns in the display buffer on a specified page (for example...
void LCD_bufferClearPage(LCD_Handle handle, unsigned int bufIndex, LCD_Page iPage)
This function clears the page specified by iPage in the given buffer.
void LCD_Params_init(LCD_Params *params)
Function to initialize the LCD_Params struct to its defaults.
char setPage
Definition: LCDDogm1286.h:391
void LCD_writeLine(LCD_Handle handle, unsigned int bufIndex, char *str, unsigned int uiValue, unsigned char ucFormat, unsigned char ucLine)
Function that writes a string and value to a buffer and sends it to the LCD display. The written page is being cleared before it is written to.
void LCD_bufferPrintString(LCD_Handle handle, unsigned int bufIndex, const char *pcStr, unsigned char ucX, LCD_Page iPage)
Function that writes a string to the specified buffer.
void LCD_bufferCopy(LCD_Handle handle, unsigned int fromBufIndex, unsigned int toBufIndex)
This function copies the content of fromBufIndex to toBufIndex.
Definition: LCDDogm1286.h:306
unsigned int bufSize
Definition: LCDDogm1286.h:410
char contrastSet1
Definition: LCDDogm1286.h:386
void LCD_bufferClearVLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function clears a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) from the buffer specified...
void LCD_bufferSetPx(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY)
This function sets a pixel on (ucX,ucY).
Serial Peripheral Interface (SPI) Driver Interface.
void LCD_bufferClear(LCD_Handle handle, unsigned int bufIndex)
Function that empties the specified LCD buffer.
struct LCD_Config LCD_Config
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
bool isOpen
Definition: LCDDogm1286.h:422
LCD_Align
LCD alignment enum.
Definition: LCDDogm1286.h:302
void LCD_bufferPrintFloat(LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, unsigned char ucX, LCD_Page iPage)
This function writes a number of data type float to the given buffer at a specified column and page...
uint8_t spiIndex
Definition: LCDDogm1286.h:457
char adcSet
Definition: LCDDogm1286.h:378
struct LCD_Params LCD_Params
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set usin...
LCD Object.
Definition: LCDDogm1286.h:419
unsigned int lcdWriteTimeout
Definition: LCDDogm1286.h:424
struct LCD_HWAttrs LCD_HWAttrs
LCD Hardware attributes.
char columnLo
Definition: LCDDogm1286.h:393
LCD_Buffer used to store data to be printed on the LCD display.
Definition: LCDDogm1286.h:407
char staticIndicator1
Definition: LCDDogm1286.h:389
static const LCD_Command LCD_initCmd
Definition: LCDDogm1286.h:482
Definition: LCDDogm1286.h:338
void LCD_bufferClearHLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function clears a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) from the specified buffer...
struct LCD_Object LCD_Object
LCD Object.
void LCD_bufferPrintIntAligned(LCD_Handle handle, unsigned int bufIndex, int i32Number, LCD_Align iAlignment, LCD_Page iPage)
This function writes an integer to the given buffer as specified by the iAlignment argument...
void LCD_bufferSetLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function draws a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
Definition: LCDDogm1286.h:304
uint8_t lcdCsnPin
Definition: LCDDogm1286.h:454
LCD_Page
LCD page enum.
Definition: LCDDogm1286.h:316
#define LCD_ROWS
Definition: LCDDogm1286.h:276
SPI_FrameFormat spiFrameFormat
Definition: LCDDogm1286.h:368
void LCD_close(LCD_Handle handle)
Function to close the LCD instance specified by the LCD handle.
void LCD_bufferClearLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function clears a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
Definition: LCDDogm1286.h:319
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set usin...
Definition: LCDDogm1286.h:362
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
Definition: LCDDogm1286.h:466
LCD_Handle LCD_open(LCD_Buffer *buffers, uint8_t nBuffers, LCD_Params *params)
Function to set up the DOGM128W-6 LCD display.
struct LCD_Buffer LCD_Buffer
LCD_Buffer used to store data to be printed on the LCD display.
void LCD_init(void)
This function initializes the LCD driver module.
void LCD_bufferPrintFloatAligned(LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, LCD_Align iAlignment, LCD_Page iPage)
This function writes a float number to the given buffer as specified by the iAlignment argument...
#define LCD_COLS
Definition: LCDDogm1286.h:270
void LCD_bufferPrintInt(LCD_Handle handle, unsigned int bufIndex, int i32Number, unsigned char ucX, LCD_Page iPage)
Function that writes an integer to the specified buffer.
LCD_X_Limit
LCD x-axis enum.
Definition: LCDDogm1286.h:336
Definition: LCDDogm1286.h:321
void LCD_bufferPrintStringAligned(LCD_Handle handle, unsigned int bufIndex, const char *pcStr, LCD_Align iAlignment, LCD_Page iPage)
This function writes a string to the given buffer specified by the iAlignment argument.
char contrastSet2
Definition: LCDDogm1286.h:387
char columnHi
Definition: LCDDogm1286.h:392
void LCD_bufferClearPx(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY)
This function clears the pixel at (ucX,ucY).
uint8_t nBuffers
Definition: LCDDogm1286.h:428
Definition: LCDDogm1286.h:324
void LCD_bufferClearPart(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo)
This function clears the pixels in a given piece of a page. Resolution is given in coulmns [0–127] a...
uint8_t lcdModePin
Definition: LCDDogm1286.h:450
LCD Hardware attributes.
Definition: LCDDogm1286.h:445
Definition: LCDDogm1286.h:320
char staticIndicator0
Definition: LCDDogm1286.h:388
unsigned int lcdWriteTimeout
Definition: LCDDogm1286.h:364
Definition: LCDDogm1286.h:325
struct LCD_Config * LCD_Handle
A handle that is returned from a LCD_open() call.
Definition: LCDDogm1286.h:293
char outputMode
Definition: LCDDogm1286.h:379
struct LCD_Command LCD_Command
Format of LCD commands used by the LCD controller.
char contrastSet0
Definition: LCDDogm1286.h:385
SPI Global configuration.
Definition: SPI.h:744
uint8_t lcdResetPin
Definition: LCDDogm1286.h:452
Definition: LCDDogm1286.h:305
LCD_Buffer * lcdBuffers
Definition: LCDDogm1286.h:426
char displayType
Definition: LCDDogm1286.h:380
void LCD_bufferVArrow(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function draws a vertical arrow from (ucX,ucYFrom) to (ucX,ucYTo) to the buffer specified...
void LCD_update(LCD_Handle handle, unsigned int bufIndex)
Function that writes the specified buffer to the LCD display.
char lcdBias
Definition: LCDDogm1286.h:381
void LCD_bufferSetVLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function draws a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) into the specified buffer...
char boosterRadio1
Definition: LCDDogm1286.h:384
void LCD_bufferInvert(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function inverts the pixels (bits) in a given region of the specified buffer.
Definition: LCDDogm1286.h:339
void LCD_updatePart(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo)
Function that sends the specified part of the given buffer to the corresponding part on the LCD...
Definition: LCDDogm1286.h:352
LCD_Object * object
Definition: LCDDogm1286.h:469
Definition: LCDDogm1286.h:323
char displayEn
Definition: LCDDogm1286.h:390
Definition: LCDDogm1286.h:351
char * pcBuffer
Definition: LCDDogm1286.h:409
Format of LCD commands used by the LCD controller.
Definition: LCDDogm1286.h:375
char powerControl
Definition: LCDDogm1286.h:382
void LCD_bufferSetHLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function draws a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) into the specified buffer...
void LCD_bufferHArrow(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function draws a horizontal arrow from (ucXFrom,ucY) to (ucXTo,ucY) to buffer specified...
Definition: LCDDogm1286.h:318
SPI_Handle spiHandle
Definition: LCDDogm1286.h:423
SemaphoreP_Struct lcdMutex
Definition: LCDDogm1286.h:425
void LCD_setContrast(LCD_Handle handle, unsigned char ucContrast)
This Function sets the LCD contrast.
char boosterRadio0
Definition: LCDDogm1286.h:383
unsigned int spiBitRate
Definition: LCDDogm1286.h:367
SPI_FrameFormat
Definitions for various SPI data frame formats.
Definition: SPI.h:601
Definition: LCDDogm1286.h:326
Definition: LCDDogm1286.h:322
SemaphoreP_Struct bufMutex
Definition: LCDDogm1286.h:411
LCD_HWAttrs const * hwAttrs
Definition: LCDDogm1286.h:471
LCD_Y_Limit
LCD y-axis enum.
Definition: LCDDogm1286.h:349