33 #ifndef ti_drivers_cryptoutils_ecc_ECCParamsCC26X4_s__include 34 #define ti_drivers_cryptoutils_ecc_ECCParamsCC26X4_s__include int_fast16_t ECCParams_s_getUncompressedGeneratorPoint(const ECCParams_CurveParams *curveParams, uint8_t *buffer, size_t length)
Veneer to extract the curve generator point from an ecliptic curve description.
const ECCParams_CurveParams * ECCParams_s_getCurveParams(const ECCParams_CurveParams *curveParams)
Returns a pointer to curve params stored in secure memory.
A structure containing the parameters of an elliptic curve.
Definition: ECCParams.h:140