69 #ifndef ti_drivers_aesctr_AESCTRCC26XX__include 70 #define ti_drivers_aesctr_AESCTRCC26XX__include 77 #include <ti/devices/DeviceFamily.h> 78 #include DeviceFamily_constructPath(driverlib/aes.h) 115 uint32_t counter[AES_BLOCK_SIZE / 4];
138 bool AESCTR_acquireLock(
AESCTR_Handle handle, uint32_t timeout);
volatile int_fast16_t returnStatus
Definition: AESCTRCC26XX.h:123
void(* AESCTR_CallbackFxn)(AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_OperationUnion *operation, AESCTR_OperationType operationType)
The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_C...
Definition: AESCTR.h:666
size_t inputLength
Definition: AESCTRCC26XX.h:121
AES Global configuration.
Definition: AESCommon.h:154
const uint8_t * input
Definition: AESCTRCC26XX.h:119
AESCTR_OperationType
Enum for the operation types supported by the driver.
Definition: AESCTR.h:623
CryptoKey datastructure.
Definition: CryptoKey.h:198
AESCTR_ReturnBehavior
The way in which CTR function calls return after performing an encryption or decryption operation...
Definition: AESCTR.h:482
volatile bool cryptoResourceLocked
Definition: AESCTRCC26XX.h:128
volatile bool hwBusy
Definition: AESCTRCC26XX.h:129
uint32_t semaphoreTimeout
Definition: AESCTRCC26XX.h:116
uint8_t intPriority
Crypto Peripheral's interrupt priority.
Definition: AESCTRCC26XX.h:105
bool isOpen
Definition: AESCTRCC26XX.h:126
CryptoKey key
Definition: AESCTRCC26XX.h:122
AESCTRCC26XX Object.
Definition: AESCTRCC26XX.h:113
uint8_t * output
Definition: AESCTRCC26XX.h:120
AESCTR_ReturnBehavior returnBehavior
Definition: AESCTRCC26XX.h:124
AESCTRCC26XX Hardware Attributes.
Definition: AESCTRCC26XX.h:90
AESCTR_OperationUnion * operation
Definition: AESCTRCC26XX.h:118
Union containing a reference to a one-step and segmented operation structure.
Definition: AESCTR.h:585
AESCTR_CallbackFxn callbackFxn
Definition: AESCTRCC26XX.h:117
AESCTR_OperationType operationType
Definition: AESCTRCC26XX.h:125
volatile bool operationInProgress
Definition: AESCTRCC26XX.h:130
bool threadSafe
Definition: AESCTRCC26XX.h:127