|
|
[HW_INC] | Hardware interface description |
[DRV_API] | Driverlib Application interface |
[DRV_SRC] | Driverlib source code |
[DRV_DOC] | Driverlib documentation |
[DRV_LIB] | Prebuilt libraries |
ChipInfo_ChipFamilyIs_CC13x4_CC26x4()
(LPRFXXWARE-670)GPIO_readMultiDio()
, GPIO_writeMultiDio()
, GPIO_setMultiDio()
, GPIO_clearMultiDio()
SysCtrlShutdownWithAbort()
so it aborts on the first pin with an event, rather than checking them allCCFG_MODE_CONF.VDDR_CAP
from all supported devices (LPRFXXWARE-361)
ADI_4_AUX_O_MUX2
in aux_dac.c causing a fault on CC13x4/CC26x4 family devices (Cortex-M33F) due to its unaligned address (LPRFXXWARE-607)XOSC_HF_COLUMN_Q12
setting in FCFG1. The workaround is disabled by default, but can be enabled by setting CCFG_SIZE_AND_DIS_FLAGS_DIS_LINEAR_CAPARRAY_DELTA_WORKAROUND = 0
in the Customer Configuration Area (CCFG) (LPRFXXWARE-444, LPRFXXWARE-487, LPRFXXWARE-489).