Using the AUX RAM as RAM¶
For variants other than the CC13x1x3 or CC26x1x3, you can use this memory as RAM for your application if it does not use the Sensor Controller. However, access to this memory is significantly slower than access to the SRAM. This may lead to increased power consumption and slower program execution. Additionally, if using the AUX RAM as RAM it is important that you test thoroughly. Certain objects, when put in AUX RAM can cause the application to crash. One should test for each object they want to store in AUX RAM.
Important
The Application Processor (AP) can do other tasks while the data is being transferred to AUX RAM, but if the bus buffer gets full during back to back writes, it will stall the AP until there is free space in the buffer. After you write a series of data to AUX RAM you should implement a singe read access to make sure all the data has been written. The read access will stall the AP until all the data has been transferred to AUX RAM.
Modifying the application¶
Open the project properties and add the symbol
AUX_AS_RAM=1
to the linker options:
In CCS, right click on the Project → select Properties → Build → ARM Linker → Advanced Options → Command File Preprocessing. Click on the small Add… button at the top right of the box Pre-define preprocessor macro _name_to_value_ and type the symbol
AUX_AS_RAM=1
.In IAR, right click on the Project → Options → Linker. Locate the box Configuration file symbol definitions and type the symbol
AUX_AS_RAM=1
.
Modify the linker command/configuration file. Each toolchain has different options, pragmas and syntax, therefore check the steps below for the three supported toolchains: TI ARMCL, TI ARM Clang and IAR.
TI ARMCL:
In the linker command file
cc26xx_app.cmd
, define the AUX_RAM memory area:#ifdef AUX_AS_RAM #define AUX_RAM_BASE 0x400E0000 #define AUX_RAM_SIZE 0x800 #endif /* AUX_AS_RAM */
Create a AUX_RAM memory section in
MEMORY{}
#ifdef AUX_AS_RAM AUX_RAM (RWX) : origin = AUX_RAM_BASE, length = AUX_RAM_SIZE #endif /* AUX_AS_RAM */
Add sections of memory or code to AUX_RAM in
SECTIONS{}
#ifdef AUX_AS_RAM reorganized_into_auxram { simple_peripheral.obj(.data) devinfoservice.obj(.data) simple_gatt_profile.obj(.data) icall.obj(.data) board.obj(.bss) } > AUX_RAM #endif/* AUX_AS_RAM */
The .obj files are listed in the FlashROM folder of the app project. They are also listed with size in the .map file. A detailed description of the linker command file and memory sections is given in this article Linker Command File Primer.
If you want more control over what is stored in AUX_RAM, individual
variables can be stored there with the #pragma DATA_SECTION
command.
Please note that this is only possible for global variables.
// Display Interface #pragma DATA_SECTION(dispHandle, "my_section") Display_Handle dispHandle = NULL;
You can find my_section
in the map-file. Here you will find the names of the
objects included in my_section
. In this case, the object is
simple_peripheral.obj (my_section)
.
#ifdef AUX_AS_RAM reorganized_into_auxram { simple_peripheral.obj(my_section) } > AUX_RAM #endif /* AUX_AS_RAM */
Important
When making alterations only to the linker command file, please make sure to press Rebuild, not just Build. (CCS will not recognize that you have made changes to the project before you press Rebuild.)
TI ARM Clang:
The linker command file is very similar to the TI ARMCL toolchain. For additional details, check chapter 5 of the TI ARM Clang User’s Guide.
In the linker command file
cc26xx_app.cmd
, define the AUX_RAM memory area:#ifdef AUX_AS_RAM #define AUX_RAM_BASE 0x400E0000 #define AUX_RAM_SIZE 0x800 #endif /* AUX_AS_RAM */
Create a AUX_RAM memory section in
MEMORY{}
#ifdef AUX_AS_RAM AUX_RAM (RWX) : origin = AUX_RAM_BASE, length = AUX_RAM_SIZE #endif /* AUX_AS_RAM */
Add sections of memory or code to AUX_RAM in
SECTIONS{}
#ifdef AUX_AS_RAM reorganized_into_auxram { simple_peripheral.o(.data) devinfoservice.o(.data) simple_gatt_profile.o(.data) icall.o(.data) board.o(.bss) } > AUX_RAM #endif/* AUX_AS_RAM */
The .o files are listed in the FlashROM folder of the app project. They are also listed with size in the .map file. A detailed description of the linker command file and memory sections is given in this article Linker Command File Primer.
If you want more control over what is stored in AUX_RAM, individual
variables can be stored there with the __attribute__((section("section_name")))
command.
Please note that this is only possible for global variables.
// Display Interface __attribute__((section("my_section"))) Display_Handle dispHandle = NULL;
You can find my_section
in the map-file. Here you will find the names of the
objects included in my_section
. In this case, the object is
simple_peripheral.o (my_section)
.
#ifdef AUX_AS_RAM reorganized_into_auxram { simple_peripheral.o(my_section) } > AUX_RAM #endif /* AUX_AS_RAM */
Important
When making alterations only to the linker command file, please make sure to press Rebuild, not just Build. (CCS will not recognize that you have made changes to the project before you press Rebuild.)
IAR:
Open the linker configuration file
cc26xx_app.icf
. UnderMemory Definitions
, add//////////////////////////////////////////////////////////////////////////////// // AUX_RAM // if ( isdefinedsymbol(AUX_AS_RAM) ) { define symbol AUX_RAM_START = 0x400E0000; define symbol AUX_RAM_SIZE = 0x800; define symbol AUX_RAM_END = AUX_RAM_START + AUX_RAM_SIZE; }
Under
Memory Regions
, addif ( isdefinedsymbol(AUX_AS_RAM) ) { define region AUX_RAM = mem:[from AUX_RAM_START to AUX_RAM_END]; }
Under
Memory Placement
, addif ( isdefinedsymbol(AUX_AS_RAM) ) { // AUX_RAM define block AUXDATA { section .data object simple_peripheral.o, section .data object devinfoservice.o, section .data object simple_gatt_profile, section .data object icall.o, section .data object board.o}; place in AUX_RAM { block AUXDATA }; }
The .o-files are listed in the .map file. For more information on the linker configuration file, please see IAR C/C++ Development Guide.
If you want more control over what is stored in AUX_RAM, individual
variables can be stored there with the #pragma location
command.
Please note that this is only possible for global variables.
Listing 37. Move the global display handle variable into a new Cache RAM section calledmy_section
.¶// Display Interface #pragma location="my_section" Display_Handle dispHandle = NULL;
You can find my_section
in the map-file. Here you will find the names of the
objects included in my_section
. In this case, the object is
simple_peripheral.o (my_section)
.
if ( isdefinedsymbol(AUX_AS_RAM) ) { // AUX_RAM define block AUXDATA { section my_section object simple_peripheral.o }; place in AUX_RAM { block AUXDATA }; }