AESGCMCC26X4.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
70 #ifndef ti_drivers_aesgcm_AESGCMCC26X4__include
71 #define ti_drivers_aesgcm_AESGCMCC26X4__include
72 
73 #include <stdint.h>
74 #include <stdbool.h>
75 
76 #include <ti/drivers/Power.h>
77 #include <ti/drivers/AESGCM.h>
79 
80 #include <ti/drivers/dpl/HwiP.h>
81 #include <ti/drivers/dpl/SwiP.h>
82 #include <ti/drivers/dpl/SemaphoreP.h>
83 
84 #include <ti/devices/DeviceFamily.h>
85 #include DeviceFamily_constructPath(driverlib/aes.h)
86 
87 #ifdef __cplusplus
88 extern "C" {
89 #endif
90 
97 typedef struct
98 {
112  uint8_t intPriority;
114 
120 typedef struct
121 {
122  uint32_t intermediateIV[AES_IV_LENGTH_BYTES / 4];
123  uint32_t intermediateTag[AES_TAG_LENGTH_BYTES / 4];
124  uint32_t blockCounter;
133  volatile int_fast16_t returnStatus;
136  /* Track when to set gcm_ccm_continue or continue_aad bit */
139  bool isOpen;
140  volatile bool operationInProgress;
141  volatile bool hwBusy;
142  volatile bool cryptoResourceLocked;
144 
145 #ifdef __cplusplus
146 }
147 #endif
148 
149 #endif /* ti_drivers_aesgcm_AESGCMCC26X4__include */
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESGCMCC26X4.h:112
volatile int_fast16_t returnStatus
Definition: AESGCMCC26X4.h:133
The CryptoKey type is an opaque representation of a cryptographic key.
AESGCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESGCM.h:860
size_t actualAADLength
Definition: AESGCMCC26X4.h:130
uint32_t semaphoreTimeout
Definition: AESGCMCC26X4.h:125
volatile bool operationInProgress
Definition: AESGCMCC26X4.h:140
Power Manager.
AESGCM driver header.
CryptoKey datastructure.
Definition: CryptoKey.h:192
AESGCM_ReturnBehavior returnBehavior
Definition: AESGCMCC26X4.h:134
AESGCMCC26X4 Object.
Definition: AESGCMCC26X4.h:120
size_t expectedPlaintextLength
Definition: AESGCMCC26X4.h:129
AESGCM_OperationType operationType
Definition: AESGCMCC26X4.h:135
bool isOpen
Definition: AESGCMCC26X4.h:139
void(* AESGCM_CallbackFxn)(AESGCM_Handle handle, int_fast16_t returnValue, AESGCM_OperationUnion *operation, AESGCM_OperationType operationType)
The definition of a callback function used by the AESGCM driver when used in AESGCM_RETURN_BEHAVIOR_C...
Definition: AESGCM.h:890
AESGCM_ReturnBehavior
The way in which GCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESGCM.h:674
bool continueAADOperation
Definition: AESGCMCC26X4.h:137
bool continueDataOperation
Definition: AESGCMCC26X4.h:138
volatile bool cryptoResourceLocked
Definition: AESGCMCC26X4.h:142
size_t actualPlaintextLength
Definition: AESGCMCC26X4.h:131
size_t expectedAADLength
Definition: AESGCMCC26X4.h:128
AESGCMCC26X4 Hardware Attributes.
Definition: AESGCMCC26X4.h:97
volatile bool hwBusy
Definition: AESGCMCC26X4.h:141
Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize oper...
Definition: AESGCM.h:848
AESGCM_CallbackFxn callbackFxn
Definition: AESGCMCC26X4.h:126
CryptoKey key
Definition: AESGCMCC26X4.h:132
AESGCM_OperationUnion * operation
Definition: AESGCMCC26X4.h:127
uint32_t blockCounter
Definition: AESGCMCC26X4.h:124
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale