AESECBCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
72 #ifndef ti_drivers_aesecb_AESECBCC26XX__include
73 #define ti_drivers_aesecb_AESECBCC26XX__include
74 
75 #include <stdint.h>
76 #include <stdbool.h>
77 
78 #include <ti/drivers/Power.h>
79 #include <ti/drivers/AESECB.h>
81 
82 #include <ti/drivers/dpl/HwiP.h>
83 #include <ti/drivers/dpl/SwiP.h>
84 #include <ti/drivers/dpl/SemaphoreP.h>
85 
86 #ifdef __cplusplus
87 extern "C" {
88 #endif
89 
96 typedef struct
97 {
114  uint8_t intPriority;
116 
122 typedef struct
123 {
128  volatile int_fast16_t returnStatus;
131  bool isOpen;
133  volatile bool hwBusy;
134  volatile bool operationInProgress;
135  volatile bool cryptoResourceLocked;
137 
139 
145 bool AESECB_acquireLock(AESECB_Handle handle, uint32_t timeout);
146 void AESECB_releaseLock(AESECB_Handle handle);
147 void AESECB_enableThreadSafety(AESECB_Handle handle);
148 void AESECB_disableThreadSafety(AESECB_Handle handle);
150 
151 #ifdef __cplusplus
152 }
153 #endif
154 
155 #endif /* ti_drivers_aesecb_AESECBCC26XX__include */
AESECB_ReturnBehavior returnBehavior
Definition: AESECBCC26XX.h:129
bool isOpen
Definition: AESECBCC26XX.h:131
The CryptoKey type is an opaque representation of a cryptographic key.
volatile bool operationInProgress
Definition: AESECBCC26XX.h:134
uint32_t semaphoreTimeout
Definition: AESECBCC26XX.h:126
Power Manager.
AES Global configuration.
Definition: AESCommon.h:154
AESECB_CallbackFxn callbackFxn
Definition: AESECBCC26XX.h:125
CryptoKey datastructure.
Definition: CryptoKey.h:192
volatile bool cryptoResourceLocked
Definition: AESECBCC26XX.h:135
volatile int_fast16_t returnStatus
Definition: AESECBCC26XX.h:128
AESECB_ReturnBehavior
The way in which ECB function calls return after performing an encryption + authentication or decrypt...
Definition: AESECB.h:547
Struct containing the parameters required for encrypting/decrypting and a message.
Definition: AESECB.h:581
AESECB driver header.
volatile bool hwBusy
Definition: AESECBCC26XX.h:133
void(* AESECB_CallbackFxn)(AESECB_Handle handle, int_fast16_t returnValue, AESECB_Operation *operation, AESECB_OperationType operationType)
The definition of a callback function used by the AESECB driver when used in AESECB_RETURN_BEHAVIOR_C...
Definition: AESECB.h:652
bool threadSafe
Definition: AESECBCC26XX.h:132
AESECB_OperationType operationType
Definition: AESECBCC26XX.h:130
AESECB_OperationType
Enum for the operation types supported by the driver.
Definition: AESECB.h:627
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESECBCC26XX.h:114
AESECBCC26XX Hardware Attributes.
Definition: AESECBCC26XX.h:96
CryptoKey key
Definition: AESECBCC26XX.h:127
AESECB_Operation * operation
Definition: AESECBCC26XX.h:124
AESECBCC26XX Object.
Definition: AESECBCC26XX.h:122
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale