AESCCMCC26X4.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2021, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
70 #ifndef ti_drivers_aesccm_AESCCMCC26X4__include
71 #define ti_drivers_aesccm_AESCCMCC26X4__include
72 
73 #include <stdint.h>
74 #include <stdbool.h>
75 
76 #include <ti/drivers/Power.h>
77 #include <ti/drivers/AESCCM.h>
79 
80 #include <ti/drivers/dpl/HwiP.h>
81 #include <ti/drivers/dpl/SwiP.h>
82 #include <ti/drivers/dpl/SemaphoreP.h>
83 
84 #include <ti/devices/DeviceFamily.h>
85 #include DeviceFamily_constructPath(driverlib/aes.h)
86 
87 #ifdef __cplusplus
88 extern "C" {
89 #endif
90 
97 typedef struct
98 {
112  uint8_t intPriority;
114 
120 typedef struct
121 {
122  uint32_t intermediateIV[AES_IV_LENGTH_BYTES / 4];
123  uint32_t intermediateTag[AES_TAG_LENGTH_BYTES / 4];
124  uint32_t blockCounter;
125  uint32_t alignmentInfo;
134  volatile int_fast16_t returnStatus;
137  /* MAC and nonceLength are stored for configuring the AESCTL register */
138  uint8_t macLength;
139  uint8_t nonceLength;
140  /* Track when to set gcm_ccm_continue or continue_aad bit */
143  bool isOpen;
144  volatile bool operationInProgress;
145  volatile bool hwBusy;
146  volatile bool cryptoResourceLocked;
148 
149 #ifdef __cplusplus
150 }
151 #endif
152 
153 #endif /* ti_drivers_aesccm_AESCCMCC26X4__include */
uint8_t macLength
Definition: AESCCMCC26X4.h:138
The CryptoKey type is an opaque representation of a cryptographic key.
uint32_t semaphoreTimeout
Definition: AESCCMCC26X4.h:126
AESCCM_ReturnBehavior returnBehavior
Definition: AESCCMCC26X4.h:135
uint8_t nonceLength
Definition: AESCCMCC26X4.h:139
Power Manager.
bool continueAADOperation
Definition: AESCCMCC26X4.h:141
CryptoKey datastructure.
Definition: CryptoKey.h:192
volatile int_fast16_t returnStatus
Definition: AESCCMCC26X4.h:134
CryptoKey key
Definition: AESCCMCC26X4.h:133
uint32_t alignmentInfo
Definition: AESCCMCC26X4.h:125
size_t expectedPlaintextLength
Definition: AESCCMCC26X4.h:130
volatile bool cryptoResourceLocked
Definition: AESCCMCC26X4.h:146
AESCCM_OperationType operationType
Definition: AESCCMCC26X4.h:136
size_t expectedAADLength
Definition: AESCCMCC26X4.h:129
size_t actualAADLength
Definition: AESCCMCC26X4.h:131
volatile bool hwBusy
Definition: AESCCMCC26X4.h:145
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_OperationUnion *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:1059
Union containing a reference to a one step, segmented AAD, segmented data, or segmented finalize oper...
Definition: AESCCM.h:1017
AESCCMCC26X4 Hardware Attributes.
Definition: AESCCMCC26X4.h:97
size_t actualPlaintextLength
Definition: AESCCMCC26X4.h:132
AESCCMCC26X4 Object.
Definition: AESCCMCC26X4.h:120
uint32_t blockCounter
Definition: AESCCMCC26X4.h:124
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:1029
bool isOpen
Definition: AESCCMCC26X4.h:143
uint8_t intPriority
Crypto Peripheral&#39;s interrupt priority.
Definition: AESCCMCC26X4.h:112
AESCCM_ReturnBehavior
The way in which CCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESCCM.h:836
AESCCM_OperationUnion * operation
Definition: AESCCMCC26X4.h:128
AESCCM driver header.
volatile bool operationInProgress
Definition: AESCCMCC26X4.h:144
bool continueDataOperation
Definition: AESCCMCC26X4.h:142
AESCCM_CallbackFxn callbackFxn
Definition: AESCCMCC26X4.h:127
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale