Clock accuracies and Bluetooth LE

The Bluetooth Core Specifications Version 5.2 defines two clock accuracies, the “Active clock accuracy” (Bluetooth Core Specifications Version 5.2 Vol 6, Part B, §4.2.1) and the “Sleep clock accuracy” (Bluetooth Core Specifications Version 5.2 Vol 6, Part B, §4.2.1). In general, the HF XTAL (high frequency crystal oscillator) is used as active clock and the LF XTAL (low frequency crystal oscillator) is used as sleep clock. Tuning of the HF XTAL and LF XTAL is discussed in the HW Configuration Guide.

The Bluetooth Core Specifications Version 5.2 require the active clock to have a drift less than or equal to ±50 ppm and there is no way (nor need) to specify its accuracy to the TI BLE5-Stack.

The Bluetooth Core Specifications Version 5.2 require the sleep clock to have a drift less than or equal to ±500 ppm. The accuracy of this clock has a real impact on the timing of the radio operations. This is why its accuracy should be communicated to the TI BLE5-Stack using the function HCI_EXT_SetSCACmd().

As mentioned before, the accuracy of the sleep clock has an impact on the timing of the radio operations. This effect is called window widening and is described in details in the Bluetooth Core Specifications Version 5.2 Vol 6, Part B, §4.2.4.

The Link Layer is expecting to receive a packet within a certain window (extending from receiveWindowStart to receiveWindowEnd) or at a certain time (in which case receiveWindowStart and receiveWindowEnd are both that time) but, because of active clock accuracies and sleep clock accuracies there is uncertainty as to the exact timing of that window at the sending Link Layer. The recipient should therefore adjust its listening time to allow for this uncertainty. The increase in listening time is called the window widening. Assuming the clock inaccuracies are purely given in parts per million (ppm), it is calculated as follows:

\textrm{transmitterAllowance} = (\textrm{txCA} / \textrm{1000000}) * (\textrm{receiveWindowEnd} - \textrm{timeOfLastSync}) + \textrm{J us}

where J shall be 2 when the active clock applies and 16 when the sleep clock applies and the other parameters are specified in Table 4.1. of Bluetooth Core Specifications Version 5.2 Vol 6, Part B, §4.2.4.

The connection parameters can be chosen independently of the clock accuracy – absolutely all the combinations of clock accuracy and connection parameters are allowed. As can be observed in the formula, for a given clock accuracy, the listening window length is proportional to the effective connection interval. At a certain point this might have a significant impact on the energy consumption.

Using 32-kHz Crystal-Less Mode

BLE5-Stack 2.02.06.00 includes support for operating the CC13xx or CC26xx in a 32-kHz crystal-less mode for peripheral and broadcaster (beacon) role configurations. By using the internal low-frequency RC oscillator (RCOSC_LF), the 32-kHz crystal can be removed from the board layout.

The Running Bluetooth Low Energy on CC2640 Without 32 kHz Crystal application note provides details on the tradeoffs of such configuration.

There are a few steps that must be taken to enable 32-kHz crystal-less mode. Please refer to below sections based on the type of project.

  • SysConfig enabled projects

  • BIM projects (bim_onchip and bim_offchip)

  • non-SysConfig enabled projects

SysConfig enabled projects

Bluetooth LE examples should be configured to use RCOSC_LF using the SysConfig Advanced Settings.

For OAD projects, make sure to also configure the BIM to use RCOSC_LF (see below).

BIM projects

Review the comments in the file Application`ccfg_app.c` and add the following code at the end of the file.

Listing 172. Set CCFG to use RCOSC_LF as LF clock source
#define SET_CCFG_MODE_CONF_SCLK_LF_OPTION       0x3

Non-SysConfig enabled projects

Note

Certain projects provide a build target already enabling the following. In that case we recommend to leverage it.

For any peripheral project, the following change is required in order to enable RCOSC_LF. You will find more detail regarding this feature in the aforementioned application note.

  1. Include `rcosc_calibration.c, rcosc_calibration.h and ccfg_app_ble_rcosc.c files which are located at <SDK_INSTALL_DIR>\source\ti\ble5stack\common\cc26xx\rcosc

  2. Exclude ccfg_app_ble.c from build.

  3. Add USE_RCOSC to the .opt file containing the application defines.

  4. Add the following code to your peripheral project.c

    Listing 173. RCOSC calibration include
    #ifdef USE_RCOSC
    #include "rcosc_calibration.h"
    #endif //USE_RCOSC
    
  5. Add the following code to your peripheralproject_init function in peripheral project.c

    Listing 174. RCOSC calibration enable
    #ifdef USE_RCOSC
    RCOSC_enableCalibration();
    #endif // USE_RCOSC
    
  6. If using a custom board file, enable the RCOSC in the power policy. When using SysConfig to generate a board file, be sure to select Calibrate RCOSC_LF in the TI Drivers -> Power settings menu in SysConfig.

  7. Constrain the temperature variation to be less than 1°C/sec. If the temperature is to change faster than 1°C/sec, then a short calibration interval must be used. Calibration interval can be tuned in rcosc_calibration.h

    Listing 175. RCOSCLF calibration interval
    // 1000 ms
    #define RCOSC_CALIBRATION_PERIOD   1000
    

Note

Use of the internal RCOSC_LF requires a sleep clock accuracy (SCA) of 500 ppm.

Initial Board Bring Up

When powering up a custom board with the CC13xx or CC26xx for the first time, it is recommended to follow the Board Bring-Up section on CC13xx/CC26xx Hardware Configuration and PCB Design Considerations. After confirming that the board is being powered correctly by the battery or power supply and can be identified by the JTAG tool, programming the device with a minimal SW application to verify stability is also suggested.

TI recommends using the simple_peripheral sample application for initial board bring up with modifications to the ti_drivers_config.c file to:

  1. Disable all GPIO pin access

  2. Select the correct RF front end setting (done by SysConfig)

The TI BLE5-Stack does not require any GPIO pins to be configured in order to establish and maintain a BLE connection. Ensure that Display_DISABLE_ALL is defined in the application Predefined Symbols so that diagnostic logging data is not routed to any GPIO pin. If your custom board uses a different device configuration, such as the 32 kHz crystal-less RCOSC_LF configuration, be sure to make these device changes to the project. With this minimal application configuration you should be able to establish a BLE connection (e.g., with a smart phone or BTool) to your board at the expected range. If you are not able to complete this step, then it is likely there is a misconfiguration of the RF front end or you have other board related or layout issues.

After confirming that your board can maintain a BLE connection, you can now validate that your BLE application functions as expected on the custom board. Again, it is suggested to enable your GPIO pins one at a time in the board file and comment-out access to other GPIO pins in your application. If you do encounter a CPU exception (HWI abort) during this phase it is likely that a GPIO pin is incorrectly mapped in your custom board file or your application is attempting to access a GPIO pin that does not exist in your device package type.