CC13xx/CC26xx SimpleLink Core SDK 6.10.00.13 Release Notes
Table of Contents
Introduction
This is a GA release of the Core SDK 6.10.00.13 for the CC26xx and CC13xx devices.
Documentation
Open the documentation overview web page file in the SDK’s Doc folder for a full list of documentation.
What’s New
- Added board support and examples for LP_CC2651R3SIPA.
- Implements new RNG driver. This new RNG driver will wrap TRNG and AES CTR DRBG drivers to provide a singleton instance driver, which provides a single source of entropy for the system.
- A summary of changes made in the current release of this product can be found in the product Change Log.
Upgrade and Compatibility Information
- Deprecating and removing support for PIN Driver in the next release.
- Deprecating and removing support for TIRTOS version 6 (tirtos) in the next release.
- Deprecating UART driver, in favor of UART2 in the next release.
Host Support
See the SDK release notes for a description of which host operating systems are supported in this release.
Dependencies
See the SDK release notes for a description of which components and tools are required to work with this product.
Device Support
See the SDK release notes for a list of TI devices that are supported in this product.
Validation Information
The Core SDK was validated with the following components:
- Code Composer Studio 11.2.0
- ARM 20.2.5.LTS
- GNU Code Generation Tools
- ARM GCC 9.2019.q4.major
- IAR Code Generation Tools
- ARM 8.50.1
- TI Clang Code Generation Tools
- ARM ti-cgt-armllvm_1.3.1.LTS
- FreeRTOS 202104.00
- SysConfig 1.10.0
- XDCTools 3.62.01.15
New Features
| ID | Summary |
|---|---|
| TIDRIVERS-5345 | Move GPIO_INVALID_INDEX validation into the driver |
| TIDRIVERS-5124 | Add support for little endian Curve25519 keys in ECDH driver |
| TIDRIVERS-5116 | Implement new RNG driver |
| LPRFXXWARE-619 | Add support for CC13x2x7/CC26x2x7 HW revision B (1.1) |
Fixed Issues
| ID | Summary |
|---|---|
| TIDRIVERS-5343 | Improper casting of initialization vector pointer in AES GCM driver |
| TIDRIVERS-5266 | Some includes are missing from the QueueP.h file |
| TIDRIVERS-5237 | PowerCC26X2_calibrateRCOSC.c does not implement TDC 4-phase handshake correctly |
| TIDRIVERS-5207 | LP_CC2652RSIP example projects target wrong device in CCS |
| TIDRIVERS-5206 | CC26X2R1_LAUNCHXL example projects target wrong device in CCS |
| TIDRIVERS-5171 | Default FreeRTOS CCS project has optimisation disabled |
| TIDRIVERS-5122 | Implicit invocation of intrinsics without including header |
| TIDRIVERS-5047 | UART2_close can cause hanging power constraints if used once a write operation concludes but before the End of Transmision interrupt occurs |
| TIDRIVERS-5046 | UART2_close can leave UART hardware instance UART_FR_BUSY bit set |
| TIDRIVERS-5044 | Abnormally high power consumption from DAC after disabling and closing |
| LPRFXXWARE-611 | CPUDelay() doesn't compile for TICLANG |
Known Issues
| ID | Summary |
|---|---|
| TIDRIVERS-5318 | GPIO_init clears external LF clock pin and stalls the device |
| TIDRIVERS-5310 | spiPollingTransfer at high clock frequency might cause RX FIFO overflow and lose data in master mode |
| TIDRIVERS-4844 | Implement restrictions in errata note IOC_01 in SysConfig |
| TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
| TIDRIVERS-1642 | NVSSPI25x driver does not work when using internal SPI CS |
Customer Support
- Use the E2E support forums for customer support.
- Use the External Bug and Enhancement System to track issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.
Prior Release Changes
A summary of changes made in previous releases of this product can be found in the product Change Log.