TI Wi-SUN FAN 1.0 Stack 01.00.03.00 Release Notes

Table of Contents

Introduction

Wi-SUN is an open, standards-based IPv6 Sub-1GHz mesh networking protocol designed for robust self-healing and secure large-scale networks with thousands of nodes. The network typically consists of line powered routers and gateways or border routers.

The TI Wi-SUN FAN 1.0 Stack is a set of sample applications, tools, APIs and protocol stack libraries that enable engineers to develop Wi-SUN FAN 1.0 standalone or network processor applications on the SimpleLink™ CC13xx family of wireless MCUs.

As part of the network processor offering, TI provides a python framework and an example host application. This can be found on TI Wi-SUN FAN Spinel CLI Reference on github.

In TI Wi-SUN FAN Stack, the 6LoWPAN, RPL, IPv6, ICMPv6 and UDP layers have been adapted from open source components. Additional information about TI’s Wi-SUN FAN solutions can be found at www.ti.com/wi-sun.

Key Features

Documentation

The SimpleLink CC13xx and CC26xx Software Development Kit (SDK) allows easier product development by combining TI-RTOS and the TI Wi-SUN FAN Stack in one unified SDK. All Wi-SUN sample applications are based off the TI-RTOS Kernel. Key documents needed for application development include:

Installation and Usage

What’s New

ID Summary
WISUN-499 Add TIRTOS7 support for CC13x2x7 devices
WISUN-476 Implement NCP command to read RSSI details of neighbor nodes

Fixed Issues

ID Summary
WISUN-507 Fixed issue in which operating mode ID not updated with Region for EU 50kbps PHY

Known Issues

ID Summary
WISUN-515 wisunstack stop command has no effect. Use software induced reset as a work-around to disconnect node
WISUN-502 Wi-SUN CC13x2 TIRTOS-6 projects do not build in CCS Cloud. Use standalone CCS as a work-around
WISUN-492 Wi-SUN: Border Router (BR) with FreeRTOS OS is limited to network size of 50 nodes for optimal performance. Note: TIRTOS based BR can scale up to network size of 100 nodes.

Upgrade and Compatibility Information

The frequency tolerance of the crystals on TI LaunchPads are not Wi-SUN compliant at extreme temperatures. For end products requiring very high or very low temperatures, make sure to use a crystal that ensures accuracy within the Wi-SUN specification.

Operating System Support

Please refer to the SDK release notes.

Dependencies

The TI Wi-SUN FAN sample applications were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.

Note: Earlier IDE/toolchain versions are not supported and compatibility with newer versions of supported IDEs is not assured.

The TI Wi-SUN FAN sample applications NWP mode were tested with the TI Wi-SUN FAN Spinel CLI Reference with release tag TI_WiSUN_STACK_01_00_02.

Device Support

Development Board Support

Validation

The TI Wi-SUN FAN sample applications were built & tested with versions of the following Integrated Development Environments (IDEs) and tool chains listed in the top-level SDK release notes:

Versioning

This product follows a version format, M.mm.pp.bb, where:

Technical Support and Product Updates