Power Management¶
All power-managment functionality is handled by the TI-RTOS power driver and are used by the peripheral drivers (e.g. UART, SPI, I2C, etc..). Applications can prevent, if they choose, the CC13xx or CC26xx from entering low power modes by setting a power constraint.
By default, all the examples in SimpleLink CC13xx/CC26xx SDK will put the CC13xx or CC26xx in standby mode if there is no task running. This is achieved by configuring the TI power driver and the kernel to do so, as shown in the following step.
In the
.cfgor.xscfg, you can find the following setting:/* ================ Idle configuration ================ */ var Idle = xdc.useModule('ti.sysbios.knl.Idle'); /* * The Idle module is used to specify a list of functions to be called when no * other tasks are running in the system. * * Functions added here will be run continuously within the idle task. * * Function signature: * Void func(Void); */ /* Allow power management */ Idle.addFunc('&Power_idleFunc');By doing this, the TI-RTOS kernel will call Power_idleFunc whenever this is no task running.
Power_idleFunctakes in policyFxn and policyFxn is defined using SysConfig tool Figure 19.. By default, TI sets thePowerCCxxxx_standbyPolicyas policyFxn.Power_idleFuncis defined in{SDK_INSTALL_DIR}\source\ti\drivers\power\PowerCCxxxx.candPowerCCxxxx_standbyPolicycan be found in{SDK_INSTALL_DIR}\kernel\tirtos\packages\ti\dpl\PowerCCxxxx_tirtos.c
Figure 19. Configure Power Policy for Idle Function.¶
In the sysconfig generated files, you will find the following example in ti_drivers_config.c.
1const PowerCC26XX_Config PowerCC26XX_config = { 2 .enablePolicy = true, 3 .policyInitFxn = NULL, 4 .policyFxn = PowerCC26XX_standbyPolicy, 5 .calibrateFxn = PowerCC26XX_calibrate, 6 .calibrateRCOSC_LF = true, 7 .calibrateRCOSC_HF = true, 8 .enableTCXOFxn = NULL 9};
More information on power-management functionality, see Power Management User’s Guide. These APIs are required only when using a custom driver.