SimpleLink CC13xx_CC26xx SDK Overview¶
TI’s royalty-free SimpleLink CC13xx/CC26xx SDK is a complete software platform for developing applications that require low-power, security, reliability, and mesh networking. This kit is based on the CC13xx or CC26xx SimpleLink Wireless MCU. Visit the SimpleLink MCU Platform homepage for more information about the SimpleLink ecosystem.
The SDK directory structure is broken down into a few major directories at the root to allow easy differentiation between documentation, examples, kernel source, and other source code. From the root directory, the sub-directories are:
docs/: All documentation for the SDK.
examples/: Source code and project definitions for example projects in the SDK.
kernel/: Source code and build tools for the kernels supported by the SDK.
source/ti/: Source code from Texas Instruments, excluding the kernel.
source/third_party/: Source code from third party vendors.
tools/: Scripts and definition files used by the SDK.
Table of contents
Further information
- TI-RTOS Kernel (SYS/BIOS) User’s Guide
Detailed information about the TI-RTOS kernel: scheduling, interrupts, synchronization.
- TI-RTOS Kernel (SYS/BIOS) API Reference
API documentation of the TI-RTOS kernel modules and their configuration parameters.
- TI Drivers API Reference
Doxygen API documentation of the high-level drivers.
- Power Management User’s Guide
Core SDK Power Management documentation.
- SimpleLink MCU SDK User’s Guide
SimpleLink MCU SDK User’s Guide.
- DriverLib API Reference
Doxygen API documentation of the low-level hardware abstraction layer.