RF commands reference

Please find a detailed description for each command in the Radio chapter of the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.

Protocol-Independent Direct Commands

Command name

Description

CMD_ABORT

Abort a running radio operation command immediately.

CMD_GET_RSSI

Read the current RSSI while an RX command is running.

CMD_PING

Respond with an interrupt event.

CMD_START_RAT

Start the RAT without synchronization to the RTC.

CMD_STOP

Abort a running radio operation command at the next possibility.

Protocol-Independent Immediate Commands

Command name

Description

CMD_ARM_RAT_CH

Enable counting for a given RAT channel.

CMD_BUS_REQUEST

Set or reset a dependency on the system bus.

CMD_DISABLE_RAT_CH

Disable RAT channel.

CMD_DISARM_RAT_CH

Disable counting for a given RAT channel.

CMD_GET_FW_INFO

Request information about the RF core firmware.

CMD_READ_RFREG

Read a register on the RF core and return its value.

CMD_SET_RAT_CMP

Set a RAT channel into compare mode and load the comparison register.

CMD_SET_RAT_CPT

Set a RAT channel into capture mode and configure a capture input.

CMD_SET_RAT_OUTPUT

Set the operation mode for a RAT channel output.

CMD_SET_TX_POWER

Update the TX output power to a new value.

CMD_SET_TX20_POWER

Set Transmit Power of the 20-dBm PA.

CMD_TRIGGER

Fire a trigger in a currently running radio operation.

|CMD_MODIFY_FS|

Set new synthesizer frequency without doing a re-calibration.

CMD_UPDATE_RADIO_SETUP

Execute a set of register overrides.

Immediate Commands for Data Queue Manipulation

Command name

Description

CMD_ADD_DATA_ENTRY

Add Data Entry to Queue.

CMD_REMOVE_DATA_ENTRY

Remove First Data Entry From Queue.

CMD_FLUSH_QUEUE

Flush Queue.

CMD_CLEAR_RX

Clear All RX Queue Entries.

CMD_REMOVE_PENDING_ENTRIES

Remove Pending Entries From Queue.

Protocol-Independent Radio Operation Commands

Command name

Description

CMD_NOP

The command only waits for the start trigger, and then ends.

CMD_RADIO_SETUP

Set Up Radio Settings Command.

CMD_FS_POWERUP

Power Up Frequency Synthesizer.

CMD_FS_POWERDOWN

Power Down Frequency Synthesizer.

CMD_FS

Set the synthesizer frequency.

CMD_FS_OFF

Turn Off Frequency Synthesizer.

CMD_RX_TEST

Set the RF core into receive state without using the CPE.

CMD_TX_TEST

Send a modulated or unmodulated test signal.

CMD_SYNC_STOP_RAT

Stop the RAT and save its state.

CMD_SYNC_START_RAT

(Re-)start the RAT and synchronize it to the RTC.

CMD_COUNT

Count the own execution.

CMD_SCH_IMM

Wrap a direct or immediate command in a radio operation.

CMD_COUNT_BRANCH

Branch to alternative commands based on a counter value.

CMD_PATTERN_CHECK

Compare an arbitrary memory location to a given pattern.

Prop Radio Operation Commands

Command name

Description

CMD_PROP_CS

Carrier sense. Monitor the RF activity on a RF channel.

CMD_PROP_RADIO_DIV_SETUP

Setup the RF core into proprietary mode in the Sub-1 GHz band.

CMD_PROP_RADIO_SETUP

Setup the RF core into proprietary mode in the 2.4 GHz band.

CMD_PROP_RESTART_RX

Stop receiving the current packet and go back to sync search.

CMD_PROP_RX

Receive one or multiple packets in proprietary mode (simple format).

CMD_PROP_RX_ADV

Receive one or multiple packets in proprietary mode (advanced format).

CMD_PROP_RX_SNIFF

Do carrier sense and receive one or multiple packets in proprietary mode (simple format).

CMD_PROP_RX_ADV_SNIFF

Do carrier sense and receive one or multiple packets in proprietary mode (advanced format).

CMD_PROP_SET_LEN

Set the length of packet while the packet is being received.

CMD_PROP_TX

Send one packet in proprietary mode (simple format).

CMD_PROP_TX_ADV

Send one packet in proprietary mode (advanced format).

IEEE Radio Operation Commands

Command name

Description

CMD_IEEE_RX

Run receiver.

CMD_IEEE_ED_SCAN

Run energy detect scan.

CMD_IEEE_TX

Transmit packet.

CMD_IEEE_CSMA

Perform CSMA-CA.

CMD_IEEE_RX_ACK

Receive acknowledgment.

CMD_IEEE_ABORT_BG

ABORT background level operation.

CMD_FG_SCH_IMM

Behaves as CMD_SCH_IMM.

CMD_IEEE_MOD_CCA

Modify CCA parameters for running receiver.

CMD_IEEE_MOD_FILT

Modify frame filtering parameters for running receiver.

CMD_IEEE_MOD_SRC_MATCH

Modify source matching parameters for running receiver.

CMD_IEEE_ABORT_FG

ABORT foreground level operation.

CMD_IEEE_STOP_FG

Stop foreground level operation.

CMD_IEEE_CCA_REQ

Request CCA and RSSI information.

High Speed (HS) Radio Operation Commands

Command name

Description

CMD_HS_TX

High-Speed Transmit Command.

CMD_HS_RX

High-Speed Receive Command.