53 #ifndef ti_drivers_ecdsa_ECDSACC26X1__include 54 #define ti_drivers_ecdsa_ECDSACC26X1__include 63 #include <ti/devices/DeviceFamily.h> 64 #include DeviceFamily_constructPath(driverlib/rom_ecc.h) 101 uint32_t eccWorkZone[288];
TI Driver for Elliptic Curve Digital Signature Algorithm.
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:505
ECDSACC26X1 Object.
Definition: ECDSACC26X1.h:97
uint8_t trngIntPriority
TRNG Peripheral's interrupt priority.
Definition: ECDSACC26X1.h:89
TRNG driver implementation for the CC26XX family.
bool isOpen
Definition: ECDSACC26X1.h:98
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSACC26X1.h:99
ECDSACC26X1 Hardware Attributes.
Definition: ECDSACC26X1.h:76
ECC_State eccState
Definition: ECDSACC26X1.h:100