53 #ifndef ti_drivers_ecdh_ECDHCC26X1__include 54 #define ti_drivers_ecdh_ECDHCC26X1__include 61 #include <ti/devices/DeviceFamily.h> 62 #include DeviceFamily_constructPath(driverlib/rom_ecc.h) 96 #define ECDH26X1_ECC_WINDOW_SIZE 3 104 #define ECDH26X1_ECC_WORKZONE_WORDS 198 ECDHCC26X1 Hardware Attributes.
Definition: ECDHCC26X1.h:74
bool isOpen
Definition: ECDHCC26X1.h:112
uint8_t dummy
Definition: ECDHCC26X1.h:75
ECDH_CallbackFxn callbackFxn
Definition: ECDHCC26X1.h:113
ECDHCC26X1 Object.
Definition: ECDHCC26X1.h:111
ECDH_ReturnBehavior returnBehavior
Definition: ECDHCC26X1.h:114
void(* ECDH_CallbackFxn)(ECDH_Handle handle, int_fast16_t returnStatus, ECDH_Operation operation, ECDH_OperationType operationType)
The definition of a callback function used by the ECDH driver when used in ECDH_RETURN_BEHAVIOR_CALLB...
Definition: ECDH.h:655
ECC_State eccState
Definition: ECDHCC26X1.h:115
TI Driver for Elliptic Curve Diffie-Hellman key agreement scheme.
ECDH_ReturnBehavior
The way in which ECDH function calls return after performing a public key generation or shared secret...
Definition: ECDH.h:554
#define ECDH26X1_ECC_WORKZONE_WORDS
Definition: ECDHCC26X1.h:104