Running Software Examples on CC2672X3¶
Porting Software Examples for CC2672X3¶
The CC2672R3 is a SimpleLink™ Multiprotocol 2.4 GHz Wireless MCU with support for Sub-1 GHz IEEE 802.15.4 MAC. It is pin compatible with the CC1352R device. You can run any CC1352R LaunchPad 2.4 GHz software example or binary image on the CC2672R3 device without making any changes.
Note
The also applies to the CC2672P3 in relation to CC1352P device and CC1352P-2 LaunchPad projects
Choosing LaunchPad for Development¶
All CC1352P LaunchPads can be used for software development for the CC2672P3 device. However, the LaunchPads have been designed with different use-cases in mind.
- The CC1352P1 LaunchPad is optimized for transmitting with the high PA on the Sub 1 GHz frequency band and is thus less suitable for CC2672P3 development.
- The CC1352P-4 LaunchPad is optimized to showcase coin cell battery operation while transmitting +10 dBm with the high power PA on the 2.4 GHz frequency band. For more information, see the application note on this topic: Optimizing the CC1352P and CC2652P for Coin Cell Operation at 10 dBm Output Power.
- The CC1352P-2 LaunchPad is optimized to transmit +20 dBm on the 2.4 GHz frequency band.
Moving From LaunchPad to Custom Board¶
You can find instructions on how to design and configure a custom board in the Custom Hardware chapter.