179 #ifndef ti_drivers_watchdog_WatchdogCC26XX__include 180 #define ti_drivers_watchdog_WatchdogCC26XX__include 185 #include <ti/drivers/dpl/HwiP.h> void(* Watchdog_Callback)(uintptr_t handle)
Watchdog callback pointer.
Definition: Watchdog.h:289
unsigned int baseAddr
Definition: WatchdogCC26XX.h:226
Watchdog driver interface.
Watchdog hardware attributes for CC26XX.
Definition: WatchdogCC26XX.h:225
Watchdog_Callback callbackFxn
Definition: WatchdogCC26XX.h:237
bool isOpen
Definition: WatchdogCC26XX.h:236
Watchdog_DebugMode
Watchdog debug stall settings.
Definition: Watchdog.h:264
Watchdog Object for CC26XX.
Definition: WatchdogCC26XX.h:235
unsigned long reloadValue
Definition: WatchdogCC26XX.h:227
Watchdog_ResetMode resetMode
Definition: WatchdogCC26XX.h:239
const Watchdog_FxnTable WatchdogCC26XX_fxnTable
Watchdog function table for CC26XX.
Watchdog_DebugMode debugStallMode
Definition: WatchdogCC26XX.h:241
The definition of a Watchdog function table that contains the required set of functions to control a ...
Definition: Watchdog.h:362
Watchdog_ResetMode
Watchdog reset mode settings.
Definition: Watchdog.h:276
HwiP_Struct hwi
Definition: WatchdogCC26XX.h:244