33 #ifndef ti_display_DisplayDogm1286__include 34 #define ti_display_DisplayDogm1286__include 36 #include <ti/drivers/dpl/SemaphoreP.h> 60 char lcdBuffer0[1024];
72 uint8_t column,
const char *fmt, va_list va);
76 #endif // ti_display_DisplayDogm1286__include uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:584
ADC_Params params
Definition: Driver_Init.h:11
void DisplayDogm1286_close(Display_Handle)
Serial Peripheral Interface (SPI) Driver Interface.
LCD_Buffer used to store data to be printed on the LCD display.
Definition: LCDDogm1286.h:408
void DisplayDogm1286_init(Display_Handle handle)
void DisplayDogm1286_vprintf(Display_Handle handle, uint8_t line, uint8_t column, const char *fmt, va_list va)
struct DisplayDogm1286_HWAttrs DisplayDogm1286_HWAttrs
struct DisplayDogm1286_Object * DisplayDogm1286_Handle
Display_Handle DisplayDogm1286_open(Display_Handle, Display_Params *params)
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
Definition: LCDDogm1286.h:467
Display Parameters.
Definition: Display.h:498
PIN_State pinState
Definition: DisplayDogm1286.h:55
LCD driver implementation for a DOGM128W-6 LCD display.
void DisplayDogm1286_clearLines(Display_Handle handle, uint8_t fromLine, uint8_t toLine)
Generic interface for text output.
Definition: DisplayDogm1286.h:53
The definition of a Display function table that contains the required set of functions to control a s...
Definition: Display.h:557
LCD_Handle lcdHandle
Definition: DisplayDogm1286.h:48
underlying data structure for type PIN_State
Definition: PIN.h:714
SemaphoreP_Struct lcdMutex
Definition: DisplayDogm1286.h:59
LCD_Handle hLcd
Definition: DisplayDogm1286.h:57
const Display_FxnTable DisplayDogm1286_fxnTable
void DisplayDogm1286_clear(Display_Handle handle)
Definition: DisplayDogm1286.h:46
Display Global configuration.
Definition: Display.h:580
int DisplayDogm1286_control(Display_Handle handle, unsigned int cmd, void *arg)
PIN_Id powerPin
Definition: DisplayDogm1286.h:49
Display_LineClearMode lineClearMode
Definition: DisplayDogm1286.h:58
Display_LineClearMode
How to treat existing elements on a line when writing text.
Definition: Display.h:482
struct DisplayDogm1286_Object DisplayDogm1286_Object
PIN_Handle hPins
Definition: DisplayDogm1286.h:56
unsigned int DisplayDogm1286_getType(void)