48 #ifndef ti_sysbios_runtime_SysMin__include 49 #define ti_sysbios_runtime_SysMin__include 59 #define ti_sysbios_runtime_SysMin_long_names 60 #include "SysMin_defs.h" 68 typedef struct SysMin_Module_State SysMin_Module_State;
70 extern char SysMin_outbuf[];
72 struct SysMin_Module_State {
121 extern void SysMin_output(
char *buf,
unsigned int size);
123 extern void SystemSupport_init(
void);
124 extern void SystemSupport_abort(
const char * str);
125 extern void SystemSupport_exit(
int stat);
126 extern void SystemSupport_flush(
void);
127 extern void SystemSupport_putch(
char ch);
128 extern bool SystemSupport_ready(
void);
129 extern void SystemSupport_output(
char *buf,
unsigned int size);
131 extern SysMin_Module_State SysMin_Module_state;
133 #define SysMin_module ((SysMin_Module_State *) &(SysMin_Module_state)) 142 #undef ti_sysbios_runtime_SysMin_long_names 143 #include "SysMin_defs.h" const size_t SysMin_bufSize
Size (in MAUs) of the output.
void(* SysMin_OutputFxn)(char *arg1, unsigned int arg2)
Output characters in the specified buffer.
Definition: SysMin.h:89
const bool SysMin_flushAtExit
Flush the internal buffer during System_exit() or System_abort().