57 #ifndef ti_sysbios_runtime_SysCallback__include 58 #define ti_sysbios_runtime_SysCallback__include 68 #define ti_sysbios_runtime_SysCallback_long_names 69 #include "SysCallback_defs.h" 71 extern void SysCallback_init(
void);
118 #undef ti_sysbios_runtime_SysCallback_long_names 119 #include "SysCallback_defs.h" void SysCallback_defaultPutch(char c)
Default putch function that does nothing.
void SysCallback_defaultExit(int stat)
Default exit function that does nothing.
void SysCallback_defaultAbort(const char *str)
Default abort function that does nothing.
void SysCallback_defaultInit(void)
Default init function that does nothing.
void SysCallback_defaultFlush(void)
Default flush function that does nothing.
bool SysCallback_defaultReady(void)
Default ready function that does nothing.