Flash Vector Table¶
This table contains the first 16 critical interrupt vectors required for the bootup process. The location of this table is controlled by m3Hwi.resetVectorAddress within the RTOS config file (*.cfg), it defaults to address 0x00000000. At bootup time, the RTOS kernel will run a first function to initialize the Hwi module.
For more information on the kernel boot process and first functions, please see the TI-RTOS Kernel Users Guide.
Customer Configuration (CCFG) Table¶
The CCFG is placed at the end of the last flash page and lets customer configure various chip and system parameters in the Customer Configuration (CCFG) table. The CCFG table is defined in ccfg.c in the provided examples. Parameters can be determined in the SysConfig (.syscfg) file through the *TI Devices → Device Configuration options. The last (sizeof(ccfg_t)) bytes of the CCFG sector are reserved by the system for the CCFG table. By default, the linker allocates the unused flash of the last flash page to the application image for code and data use.
See the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual for details on CCFG fields and related configuration options, including how to set the CCFG to disable access to internal flash memory contents.
Note
The CCFG cannot be relocated, and must reside at the end of the last page of flash. Consult the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual for more information.
Note
If SET_CCFG_ERASE_CONF_CHIP_ERASE_DIS_N is set to 0 it’s not possible to do mass erase.
RAM¶
There is 36 kB of RAM available in the CC13xx or CC26xx. The various sections of RAM and their associated linker files are as follows.
- CSTACK: This the system callstack used by the C main function and HWIs. See System Stack for more information
- RAM Reset Vector Table: This table holds entries for all supported reset vectors. It is initialized from the flash reset vector table at boot time and is used to plug interrupt table entries at runtime. See RAM Vector Table for more information.
- HEAP: See Dynamic Memory Allocation for information about heaps.
For projects where the stack project builds a library:
- Application and Stack statically allocated data: This includes any initialized and uninitialized variables used by the application or stack. (.data,.bss)
RAM Vector Table¶
This table is initialized at kernel boot time with the contents of
the flash vector table. The location of this table is controlled by
m3Hwi.vectorTableAddress
within
the RTOS config file (*.cfg), it defaults to address 0x20000000.
The VTOR register will point to this table, which allows the creation of
dynamic interrupts at runtime. This table will contain entries for all 50
supported interrupts.
System Stack¶
As described in Tasks, each task has its own runtime stack for context switching. Another runtime stack is used by the RTOS for main(), HWIs, and SWIs. This system stack is allocated in the application linker file to be placed at the end of the RAM of the application.
For IAR, this RTOS system stack is defined by the CSTACK symbol in the .icf
file:
////////////////////////////////////////////////////////////////////////////////
// Stack
define symbol STACK_SIZE = 0x400;
define symbol STACK_START = RAM_END + 1;
define symbol STACK_END = STACK_START - STACK_SIZE;
//
define symbol STACK_TOP = RAM_END + 1;
export symbol STACK_TOP;
////////////////////////////////////////////////////////////////////////////////
// Memory Placement
////////////////////////////////////////////////////////////////////////////////
//...
// Runtime Stack
define block CSTACK with alignment = 8, size = STACK_SIZE { section .stack };
//...
define block END_OF_RAM with fixed order {
block HEAP_END,
block CSTACK
};
place at end of RAM { block END_OF_RAM };
In IAR, to change the size of the CSTACK, adjust the STACK_SIZE symbol value in the linker configuration file (.icf file) of the application.
For CCS the RTOS system stack is defined by the Program.stack
parameter in
the RTOS configuration file (the .cfg
file):
/* ================ Program configuration ================ */
// ...
Program.stack = 1024;
and placed by the linker in the RAM space of the application (.cmd
file):
/* Create global constant that points to top of stack */
/* CCS: Change stack size under Project Properties */
__STACK_TOP = __stack + __STACK_SIZE;
Dynamic Memory Allocation¶
The system uses a single heap for dynamic memory allocation. This heap is shared between TI-RTOS, the protocol stack, and the application.
The RTOS configuration file that configures the heap depends on the project’s
build configuration. The RTOS configuration file ends with .cfg
, e.g.
ble_release.cfg
.
Using the RTOS configuration file above the heap can be configured in one of three ways. Regardless of the underlying heap implementation, the APIs to access the heap are common.
- TI-RTOS HeapMem - The most flexible heap implementation offered by the TI-RTOS kernel. HeapMem supports creating variable sized blocks as well as freeing blocks. It is implemented by
rtos_heapmem.h
when using RTOS in ROM and by direct calls when using RTOS in flash. See HeapMem with TI-RTOS in ROM for details on using the HeapMem module in ROM with the stack.- TI-RTOS HeapMem with HeapTrack - The most flexible heap implementation offered by the TI-RTOS kernel. HeapMem supports creating variable sized blocks as well as freeing blocks. It is implemented by
rtos_heaptrack.h
when using RTOS in ROM and by direct calls when using RTOS in flash. On top of the functionality offered by HeapMem, HeapTrack offers additional debugging capability, at the cost of runtime performance. See HeapMem with TI-RTOS in ROM for details on using the HeapMem module in ROM with the stack.
Configuring the Heap¶
The active heap configuration is set via the HEAPMGR_CONFIG
variable. If
auto heapsizing is not used, the size of the heap is controlled via
HEAPMGR_SIZE
.The location of both the HEAPMGR_CONFIG
and
HEAPMGR_SIZE
variables are dependent on the project’s current build
configuration. These variables are defined in the app’s .cfg
file.
The system will default to using the OSAL heap with auto heap size. The table
below shows the possible configurations of the heap along with their associated
values of HEAPMGR_CONFIG
and HEAPMGR_SIZE
.
HEAPMGR_CONFIG |
Active Heap Configuration | Heap Size |
0x00 | OSAL HeapMgr, static heap size | Set by HEAPMGR_SIZE |
0x80 | OSAL HeapMgr, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
0x01 | HeapMem, static heap size | Set by HEAPMGR_SIZE |
0x81 | HeapMem, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
0x02 | HeapMem + HeapTrack, static heap size | Set by HEAPMGR_SIZE |
0x82 | HeapMem + HeapTrack, automatic heap size | Automatically determined by the amount of free space available at link time between heapStart and heapEnd symbols |
Warning
If autoheap size is to be used, heapStart
and heapEnd
symbols must
be defined in the linker file. See your application’s map file for the
location of these sections in the StackLibrary configuration.
heapStart
– Placed at end of static allocation sectionheapEnd
– Placed right before beginning of CSTACK section
See the snippet below from the app’s .cfg
to see how to change the
active heap configuration. Change the variable in the highlighted line to one of
the values supported in the table above.
1 2 3 4 var Memory = xdc.useModule('xdc.runtime.Memory'); var HEAPMGR_CONFIG = 0x00; //set to OSAL HeapMgr, static heap size var HEAPMGR_SIZE = 8000; //only valid if static size is used. This is the //size of the buffer allocated for Heap.
Hint
When using static heap size, it’s a good idea to review the heap size thoroughly.