![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.03.00
|
This file contains the host abstraction layer for a RTLS Host.
Go to the source code of this file.
Typedefs | |
typedef void(* | pfnRtlsCtrlProcessMsgCb) (rtlsHostMsg_t *pMsg) |
RTLS Host application callback. | |
Enumerations | |
enum | rtlsHostMsgType_e { HOST_ASYNC_REQ, HOST_ASYNC_RSP, HOST_SYNC_REQ, HOST_SYNC_RSP } |
Enumeration for Host Message types. | |
Functions | |
void | RTLSHost_openHostIf (pfnRtlsCtrlProcessMsgCb rtlsHostMsgCb) |
This function opens the host interface and registers the application callback. More... | |
uint8_t | RTLSHost_sendMsg (uint8_t cmdId, uint8_t cmdType, uint8_t *pData, uint16_t dataLen) |
This function is an abstraction of sending messages to a RTLS Host. More... | |