SimpleLink™ CC13X2 TI 15.4-Stack User's Guide
2.07.00.00
  • Introduction
  • CC13X2 Overview
  • TI-RTOS (RTOS Kernel) Overview
  • TI 15.4-Stack
  • Debugging
  • Over-the-Air Download (OAD)
  • Dynamic Multi-protocol Manager (DMM)
    • Architectural Overview
    • System States and Scheduling Policies
    • RF Command Scheduling
    • System Performance and Limitations
    • Example Applications
    • DMM API reference
  • EnergyTrace User Guide
  • Migration Guide
  • API References
  • References
  • Terms and Acronyms
SimpleLink™ CC13X2 TI 15.4-Stack User's Guide
  • Docs »
  • Dynamic Multi-protocol Manager (DMM)

Dynamic Multi-protocol Manager (DMM)¶

The Dynamic Multi-protocol Manager (DMM) allows multiple wireless stacks to coexist and operate concurrently. It acts as an arbiter between multiple stacks and the shared RF core resource.

Note

Currently the only supported stacks are BLE, TI 15.4 and EasyLink. This chapter will cover the DMM as generally as possible, but when necessary will use the BLE and EasyLink stacks as examples.

  • Architectural Overview
  • System States and Scheduling Policies
    • Creating A Policy Table
    • Choosing A Stack Role
    • Creating a DMM State
    • Initializing the Policy Table
    • Setting the State of the Stack
    • Registering Policy Callbacks
    • Sample Policies
    • BLE Peripheral + WSN Node Sample Policy
    • BLE Peripheral + TI 15.4 Sensor Sample Policy
  • RF Command Scheduling
  • System Performance and Limitations
    • DMM Current Limitations
    • Protocol Stack Limitations
    • Considerations when using Sub-1 GHz SimpleLink Long Range Mode (LRM) PHYs
    • Adjusting the BLE connection interval
  • Example Applications
    • Running the Applications
    • WSN Node + BLE Remote Display Example Application
    • WSN Node + BLE Simple Peripheral Example Application
    • TI 15.4 Sensor + BLE Remote Display Example Application
  • DMM API reference
    • DMM Policy Interface
    • DMM Mode Manager Scheduler
Next Previous

2016-2018, Texas Instruments, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale