Stack Configurations¶
Configuring Bluetooth low energy Protocol Stack Features¶
The Bluetooth low energy protocol stack can be configured to include
or exclude certain Bluetooth Low Energy features by changing the
library configuration in the stack project. The available Bluetooth
low energy features are defined in the build_config.opt file in
the Tools folder of the stack project within the IDE. Based on the
features selected in the build_config.opt file, the lib_search.exe tool
selects the respective precompiled library during the build process of the
stack project.
Note
Selecting the correct stack configuration is essential in optimizing the amount of flash memory available to the application. To conserve memory, exclude certain Bluetooth Low Energy protocol stack features that may not be required.
Run-Time Bluetooth low energy Protocol Stack Configuration¶
The Bluetooth low energy protocol stack can be configured with
various parameters that control its runtime behavior and RF antenna
layout. The available configuration parameters are described in
the ble_user_config.h file in the ICallBLE IDE folder of the
application. During initialization, these parameters are supplied to the
Bluetooth Low Energy protocol stack by the user0Cfg structure, declared in
main.c.
#include "ble_user_config.h"
// BLE user defined configuration
bleUserCfg_t user0Cfg = BLE_USER_CFG;
Because the ble_user_config.h file is shared filed between the Bluetooth
Low Energy projects within the SDK, TI recommends defining configuration
parameters in the .opt files found under TOOLS\defines. The .opt
files contain preprocessor symbols of the application when the default value
isn’t sufficient. For example, to change the maximum PDU size from the default
27 to 162, set the preprocessor symbol MAX_PDU_SIZE=162 in the
preprocessor symbols for the application project. Increasing certain
parameters may increase heap memory use by the protocol stack;
adjust the HEAPMGR_SIZE as required (if not using auto sized heap).
Table 10. and Table 10.
list the available configuration parameters.
| Configurable? | Define | Description |
|---|---|---|
| Y | BOARD_DISPLAY_USE_LCD | 0 or 1 determines if the Display driver should use LCD |
| Y | BOARD_DISPLAY_USE_UART | 0 or 1 determines if the Display driver should use UART |
| Y | BOARD_DISPLAY_USE_UART_ANSI | 0 or 1 determines if the Display driver should use UART ANSI |
| N | CC26X2 | This selects the chipset |
| Y | CC26X2R1_LAUNCHXL | This define may be changed when migrating to a custom development board |
| N | CC26XX | This selects the chipset |
| N | DeviceFamily_CC26X2 | This selects the chipset |
| Y | Display_DISABLE_ALL | If set, the Display module will be disabled. |
| Y | EXT_HAL_ASSERT | Defining this assert will forward ble5stack asserts to the application |
| Y | HEAPMGR_METRICS | Defining this will enable heap profiling. |
| N | ICALL_EVENTS | This define is used with ICALL - do not modify |
| N | ICALL_JT | This define is used with ICALL - do not modify |
| N | ICALL_LITE | This define is used with ICALL - do not modify |
| Y | ICALL_MAX_NUM_ENTITIES | This Maximum number of entities that use ICall, including service entities and application entities. |
| Y | ICALL_MAX_NUM_TASKS | Defines the max number of ICall enabled tasks. Must be the same as OSAL_MAX_NUM_PROXY_TASKS. Default is 2. |
| Y | L2CAP_NUM_CO_CHANNELS | Maximum number of L2CAP Connection-Oriented (CO) Channels. Default is 3. |
| Y | L2CAP_NUM_PSM | Maximum number of L2CAP Protocol/Service Multiplexers (PSM). Default is 3. |
| Y | MAX_NUM_BLE_CONNS | This is the maximum number of simultaneous Bluetooth low energy collections allowed. Adding more connections uses more RAM and may require increasing HEAPMGR_SIZE. Profile heap usage accordingly |
| Y | MAX_NUM_PDU | Maximum number of Bluetooth low energy HCI PDUs. Default is 5. If the maximum number of connections is set to 0, then this number should also be set to 0. |
| Y | MAX_PDU_SIZE | Maximum size in bytes of the Bluetooth low energy HCI PDU. Default is 27. Valid range is 27 to 255. The maximum ATT_MTU is MAX_PDU_SIZE - 4. See Configuring for Larger MTU Values. |
| Y | NPI_SPI_CONFIG | When NPI_USE_API is defined, this will allows you to choose which SPI driver instance NPI will be used. |
| Y | NPI_USE_SPI | Configure NPI to use SPI. Do not define NPI_USE_UART and NPI_USE_SPI at the same time. |
| Y | NPI_USE_UART | Configure NPI to use UART. Do not define NPI_USE_SPI and NPI_USE_UART at the same time. |
| Y | PM_STARTUP_MARGIN | Defines time in microseconds (us) the system will wake up before the start of the connection event. Default is 300. This value is optimized for the example projects. |
| Y | POWER_SAVING | Power management is enabled when defined, and disabled when not defined. Requires same option in stack project |
| N | STACK_LIBRARY | Build/Use the build configuration where the stack is built as a library |
| Y | TBM_ACTIVE_ITEMS_ONLY | When using the Two Button Menu, Only active items will be displayed |
| N | USE_ICALL | This define is used with ICALL - do not modify |
| Configurable? | Define | Description |
|---|---|---|
| N | CC26X2 | This selects the chipset |
| N | CC26XX | This selects the chipset |
| N | DeviceFamily_CC26X2 | This selects the chipset |
| Y | EXT_HAL_ASSERT | Defining this assert will forward ble5stack asserts to the application |
| Y | FLASH_ROM_BUILD | Setting this option will use the ble5stack with ROM APIs - decreasing flash footprint |
| N | ICALL_EVENTS | This define is used with ICALL - do not modify |
| N | ICALL_JT | This define is used with ICALL - do not modify |
| N | ICALL_LITE | This define is used with ICALL - do not modify |
| Y | OSAL_CBTIMER_NUM_TASKS | Defines the number of osal callback tasks. Each osal callback task can contain up to 16 osal callback functions. Default is 1. |
| Y | OSAL_MAX_NUM_PROXY_TASKS | Defines the max number of ICall enabled tasks. Must be the same as ICALL_MAX_NUM_TASKS. Default is 2. |
| Y | OSAL_SNV | Define the number of non-volatile flash pages are to be used with the Simple Non-Volatile module. Default is 2. |
| Y | POWER_SAVING | Power management is enabled when defined, and disabled when not defined. Requires same option in stack project |
| Y | RF_FE_MODE_AND_BIAS | Defines the RF antenna front end and bias configuration. Set this value to match the actual hardware antenna layout. This value can be set directly, or through Board.h. |
| Y | SC_HOST_DEBUG | Defining this will allow you to capture over-the-air bluetooth low energy traffic that use LE Secure Connections. |
| N | STACK_LIBRARY | Build/Use the build configuration where the stack is built as a library |
| N | USE_ICALL | This define is used with ICALL - do not modify |