Creating a Production Image

A production image is an image that is ready for flashing at the factory, and to be released in a commercial OAD enabled product.

Change to Release BIM

By default, the projects in the SimpleLink CC13x2 SDK will use a debug version of the BIM. This is helpful for evaluation of the TI OAD solution, but is not recommended for a production OAD build for the following reasons:

  • The debug configuration of BIM will not check the CRC of the image before booting. This removes a layer of redundancy in the system in favor of allowing the develop to load an OAD image straight from the IDE

In order to change the release version, removing the following defines which may be used for debugging:

  • JTAG_DEBUG
  • NO_COPY

Additionally, it may be desirable to remove the secondary device trim in the application for production images. See Device trim for more information.

Secure OAD: Change default keys

If you are using the secure version of OAD, new OAD keys should be generated and stored on the device. It is a security risk to use the placeholder keys that are provided with TI as these are publically available.

See Generating new security keys for more information on how to generate and install new keys on the device. If using unsecure OAD, this step is not necessary.

Loading a Production Image

Production images should use both the release configuration of BIM as discussed above. As mentioned above, the release configuration of the BIM will check for a valid CRC and signature. Images loaded straight from the IDE will not have a valid CRC or signature. However, the oad_image_tool will add the CRC and signature automatically at the completion of each build. Refer to Figure 65. for a diagram of the build process.

Before loading the application, be sure to load the release BIM project. This can be flash via the BIM’s hex file in UNIFLASH.

Warning

If flashing the BIM image (or a merged image containing BIM) using uniflash, be sure that the Keep CCFG data box is not checked. (Settings & Utilities –> Download). BIM will use a custom CCFG, so it is important that any existing image on the device is removed. Another safeguard is the mass erase the device before starting with OAD.

In release configurations, it is necessary to load the device using the *_oad.bin application file that is output by the oad_image_tool using UNIFLASH.

  • The binary from the tool will be placed in the build folder alongside the default .out file.

The address offset should be 0x0000000 as shown in the screen capture below

../_images/uniflash_load_production_image1.png

Note the following error is benign and can be ignored for OAD images. Verify the device has booted correctly by verifying the terminal output.

../_images/uniflash_benign_error_oad1.png