0.01.00
Network Interfaces

This module includes definitions for IPv6 network interfaces. More...

Classes

class  ot::Ip6::LinkAddress
 This class represents an IPv6 Link Address. More...
 
class  ot::Ip6::NetifUnicastAddress
 This class implements an IPv6 network interface unicast address. More...
 
class  ot::Ip6::NetifMulticastAddress
 This class implements an IPv6 network interface multicast address. More...
 
class  ot::Ip6::Netif
 This class implements an IPv6 network interface. More...
 

Detailed Description

This module includes definitions for IPv6 network interfaces.