rfSynchronizedPacketRx Example
Example Summary
In this example you will learn how to build a time-synchronized connection between one transmitter and a receiver. Time-synchronization enables both communication partners to transfer data quickly at predictable time points. Unlike the wake-on-radio example, the transmitter does not need to send a very long preamble and the receiver does not need to wait and check for a signal on air. This leads to the lowest possible power consumption on both sides. It also fits very well to the SimpleLink Long-range mode. Time synchronization builds also the foundation for Frequency and Time Division Multiple Access, FDMA and TDMA respectively.
This example project shows the receiver part. The transmission part can be found in the Synchronized Packet TX example.
Peripherals Exercised
Board_BUTTON1- Toggles between periodic and spontaneous beacon mode.Board_LED1- Reflects the status ofBoard_LED1on the transmitter.Board_LED2- On while the receiver is enabled (LNA enable), off when in standby.
Resources & Jumper Settings
This section explains the resource mapping across various boards. If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
SmartRF06 in combination with one of the CC13x0 evaluation modules
| Resource | Mapping / Notes |
|---|---|
BUTTON1 |
BTN_UP (up button) |
BUTTON1 |
BTN_DN (down button) |
LED1 |
LED1 |
LED2 |
LED2 |
CC1310 / CC1350 / CC2640R2 Launchpad
| Resource | Mapping / Notes |
|---|---|
BUTTON1 |
BTN-1 (left button) |
BUTTON2 |
BTN_2 (right button) |
LED1 |
Green LED |
LED2 |
Red LED |
Board Specific Settings
- The default frequency is:
- 433.92 MHz for the CC1350-LAUNCHXL-433
- 433.92 MHz for the CC1352P-4-LAUNCHXL
- 2440 MHz on the CC2640R2-LAUNXHL
- 868.0 MHz for other launchpads In order to change frequency, modify the smartrf_settings.c file. This can be done using the code export feature in Smart RF Studio, or directly in the file
- On the CC1352P1 the high PA is enabled (high output power) for all Sub-1 GHz modes by default. The user must set USE_SUB1_HIGH_PA_SETTING to 0 in smartrf_settings.h and smartrf_settings_predefined.h, and rebuild the example, to disable the high PA and use the default PA
- On the CC1352P-2 the high PA operation for Sub-1 GHz modes is not supported
- On the CC1352P-4 the default PA is used for all Sub-1 GHz physical modes by default. The user must set USE_SUB1_HIGH_PA_SETTING to 1 in the smartrf_settings.h and smartrf_settings_predefined.h, and rebuild the example, to enable the high PA (high output power) CAUTION
- This will change the center frequency for 2-GFSK to 490 MHz
- The center frequency for SimpleLink long range (SLR) stays at 433.92 MHz, but the high output power violates the maximum power output requirement for this band
- This will change the center frequency for 2-GFSK to 490 MHz
- The CC2640R2 is setup to run all proprietary physical modes at a center frequency of 2440 MHz, at a data rate of 250 Kbps
Example Usage
This section is similar for both TX and RX. You need 2 boards: one running the rfSynchronizedPacketTx application (TX board) and another one running the rfSynchronizedPacketRx application (RX board).
Initial synchronization
Build and run the
rfSynchronizedPacketRxexample on the RX board. You will seeLED2on the RX board being on all the time.Build and run the
rfSynchronizedPacketTxexample on the TX board. You will seeLED2on the TX board flashing with a period of 500 ms. On the RX board, you will see thatLED2is flashing synchronously.Push
BUTTON1on the TX board.LED1will toggle immediately. On the RX board,LED1follows after a short delay.You may push
BUTTON1several times and will see thatLED1on the RX board will always reflect the state on the TX board with some delay.
Explanation: After starting, the RX board goes into WaitingForSync state. The receiver is switched on end waits for a packet. The LNA signal (LED2) is enabled to reflect the current receiver state.
When the application on the TX board is started, it starts to send periodic beacon messages. Once the RX board has received the first beacon message, it switches the receiver off and goes into SyncedRx state. In this state, it wakes up the receiver right before the next packet from the TX board is expected.
When BUTTON1 on the TX board is pushed, the current LED state is sent in the next available time slot and is shown on the RX board as soon as the packet has arrived.
Sending spontaneous messages after synchronization
Push
BUTTON2on the TX board. You will see thatLED2on the TX board stops flashing whileLED2on the RX boards remains flashing.Push
BUTTON1on the TX board. You will see thatLED1toggles on the TX board and with a short delay also on the RX board.LED2on the TX board will flash a short while after pushing the button.
Explanation: After pushing BUTTON2 on the TX board, the TX application goes into SporadicMessage state and stops sending periodic beacons. The RX application remains in SyncedRx state and wakes up when it expects a packet. As long as no button on the TX board is pushed, the RX board will wake up only for a short time and go back to standby after a very short timeout because no packet is received.
When pushing BUTTON1 on the TX board, a packet with the new state of LED1 is transmitted. The TX board sends exactly at the same time when the RX board expects to receive a packet. The RX board receives the message and updates the state of its own LED1.
Error handling: Resynchronization due to crystal drift
Repeat step 6 for a while. After a couple of minutes, you will notice that
LED1on the RX board is not updated properly anymore.Push
BUTTON1on the RX board.LED2will remain on permanently.Push
BUTTON1on the TX board. You will seeLED1toggle on both boards andLED2on the RX board starting to flash again.
Explanation: Both TX and RX board predict the following wake-up events based on the time when synchronization happened. If both clocks have a small drift, then the wake-up time will be incorrect after some time.
By pushing BUTTON1 on the RX board, the application goes back into WaitingForSync state and re-synchronizes to the TX board.
Application Design Details
This examples consists of a single task and the exported SmartRF Studio radio settings. The RX application is implemented as a state machine with 3 states:
In order to send synchronous packets, the receiver uses absolute start triggers. Absolute start triggers are explained in the proprietary RF user’s guide and the technical reference manual.
In WaitingForSync state, the receiver waits an infinite time in RX state. That means, the power consumption is high. As soon as it receives a beacon packet from the transmitter and the packet is valid, it uses the RX time stamp as an anchor time:
/* rxTime contains a calculated time stamp when the first preamble byte
* was sent on air. As a time base for the next wake ups, we calculate
* the time when this RX command would have been started for a synchronised
* wake up. */
RF_cmdPropRx.startTime = rxTime - RX_START_TO_SETTLE_TICKS - RX_START_MARGIN;The RX time stamp is the time when the first preamble bit was on air. The RF core calculates this time based on the internal “sync word found” signal and the RF settings provided in the SETUP command. The RX_START_TO_SETTLE_TICKS needs to be subtracted because it takes some time between command start and the receiver being ready to receive. In addition, RX_START_MARGIN is subtracted to start the RX operation a bit earlier. This is necessary to compensate possible crystal drifts.
Finally, the application goes into the SyncedRx state where it calculates the time for the next RX start based on the latest received packet:
/* Start RX command to receive a single packet. Use an absolute start trigger
* and a predicted start time. The end time is calculated to be as tight as possible.
* The compensation margin for RAT drift in both directions needs to be taken into account. */
RF_cmdPropRx.startTrigger.triggerType = TRIG_ABSTIME;
RF_cmdPropRx.startTime += beacon.beaconInterval;
RF_cmdPropRx.endTrigger.triggerType = TRIG_REL_START;
RF_cmdPropRx.endTime = RX_START_TO_SETTLE_TICKS + RX_TIMEOUT_TICKS + RX_TIMEOUT_MARGIN + RX_START_MARGIN;The RF driver takes care that the RF core is powered up and running before the start trigger is due. For the end trigger, we use a time relative to the command start. That means, the timeout is determined by:
- the time needed for transmitting a whole preamble and sync word,
- the margin subtracted from the start trigger,
- an additional timeout margin to compensate possible errors in the calculation