Terms and acronyms

General Terms and Acronyms

CCA
CCFG
Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
CCS
Code Composer Studio
IAR
IAR Systems
MCU
Microcontroller Unit
OAD
Over the Air Download
ROM
Read-only Memory
SNV
Simple Non-Volatile storage

RF Core Terms and Acronyms

CPE
Command and Packet Engine
The unit on the RF core that is responsible for command execution and packet encoding/decoding. It acts as a supervisor for all other sub-modules during command execution.
MCE
Modem Control Engine
A functional unit on the RF core that sits in between the CPE and the RFE. It is responsible for signal modulation/demodulation and binary base band processing.
RAT
Radio Timer
A functional unit on the RF core that provides accurate timing for command execution. It runs with 1/4 speed of the high- frequency oscillator.
RFE
Radio Front-end Engine
A functional unit on the RF core that is responsible for the analog signal processing part. It connects the MCE to the antenna.
IB
Current Bias
One of several parameters for adjusting output power during packet transmissions. ‘I’ in ‘IB’ stands for the SI unit for current.
PA
Power Amplifier
A RF power amplifier converts a low-power RF signal into a higher power signal. Typically, RF power amplifiers drive the antenna of a transmitter.
genfsk
Used as an abbreviation for settings that uses the patch rf_patch_cpe_genfsk. genfsk supports up to 500 kbps FSK and GFSK.
SLR
RF mode designed to giv a long range. The data rate is 5 kbps.

Over the Air Download (OAD) Terms and Acronyms

BIM
Boot Image Manager
A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
Factory Image
The factory image is a “golden” image that resides in external flash as a failsafe mechanism.
OAD
Over the Air Download
The process of performing a device firmware update over the air.
OAD Target
The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx device running the TI protocol specific transport for OAD.
OAD Distributor
The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.

Dynamic Multi-protocol Manager Terms and Acronyms

Dynamic Multi-protocol Manager
DMM
An arbiter between multiple protocol stacks that are sharing the multi mode RF driver and thus the radio. The DMM aides in scheduling radio operations by way of application provided state information and timing constraints.