Overview

TI’s royalty-free TI 15.4-Stack is a complete software platform for developing applications that require extremely low-power, long-range, reliable, robust and secure wireless star-topology based networking solutions. This chapter explains in detail the different network-configuration modes supported by the TI 15.4-Stack for application development. Useful information is presented for developers using the TI 15.4-Stack for their custom application development, which lets developers quickly understand the basics of the selected configuration mode and develop their end products with ease.

Architecture Choices

TI 15.4-Stack can be used in two separate architectures based on the end product application. Figure 19. shows the two different system architectures enabled by TI 15.4-Stack.

  • A single device is shown in Figure 19. (left). The application and protocol stack are both implemented on the CC13x2 or CC26x2 as a true single-chip solution. This configuration is the simplest and most common when using the CC13x2 or CC26x2 for network nodes and also using the CC13x2 or CC26x2 as a personal area network (PAN) coordinator node. This configuration is the most cost-effective technique and provides the lowest- power performance.
  • A coprocessor is shown in Figure 19. (right). The protocol stack runs on the CC13x2 or CC26x2 while the application is executed on an external MPU or MCU. The application interfaces with the CC13x2 or CC26x2 using the network protocol interface (NPI) over a serial universal asynchronous receiver/transmitter (UART) connection. The description of the API interface is provided in the TI 15.4-Stack CoP Interface Guide document found in the docs/ti154stack folder of the SDK installation directory. This configuration is useful for applications that must add long-range wireless connectivity or peripheral applications, which execute on another device (such as an external MCU) or on a PC without the requirement to implement the complexities associated with a wireless networking protocol. In these cases, the application can be developed externally on a host processor while running TI 15.4-Stack on the CC13x2 or CC26x2, which provides ease of development and quickly adds long-range wireless connectivity to existing products.
../_images/fig-device-configuration.png

Figure 19. Single Device and Coprocessor Configuration

Data-Rate and PHY

The choice of PHY band and data rate can be made by setting the appropriate PHY Id in ApiMac_attribute_phyCurrentDescriptorId PIB attribute. The overall options are explained in Table 1.

Attention

When operating TI 15.4-Stack at 2.4 GHz (PHY ID 0) the data-rate is locked at the standard IEEE 802.15.4 data-rate of 250kbps. Channel count starts at channel 11 for this PHY.

Table 1. TI 15.4-Stack PHY’s and their channel frequencies
PHY ID PHY Data Rate Channel 0 Freq # of Channels Channel Spacing
0 250 kbps 2405 MHz (ch11) 16 5 MHz
1 50 kbps 902.2 MHz 129 200 KHz
3 50 kbps 863.125 MHz 64 200 KHz
128 50 kbps 433.05 MHz 7 200 KHz
129 5 kbps 902.2 MHz 129 200 KHz
130 5 kbps 433.05 MHz 7 200 KHz
131 5 kbps 863.125 MHz 64 200 KHz
132 200 kbps 902.4 MHz 64 400 KHz
133 200 kbps 863.225 MHz 32 400 KHz