RF commands reference¶
Please find a detailed description for each command in the Radio chapter of the CC13x2 CC26x2 SimpleLink Wireless MCU Technical Reference Manual.
Direct commands¶
Command name | Description |
---|---|
CMD_ABORT | Abort a running radio operation command immediately. |
CMD_GET_RSSI | Read the current RSSI while an RX command is running. |
CMD_PING | Respond with an interrupt event. |
CMD_START_RAT | Start the RAT without synchronization to the RTC. |
CMD_STOP | Abort a running radio operation command at the next possibility. |
Immediate commands¶
Command name | Description |
---|---|
CMD_ARM_RAT_CH | Enable counting for a given RAT channel. |
CMD_BUS_REQUEST | Set or reset a dependency on the system bus. |
CMD_DISARM_RAT_CH | Disable counting for a given RAT channel. |
CMD_GET_FW_INFO | Request information about the RF core firmware. |
CMD_READ_RFREG | Read a register on the RF core and return its value. |
CMD_SET_RAT_CMP | Set a RAT channel into compare mode and load the comparison register. |
CMD_SET_RAT_CPT | Set a RAT channel into capture mode and configure a capture input. |
CMD_SET_RAT_OUTPUT | Set the operation mode for a RAT channel output. |
CMD_SET_TX_POWER | Update the TX output power to a new value. |
CMD_TRIGGER | Fire a trigger in a currently running radio operation. |
CMD_UPDATE_FS | Set new synthesizer frequency without doing a re-calibration. |
CMD_UPDATE_RADIO_SETUP | Execute a set of register overrides. |
Radio operation commands¶
Command name | Description |
---|---|
CMD_COUNT_BRANCH | Branch to alternative commands based on a counter value. |
CMD_COUNTER | Count the own execution. |
CMD_FS | Set the synthesizer frequency. |
CMD_PATTERN_CHECK | Compare an arbitrary memory location to a given pattern. |
CMD_PROP_CS | Carrier sense. Monitor the RF activity on a RF channel. |
CMD_PROP_RADIO_DIV_SETUP | Setup the RF core into proprietary mode in the Sub-1 GHz band. |
CMD_PROP_RADIO_SETUP | Setup the RF core into proprietary mode in the 2.4 GHz band. |
CMD_PROP_RESTART_RX | Stop receiving the current packet and go back to sync search. |
CMD_PROP_RX | Receive one or multiple packets in proprietary mode (simple format). |
CMD_PROP_RX_ADV | Receive one or multiple packets in proprietary mode (advanced format). |
CMD_PROP_RX_SNIFF | Do carrier sense and receive one or multiple packets in proprietary mode (simple format). |
CMD_PROP_RX_ADV_SNIFF | Do carrier sense and receive one or multiple packets in proprietary mode (advanced format). |
CMD_PROP_SET_LEN | Set the length of packet while the packet is being received. |
CMD_PROP_TX | Send one packet in proprietary mode (simple format). |
CMD_PROP_TX_ADV | Send one packet in proprietary mode (advanced format). |
CMD_RX_TEST | Set the RF core into receive state without using the CPE. |
CMD_SCH_IMM | Wrap a direct or immediate command in a radio operation. |
CMD_SYNC_START_RAT | (Re-)start the RAT and synchronize it to the RTC. |
CMD_SYNC_STOP_RAT | Stop the RAT and save its state. |
CMD_TX_TEST | Send a modulated or unmodulated test signal. |