40 #ifndef ti_drivers_UART2Support__include 41 #define ti_drivers_UART2Support__include 161 size_t size, uint8_t *buf);
UART2 Global configuration.
Definition: UART2.h:697
void UART2Support_dmaRefreshRx(UART2_Handle handle)
Function to update RX ring buffer state.
int UART2Support_uartRxError(UART2_HWAttrs const *hwAttrs)
Function to clear receive errors.
void UART2Support_dmaStopTx(UART2_Handle handle)
Function to disable the TX DMA.
bool UART2Support_txDone(UART2_HWAttrs const *hwAttrs)
Function to determine if TX is in progress.
PRELIMINARY UART driver interface
void UART2Support_dmaStopRx(UART2_Handle handle)
Function to disable the RX DMA.
void UART2Support_enableInts(UART2_Handle handle)
Function to enable receive, receive timeout, and error interrupts.
void UART2Support_powerSetConstraint(void)
Function to set power constraint.
void UART2Support_powerRelConstraint(void)
Function to release power constraint.
void UART2Support_enableTx(UART2_HWAttrs const *hwAttrs)
Function to enable the transmit interrupt.
void UART2Support_dmaStartRx(UART2_Handle handle)
Function to configure the receive DMA.
void UART2Support_enableRx(UART2_HWAttrs const *hwAttrs)
Function to enable the receive.
uint32_t UART2Support_sendData(UART2_HWAttrs const *hwAttrs, size_t size, uint8_t *buf)
Function to send data.
void UART2Support_dmaStartTx(UART2_Handle handle)
Function to configure the tramsit DMA.
void UART2Support_disableTx(UART2_HWAttrs const *hwAttrs)
Function to disable the transmit interrupt.
int_fast16_t UART2Support_rxStatus2ErrorCode(uint32_t errorData)
Function to convert RX error status to a UART2 error code.
void UART2Support_disableRx(UART2_HWAttrs const *hwAttrs)
Function to disable the receive and receive interrupts.