![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.02.00
|
This file contains the RTLS Control API's.
Go to the source code of this file.
Data Structures | |
struct | rtlsConfiguration_t |
RTLS Configuration structure. More... | |
struct | rtlsCtrlReq_t |
RTLS Control request. More... | |
struct | rtlsEnableSync_t |
RTLS Enable Sync - This will tell the RTLS Application to start notifying RTLS Control about a specific connection. More... | |
struct | rtlsGetActiveConnInfo_t |
RTLS Get Active Connection Info - get the connection information for a specific handle. More... | |
struct | rtlsPacket_t |
RTLS Packet - Generic structure that will be translated to a specific command. More... | |
struct | rtlsTerminateLinkReq_t |
RTLS terminate link request. More... | |
struct | rtlsUpdateConnIntReq_t |
RTLS update connection interval request. More... | |
Macros | |
#define | CHIP_ID_ADDR ((uint8_t *)(0x50001000 + 0x2E8)) |
Chip Identifier Address. | |
#define | CHIP_ID_SIZE 6 |
Chip Identifier Size. | |
#define | RTLS_CONNHANDLE_ALL 0xFFFD |
#define | RTLS_CONNHANDLE_INVALID 0xFFFF |
#define | RTLS_CTRL_ASSERT_CAUSE_INVALID_PARAM 0x02 |
RTLS Assert Error code. | |
#define | RTLS_CTRL_ASSERT_CAUSE_NULL_POINTER_EXCEPT 0x03 |
RTLS Assert Error code. | |
#define | RTLS_CTRL_ASSERT_CAUSE_OUT_OF_MEMORY 0x01 |
RTLS Assert Error code. | |
#define | RTLS_CTRL_REV 0x2 |
#define | RTLS_FALSE 0 |
FALSE. | |
#define | RTLS_REQ_ADD_DEVICE_ADV_LIST 0x0E |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_AOA_ENABLE 0x07 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_BLE_LOG_STRINGS_MAX 0x9 |
#define | RTLS_REQ_CL_AOA_ENABLE 0x12 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_CLEAR_ADV_LIST 0x11 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_CONN 0x02 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_CREATE_SYNC_CANCEL 0x0B |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_ENABLE_SYNC 0x01 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_GET_ACTIVE_CONN_INFO 0x09 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_PERIODIC_RECEIVE_ENABLE 0x0D |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_READ_ADV_LIST_SIZE 0x10 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_REMOVE_DEVICE_ADV_LIST 0x0F |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SCAN 0x03 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SEND_DATA 0x04 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SET_AOA_PARAMS 0x06 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SET_CREATE_SYNC_PARAMS 0x0A |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_TERMINATE_LINK 0x05 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_TERMINATE_SYNC 0x0C |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_UPDATE_CONN_INTERVAL 0x08 |
RTLS Application Command Opcode. | |
#define | RTLS_TRUE 1 |
TRUE. | |
Typedefs | |
typedef void(* | pfnRtlsAppCb) (uint8_t *cmd) |
Application callback function. | |
Enumerations | |
enum | rtlsCapabilities_e { RTLS_CAP_NOT_INITIALIZED = 0x00000000, RTLS_CAP_CM = 0x00000001, RTLS_CAP_AOA_TX = 0x00000002, RTLS_CAP_AOA_RX = 0x00000004, RTLS_CAP_RESERVED1 = 0x00000008, RTLS_CAP_CL_AOA = 0x00000010, RTLS_CAP_RESERVED3 = 0x00000020, RTLS_CAP_RTLS_RESPONDER = 0x00000040, RTLS_CAP_RTLS_COORDINATOR = 0x00000080, RTLS_CAP_RTLS_PASSIVE = 0x00000100 } |
Enumeration for RTLS Capabilities. | |
enum | rtlsStatus_e { RTLS_SUCCESS, RTLS_FAIL, RTLS_LINK_ESTAB_FAIL, RTLS_LINK_TERMINATED, RTLS_OUT_OF_MEMORY, RTLS_CONFIG_NOT_SUPPORTED, RTLS_ILLEGAL_CMD } |
Enumeration for RTLS Status. | |
Functions | |
void | AssertHandler (uint8 assertCause, uint8 assertSubcause) |
void | RTLSCtrl_aoaResultEvt (uint16_t handle, int8_t rssi, uint8_t channel, uint16_t numIqSamples, uint8_t sampleRate, uint8_t sampleSize, uint8_t sampleCtrl, uint8_t slotDuration, uint8_t numAnt, int8_t *pIQ) |
RTLSCtrl_aoaResultEvt. More... | |
void | RTLSCtrl_connInfoEvt (uint8_t *connInfo, uint16_t connInfoLen) |
RTLSCtrl_connInfoEvt. More... | |
void | RTLSCtrl_connResultEvt (uint16_t connHandle, uint8_t status) |
RTLSCtrl_connResultEvt. More... | |
void | RTLSCtrl_dataSentEvt (uint16_t connHandle, uint8_t status) |
RTLSCtrl_dataSentEvt. More... | |
void | RTLSCtrl_open (rtlsConfiguration_t *rtlsConfig) |
RTLSCtrl_open. More... | |
void | RTLSCtrl_processClAoaEnableEvt (uint16_t opcode, uint8_t status, uint16_t syncHandle) |
void | RTLSCTRL_processPeriodicAdvReport (uint8_t opcode, uint16_t syncHandle, int8_t txPower, int8_t rssi, uint8_t cteType, uint8_t dataStatus, uint8_t dataLen, uint8_t *pData) |
void | RTLSCtrl_processSyncEstEvt (uint8_t opcode, uint8_t status, uint16_t syncHandle, uint8_t advSid, uint8_t advAddrType, uint8_t advAddress[6], uint8_t advPhy, uint16_t periodicAdvInt, uint8_t advClockAccuracy) |
RTLSCtrl_processSyncEstEvt. More... | |
void | RTLSCtrl_processSyncLostEvt (uint8_t opcode, uint16_t syncHandle) |
void | RTLSCtrl_processTerminateSyncEvt (void) |
void | RTLSCtrl_rtlsPacketEvt (uint8_t *pPkt) |
RTLSCtrl_rtlsPacketEvt. More... | |
void | RTLSCtrl_scanResultEvt (rtlsStatus_e status, uint8_t *scanResult, uint8_t size) |
RTLSCtrl_scanResultEvt. More... | |
void | RTLSCtrl_sendDebugEvt (uint8_t *debug_string, uint32_t debug_value) |
RTLSCtrl_sendDebugEvt. More... | |
void | RTLSCtrl_sendPeriodicListSize (uint8_t *pEvt) |
RTLSCtrl_sendPeriodicListSize. More... | |
void | RTLSCtrl_syncNotifyEvt (uint16_t connHandle, rtlsStatus_e status, uint32_t timeToNextEvent, int8_t rssi, uint8_t channel) |
RTLSCtrl_syncNotifyEvt. More... | |
Variables | |
char * | rtlsReq_BleLogStrings [] |