![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.02.00
|
Modules | |
HCI Constants | |
HCI Event API Parameters | |
RF Setup PHY Parameters | |
Files | |
file | hci.h |
HCI layer interface. | |
HCI Function Mapping
This section lists the mapping between stack APIs and function names, as described in the BT core spec for commands that the application can call and receive a \ corresponding event. no.
Stack API | BT Function |
---|---|
HCI_HostNumCompletedPktCmd | Host Number Of Completed Packets Command |
HCI_LE_AddDeviceToResolvingListCmd | LE Add Device to Resolving List Command |
HCI_LE_AddWhiteListCmd | LE Add Device To White List Command |
HCI_LE_ClearWhiteListCmd | LE Clear White List Command |
HCI_LE_EncryptCmd | LE Encrypt Command |
HCI_LE_RandCmd | LE Rand Command |
HCI_LE_ReadBufSizeCmd | LE Read Buffer Size Command |
HCI_LE_ReadChannelMapCmd | LE Read Channel Map Command |
HCI_LE_ReadLocalResolvableAddressCmd | LE Read Local Resolvable Address Command |
HCI_LE_ReadLocalSupportedFeaturesCmd | Read Local Supported Commands Command |
HCI_LE_ReadMaxDataLenCmd | LE Read Maximum Data Length Command |
HCI_LE_ReadPeerResolvableAddressCmd | LE Read Peer Resolvable Address Command |
HCI_LE_ReadResolvingListSizeCmd | LE Read Resolving List Size Command |
HCI_LE_ReadSuggestedDefaultDataLenCmd | LE Read Suggested Default Data Length Command |
HCI_LE_ReadSupportedStatesCmd | LE Read Supported States Command |
HCI_LE_ReadWhiteListSizeCmd | LE Read White List Size Command |
HCI_LE_RemoveDeviceFromResolvingListCmd | LE Remove Device From Resolving List Command |
HCI_LE_RemoveWhiteListCmd | LE Remove Device From White List Command |
HCI_LE_SetDataLenCmd | LE Set Data Length Command |
HCI_LE_SetEventMaskCmd | LE Set Event Mask Command |
HCI_LE_SetHostChanClassificationCmd | LE Set Host Channel Classification Command |
HCI_LE_SetResolvablePrivateAddressTimeoutCmd | LE Set Resolvable Private Address Timeout Command |
HCI_LE_SetPrivacyModeCmd | LE Set Privacy Mode Command |
HCI_LE_TestEndCmd | LE Test End Command |
HCI_LE_TransmitterTestCmd | LE Transmitter Test Command |
HCI_LE_WriteSuggestedDefaultDataLenCmd | LE Write Suggested Default Data Length Command |
HCI_ReadAuthPayloadTimeoutCmd | Read Authenticated Payload Timeout Command |
HCI_ReadBDADDRCmd | Read BD_ADDR Command |
HCI_ReadLocalSupportedCommandsCmd | Read Local Supported Commands Command |
HCI_ReadLocalSupportedFeaturesCmd | Read Local Supported Features Command |
HCI_ReadLocalVersionInfoCmd | Read Local Version Information Command |
HCI_ReadRssiCmd | Read RSSI Command |
HCI_ReadTransmitPowerLevelCmd | Read Transmit Power Level Command |
HCI_ResetCmd | Reset Command |
HCI_SetEventMaskCmd | Set Event Mask Command |
HCI_SetEventMaskPage2Cmd | Set Event Mask Page 2 Command |
HCI_LE_ReadTxPowerCmd | LE Read Tx Power Command |
HCI_LE_ReadRfPathCompCmd | LE Read Rf Path Compensation Command |
HCI_LE_WriteRfPathCompCmd | LE Write Rf Path Compensation Command |
This section lists the mapping between stack APIs and function names, as described in the Vendor Specific API guide included with the installer.
Stack API | Vendor Specific Function |
---|---|
HCI_EXT_BuildRevisionCmd | HCI Extension Build Revision |
HCI_EXT_DecryptCmd | HCI Extension Decrypt |
HCI_EXT_DisconnectImmedCmd | HCI Extension Disconnect Immediate |
HCI_EXT_EnhancedModemHopTestTxCmd | HCI Extension Enhanced Modem Hop Test Transmit |
HCI_EXT_EnhancedModemTestRxCmd | HCI Extension Enhanced Modem Test Receive |
HCI_EXT_EnhancedModemTestTxCmd | HCI Extension Enhanced Modem Test Transmit |
HCI_EXT_EnablePTMCmd | HCI Extension Enable PTM |
HCI_EXT_EndModemTestCmd | HCI Extension End Modem Test |
HCI_EXT_ModemHopTestTxCmd | HCI Extension Modem Hop Test Transmit |
HCI_EXT_ModemTestRxCmd | HCI Extension Modem Test Receive |
HCI_EXT_ModemTestTxCmd | HCI Extension Modem Test Transmit |
HCI_EXT_NumComplPktsLimitCmd | HCI Extension Number Completed Packets Limit |
HCI_EXT_OnePktPerEvtCmd | HCI Extension One Packet Per Event |
HCI_EXT_PacketErrorRateCmd | HCI Extension Packet Error Rate |
HCI_EXT_PERbyChanCmd | HCI Extension Packet Error Rate By Channel |
HCI_EXT_SaveFreqTuneCmd | HCI Extension Save Frequency Tuning |
HCI_EXT_SetFastTxResponseTimeCmd | HCI Extension Set Fast Transmit Response Time |
HCI_EXT_SetFreqTuneCmd | HCI Extension Set Frequency Tuning |
HCI_EXT_SetLocalSupportedFeaturesCmd | HCI Extension Set Local Supported Features |
HCI_EXT_SetMaxDataLenCmd | HCI Extension Set Max Data Length |
HCI_EXT_SetMaxDtmTxPowerCmd | HCI Extension Set Max DTM Transmitter Power |
HCI_EXT_SetRxGainCmd | HCI Extension Set Receiver Gain |
HCI_EXT_SetSCACmd | HCI Extension Set SCA |
HCI_EXT_SetTxPowerCmd | HCI Extension Set Transmitter Power |
HCI_EXT_SetDtmTxPktCntCmd | HCI Extension Set DTM Transmitter Packet Count |