TI-OpenThread SysConfig¶
SysConfig with TI-OpenThread provides a graphical interface to configure application-level parameters for the OpenThread stack, such as network credentials and default channel.
All TI-OpenThread examples have a SysConfig-enabled version, located under
<SDK>/examples/syscfg_preview/. When imported, the SysConfig tool is
opened by double-clicking the *.syscfg file in the project location. In
the SysConfig tool, TI-OpenThread is listed as a separate software component
under RF-stacks. Click on the component to open the TI-OpenThread
configuration view.
Figure 84. TI-OpenThread software component in SysConfig
Warning
One important note about TI-OpenThread SysConfig is how SysConfig settings and non-volatile storage settings are applied. If the LaunchPad’s non-volatile storage holds a valid Thread dataset, SysConfig settings will not be applied on boot. SysConfig settings are only applied when non-volatile storage does not hold a valid Thread dataset. To guarantee SysConfig settings are applied, perform a factory reset of the non-volatile storage.
TI-OpenThread Settings¶
The TI-OpenThread configuration is locked to the device type of the example project. In other words, if the imported example is configured for the FTD device type, the TI-OpenThread SysConfig will be locked for the FTD device type.
View available parameters by expanding parameter groups. Hovering the cursor over a parameter group or a parameter will display a question mark next to the name, which when clicked on will display more information for that particular parameter or parameter group.
Figure 85. TI-OpenThread configuration view
You can see the generated files by clicking the <> symbol in the top right
corner. The Board.c/h files was generated by the TI DRIVERS components,
the smartrf_settings/smartrf_settings.c/h was generated by the RF Driver
component, and the tiop_config.c/h files was generated by the
TI-OpenThread component.
Figure 86. Generated files from TI-OpenThread configuration
The files are generated when building the project. After the build has completed, you will find the generated files in the output folder of your project.
Attention
Whenever you re-build the project, SysConfig will re-generate the files. Because of this, any changes made directly in the generated files will be overwritten.
tiop_config Reference¶
TI-OpenThread configuration in SysConfig generates a set of defines which
configures the tiop_config file. Below is a compilation of available
SysConfig parameters for TI-OpenThread and which corresponding define names
are set for that parameter.
| Submodule | Configurable Name | Define Name |
|---|---|---|
| Top Level | Device Type | TIOP_CONFIG_LINK_MODE_D |
| Power Management | Power Mode of Operation | TIOP_CONFIG_LINK_MODE_R |
| Poll Peroid | TIOP_CONFIG_POLL_PERIOD |
|
| Radio | Default Channel | TIOP_CONFIG_LINK_CHANNEL |
| Default Power | TIOP_CONFIG_TX_POWER |
|
| Network | Set Network ID | TIOP_CONFIG_SET_NW_ID |
| PAN ID | TIOP_CONFIG_PAN_ID |
|
| Extended PAN ID | TIOP_CONFIG_EXT_PAN_ID |
|
| Thread Master Key | TIOP_CONFIG_MASTER_KEY_L
TIOP_CONFIG_MASTER_KEY_U |
|
| Network Name | TIOP_CONFIG_NETWORK_NAME |
|
| Security | Pre-Shared Key | TIOP_CONFIG_PKSD |