TI Logo
SimpleLink™ CC13x2 / CC26x2 SDK Proprietary RF User's Guide
4.10.00
  • Proprietary RF Quick Start Guide
  • SimpleLink Wireless MCU CC13x2 or CC26x2 Overview
  • Examples User’s Guide
  • Custom hardware
  • TI-RTOS (RTOS Kernel) Overview
  • noRTOS Overview
  • RF Core
  • Proprietary Physical Layer
  • EasyLink Layer
  • Debugging
  • Memory overview
  • Over-the-Air Download (OAD)
  • System Configuration Tool (SysConfig)
  • EnergyTrace User Guide
  • Migration Guides
    • Porting Guides
      • Porting From EasyLink 2.40.3 to EasyLink 2.50.1
      • Porting From EasyLink 2.40.2 to EasyLink 2.40.3
      • Upgrading from TI-RTOS 2.21 to Device SDK
      • Upgrading an Existing TI-RTOS Project to SimpleLink CC13x2 / 26x2 SDK
    • Migration Guides
  • API References
  • Terms and acronyms




SimpleLink™ CC13x2 / CC26x2 SDK Proprietary RF User's Guide
  • »
  • Migration Guides »
  • Porting From EasyLink 2.40.3 to EasyLink 2.50.1

Porting From EasyLink 2.40.3 to EasyLink 2.50.1¶

EasyLink 2.40.3 is bundled with the SimpleLink CC13x2 and CC26x2 2.40 SDK. EasyLink 2.50.1 is bundled with the SimpleLink CC13x2 and CC26x2 3.10 SDK.

For this migration guide, the rfEasyLinkTx project will be ported from EasyLink 2.40.3 to EasyLink 2.50.1. The steps should be transferable for any EasyLink example project.

This migration guide will explain how to port a SysConfig example project. If you have a non-SysConfig enabled project, you can make the same adjustments directly in the file SysConfig would build (easylink_config.c, board files).

Note

Non-SysConfig enabled projects will be deprecated from the SimpleLink CC13x2 / 26x2 SDK in a future release. If you want to migrate your non-SysConfig enabled project to use SysConfig, please see SysConfig Migration.

Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a EasyLink 2.50.1 project that contains the same base functionality as the porting target project and merge in any custom functionality.

  1. Download and install CCS 9.

    Previous versions of CCS is not supported by SysConfig in the SimpleLink CC13x2 and CC26x2 3.10 SDK

  2. Choose a EasyLink 2.50.1 example project that contains your target project’s base functionality.

    For this example, we will use rfEasyLinkTx as the starting EasyLink 2.50.1 example project.

  3. Transfer all modified application files from EasyLink 2.40.3 into the EasyLink 2.50.1 example project.

    In this example, the following files from EasyLink 2.40.3 were moved into rfEasyLinkTx EasyLink 2.50.1 example:

    • rfEasyLinkTx.c
  4. Re-do .syscfg configuration.

    By opening your EasyLink 2.40.3 .syscfg file in one window and your EasyLink 2.50.1 .syscfg file you can re-do the SysConfig configurable parameters. Note that while the groups have been slightly re-organized, the parameters stay the same. You can read about configuring with SysConfig in EasyLink Configuration.

Next Previous

2016-2020, Texas Instruments, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale