![]() |
![]() |
TI BLE5-Stack API Documentation
2.02.01.00
|
RTLS Control module interface.
This file contains the functions and structures specific to AoA.
Go to the source code of this file.
Macros | |
#define | RTLS_CMD_ADD_DEVICE_ADV_LIST 0x0D |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_ENABLE 0x14 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_ANGLE 0x23 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_PAIR_ANGLES 0x25 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_RAW 0x24 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_SET_PARAMS 0x13 |
RTLS Node Manager command. | |
#define | RTLS_CMD_BLE_LOG_STRINGS_MAX 0x32 |
#define | RTLS_CMD_CL_AOA_ENABLE 0x15 |
RTLS Node Manager Command. | |
#define | RTLS_CMD_CL_AOA_RESULT_ANGLE 0x35 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CL_AOA_RESULT_PAIR_ANGLES 0x34 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CL_AOA_RESULT_RAW 0x33 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CLEAR_ADV_LIST 0x10 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONN_INFO 0x27 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONN_PARAMS 0x02 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONNECT 0x03 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CREATE_SYNC 0x09 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CREATE_SYNC_CANCEL 0x0A |
RTLS Node Manager command. | |
#define | RTLS_CMD_GET_ACTIVE_CONN_INFO 0x32 |
RTLS Node Manager command. | |
#define | RTLS_CMD_GET_RTLS_PARAM 0x29 |
RTLS Node Manager command. | |
#define | RTLS_CMD_HEAP_SIZE 0x36 |
RTLS Node Manager command. | |
#define | RTLS_CMD_IDENTIFY 0x00 |
RTLS Node Manager command. | |
#define | RTLS_CMD_PERIODIC_RECEIVE_ENABLE 0x0C |
RTLS Node Manager command. | |
#define | RTLS_CMD_READ_ADV_LIST_SIZE 0x0F |
RTLS Node Manager command. | |
#define | RTLS_CMD_REMOVE_DEVICE_ADV_LIST 0x0E |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED 0x01 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED1 0x06 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED2 0x07 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED3 0x08 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED4 0x26 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED5 0x30 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED6 0x31 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESET_DEVICE 0x20 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN 0x04 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN_STOP 0x05 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SET_RTLS_PARAM 0x28 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TERMINATE_LINK 0x22 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TERMINATE_SYNC 0x0B |
RTLS Node Manager command. | |
#define | RTLS_CTRL_ALL_EVENTS (RTLS_QUEUE_EVT) |
RTLS Task configuration. | |
#define | RTLS_CTRL_TASK_PRIORITY 2 |
RTLS Task configuration variable. | |
#define | RTLS_CTRL_TASK_STACK_SIZE 752 |
RTLS Task configuration variable. | |
#define | RTLS_EVT_ASSERT 0x80 |
RTLS async event. | |
#define | RTLS_EVT_CL_AOA_ENABLE 0x88 |
RTLS async event. | |
#define | RTLS_EVT_CONN_INFO 0x83 |
RTLS async event. | |
#define | RTLS_EVT_DEBUG 0x82 |
RTLS async event. | |
#define | RTLS_EVT_ERROR 0x81 |
RTLS async event. | |
#define | RTLS_EVT_PERIODIC_ADV_RPT 0x86 |
RTLS async event. | |
#define | RTLS_EVT_SYNC_EST 0x84 |
RTLS async event. | |
#define | RTLS_EVT_SYNC_LOST 0x85 |
RTLS async event. | |
#define | RTLS_EVT_TERMINATE_SYNC 0x87 |
RTLS async event. | |
#define | RTLS_PARAM_2 0x02 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_PARAM_3 0x03 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_PARAM_CONNECTION_INTERVAL 0x01 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_QUEUE_EVT UTIL_QUEUE_EVENT_ID |
Event_Id_30. | |
#define | RTLSUTIL_FREE(pFree) |
RTLSUTIL_FREE memory free without icall. More... | |
#define | RTLSUTIL_MALLOC(pAlloc, size) |
RTLSUTIL_MALLOC memory allocation without icall. More... | |
Functions | |
void * | RTLSCtrl_malloc (uint32_t sz) |
This function will allocate memory, if we were unable to allocate we will report to RTLS Host. More... | |
Variables | |
uint8_t | maxNumClCteBufs |
Maximum number of buffers for CL AoA. | |
char * | rtlsCmd_BleLogStrings [] |