83 #ifndef ti_drivers_SDFatFS__include 84 #define ti_drivers_SDFatFS__include 90 #include <third_party/fatfs/ff.h> 91 #include <third_party/fatfs/diskio.h> 140 extern SDFatFS_Handle
SDFatFS_open(uint_least8_t idx, uint_least8_t drive);
SD_Handle sdHandle
Definition: SDFatFS.h:105
SD Global configuration.
Definition: SD.h:317
SDFatFS Global configuration.
Definition: SDFatFS.h:119
SDFatFS_Object * object
Definition: SDFatFS.h:121
SDFatFS_Config * SDFatFS_Handle
A handle that is returned from a SDFatFS_open() call.
Definition: SDFatFS.h:128
DSTATUS diskState
Definition: SDFatFS.h:103
SDFatFS_Handle SDFatFS_open(uint_least8_t idx, uint_least8_t drive)
Function to open a SDFatFS instance on the specified drive.
Secure Digital (SD) Driver.
void SDFatFS_close(SDFatFS_Handle handle)
Function to close a SDFatFS instance specified by the SDFatFS handle.
FATFS filesystem
Definition: SDFatFS.h:104
uint_fast32_t driveNum
Definition: SDFatFS.h:102
SDFatFS Object The application must not access any member variables of this structure! ...
Definition: SDFatFS.h:101