TI Logo
SimpleLink™ CC13x2 / CC26x2 SDK Proprietary RF User's Guide
3.20.00
  • Proprietary RF Quick Start Guide
  • SimpleLink Wireless MCU CC13x2 or CC26x2 Overview
  • Examples User’s Guide
  • Custom hardware
  • TI-RTOS (RTOS Kernel) Overview
  • noRTOS Overview
  • RF Core
  • Proprietary Physical Layer
  • EasyLink Layer
  • Debugging
  • Memory overview
  • Over-the-Air Download (OAD)
  • System Configuration Tool (SysConfig)
    • Get started with SysConfig
    • Configure The Board Files with SysConfig
    • Radio Configuration
    • EasyLink Configuration
    • Disable SysConfig
  • EnergyTrace User Guide
  • Migration Guides
  • API References
  • Terms and acronyms




SimpleLink™ CC13x2 / CC26x2 SDK Proprietary RF User's Guide
  • »
  • System Configuration Tool (SysConfig)

System Configuration Tool (SysConfig)¶

SysConfig is a graphical tool for configuring your SimpleLink SDK project. To set up SysConfig please see the section Get started with SysConfig.

  • Get started with SysConfig
    • Using Stand-alone SysConfig
    • Using SysConfig with IAR Workbench
    • Using SysConfig as a Plug-In to CCS
    • Viewing SysConfig Output
  • Configure The Board Files with SysConfig
  • Radio Configuration
    • Open An Example Project
    • Adding RF Settings
  • EasyLink Configuration
    • Open An Example Project
    • Adding RF Settings
    • EasyLink Settings
    • Adjust Your Application
  • Disable SysConfig
    • First Method: Stop SysConfig From Running
    • Second Method: Exclude SysConfig From Build
Next Previous

2016-2019, Texas Instruments, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale