608 #ifndef ti_drivers_spi_SPICC26XXDMA__include 609 #define ti_drivers_spi_SPICC26XXDMA__include 618 #include <ti/drivers/dpl/HwiP.h> 619 #include <ti/drivers/dpl/SemaphoreP.h> 620 #include <ti/drivers/dpl/SwiP.h> 658 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 667 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 675 #define SPICC26XXDMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 679 #define SPICC26XXDMA_RETURN_PARTIAL_ENABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE 680 #define SPICC26XXDMA_RETURN_PARTIAL_DISABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE 681 #define SPICC26XXDMA_SET_CSN_PIN SPICC26XXDMA_CMD_SET_CSN_PIN Definition: SPICC26XXDMA.h:701
uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:578
PIN_Id csnPin
Definition: SPICC26XXDMA.h:838
const SPI_FxnTable SPICC26XXDMA_fxnTable
uint16_t defaultTxBufValue
Definition: SPICC26XXDMA.h:787
Serial Peripheral Interface (SPI) Driver Interface.
uint32_t baseAddr
Definition: SPICC26XXDMA.h:761
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:584
Power_NotifyObj spiPostObj
Definition: SPICC26XXDMA.h:857
unsigned int bitRate
SPI bit rate in Hz.
Definition: SPICC26XXDMA.h:822
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26XXDMA.h:814
uint32_t minDmaTransferSize
Definition: SPICC26XXDMA.h:802
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:620
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26XXDMA.h:777
uint32_t rxChannelBitMask
Definition: SPICC26XXDMA.h:789
void * spiPreFxn
Definition: SPICC26XXDMA.h:854
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:221
uint32_t txChannelBitMask
Definition: SPICC26XXDMA.h:791
uint16_t scratchBuf
Definition: SPICC26XXDMA.h:851
Power manager interface for CC26XX/CC13XX.
PIN_Id clkPin
Definition: SPICC26XXDMA.h:797
SPICC26XXDMA Hardware attributes.
Definition: SPICC26XXDMA.h:759
volatile bool spiPowerConstraint
Definition: SPICC26XXDMA.h:859
PIN_Id misoPin
Definition: SPICC26XXDMA.h:795
SPI_TransferMode transferMode
Definition: SPICC26XXDMA.h:812
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:711
SPICC26XXDMA Object.
Definition: SPICC26XXDMA.h:810
Device-specific pin & GPIO driver for CC26xx family [def].
void * spiPostFxn
Definition: SPICC26XXDMA.h:855
PIN_State pinState
Definition: SPICC26XXDMA.h:841
SPI_Mode mode
Definition: SPICC26XXDMA.h:815
SPICC26XXDMA_FrameSize
Definition: SPICC26XXDMA.h:700
SPICC26XXDMA_FrameSize frameSize
Definition: SPICC26XXDMA.h:835
UDMACC26XX driver implementation.
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:563
bool returnPartial
Definition: SPICC26XXDMA.h:848
Power notify object structure.
Definition: Power.h:443
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:590
PIN_Id csnPin
Definition: SPICC26XXDMA.h:799
UDMACC26XX_Handle udmaHandle
Definition: SPICC26XXDMA.h:845
uint8_t intNum
Definition: SPICC26XXDMA.h:763
PIN_Id mosiPin
Definition: SPICC26XXDMA.h:793
unsigned int transferTimeout
Definition: SPICC26XXDMA.h:813
underlying data structure for type PIN_State
Definition: PIN.h:708
HwiP_Struct hwi
Definition: SPICC26XXDMA.h:827
SPI_FrameFormat frameFormat
Definition: SPICC26XXDMA.h:824
Power_NotifyObj spiPreObj
Definition: SPICC26XXDMA.h:856
SemaphoreP_Struct transferComplete
Definition: SPICC26XXDMA.h:829
SwiP_Struct swi
Definition: SPICC26XXDMA.h:828
size_t amtDataXferred
Definition: SPICC26XXDMA.h:833
bool isOpen
Definition: SPICC26XXDMA.h:861
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26XXDMA.h:783
Definition: SPICC26XXDMA.h:702
PowerCC26XX_Resource powerMngrId
Definition: SPICC26XXDMA.h:785
size_t currentXferAmt
Definition: SPICC26XXDMA.h:834
PIN_Handle pinHandle
Definition: SPICC26XXDMA.h:842
unsigned int dataSize
Definition: SPICC26XXDMA.h:823
SPI_FrameFormat
Definitions for various SPI data frame formats.
Definition: SPI.h:599
SPI_Transaction * currentTransaction
Definition: SPICC26XXDMA.h:832
struct SPICC26XXDMA_Object * SPICC26XXDMA_Handle