54 #ifndef ti_drivers_sha2_SHA2CC26X2__include 55 #define ti_drivers_sha2_SHA2CC26X2__include 93 #define SHA2CC26X2_MAX_BLOCK_SIZE_BYTES (SHA2_BLOCK_SIZE_BYTES_512) 94 #define SHA2CC26X2_MAX_DIGEST_LENGTH_BYTES (SHA2_DIGEST_LENGTH_BYTES_512) 103 volatile bool operationInProgress;
104 bool operationCanceled;
106 int_fast16_t returnStatus;
107 uint32_t accessTimeout;
110 uint16_t bytesInBuffer;
111 uint32_t bytesProcessed;
112 uint8_t buffer[SHA2CC26X2_MAX_BLOCK_SIZE_BYTES];
113 uint32_t digest[SHA2CC26X2_MAX_DIGEST_LENGTH_BYTES / 4];
SHA2_ReturnBehavior
The way in which SHA2 function calls return after performing an operation.
Definition: SHA2.h:282
SHA2_HashType
Enum for the hash types supported by the driver.
Definition: SHA2.h:302
Hardware-specific configuration attributes.
Definition: SHA2CC26X2.h:73
void(* SHA2_CallbackFxn)(SHA2_Handle handle, int_fast16_t returnStatus)
The definition of a callback function used by the SHA2 driver when used in SHA2_RETURN_BEHAVIOR_CALLB...
Definition: SHA2.h:373
uint8_t intPriority
Definition: SHA2CC26X2.h:74