26 #ifndef RTLS_CTRL_API_H_ 27 #define RTLS_CTRL_API_H_ 43 extern void AssertHandler(uint8 assertCause, uint8 assertSubcause);
50 #define RTLS_CTRL_ASSERT_CAUSE_OUT_OF_MEMORY 0x01 51 #define RTLS_CTRL_ASSERT_CAUSE_INVALID_PARAM 0x02 52 #define RTLS_CTRL_ASSERT_CAUSE_NULL_POINTER_EXCEPT 0x03 55 #define RTLS_CTRL_REV 0x2 58 #define RTLS_REQ_ENABLE_SYNC 0x1 59 #define RTLS_REQ_CONN 0x2 60 #define RTLS_REQ_SCAN 0x3 61 #define RTLS_REQ_SEND_DATA 0x4 62 #define RTLS_REQ_TERMINATE_LINK 0x5 63 #define RTLS_REQ_SET_AOA_PARAMS 0x6 64 #define RTLS_REQ_AOA_ENABLE 0x7 65 #define RTLS_REQ_UPDATE_CONN_INTERVAL 0x8 66 #define RTLS_REQ_GET_ACTIVE_CONN_INFO 0x9 68 #define RTLS_REQ_BLE_LOG_STRINGS_MAX 0x9 69 extern char *rtlsReq_BleLogStrings[];
72 #define CHIP_ID_ADDR ((uint8_t *)(0x50001000 + 0x2E8)) 73 #define CHIP_ID_SIZE 6 79 #define RTLS_CONNHANDLE_ALL 0xFFFD // All connection handles 80 #define RTLS_CONNHANDLE_INVALID 0xFFFF // Invalid connection handle, used for no connection handle 101 RTLS_CONFIG_NOT_SUPPORTED,
108 RTLS_CAP_NOT_INITIALIZED = 0x00000000,
109 RTLS_CAP_CM = 0x00000001,
110 RTLS_CAP_AOA_TX = 0x00000002,
111 RTLS_CAP_AOA_RX = 0x00000004,
112 RTLS_CAP_RESERVED1 = 0x00000008,
113 RTLS_CAP_RESERVED2 = 0x00000010,
114 RTLS_CAP_RESERVED3 = 0x00000020,
115 RTLS_CAP_RTLS_SLAVE = 0x00000040,
116 RTLS_CAP_RTLS_MASTER = 0x00000080,
117 RTLS_CAP_RTLS_PASSIVE = 0x00000100
240 void RTLSCtrl_syncNotifyEvt(uint16_t connHandle, rtlsStatus_e status, uint32_t timeToNextEvent, int8_t rssi, uint8_t channel);
269 void RTLSCtrl_aoaResultEvt(uint16_t connHandle, int8_t rssi, uint8_t channel, uint16_t numIqSamples, uint8_t sampleRate, uint8_t sampleSize, uint8_t sampleCtrl, uint8_t slotDuration, uint8_t numAnt, int8_t *pIQ);
#define CHIP_ID_SIZE
Chip Identifier Size.
Definition: rtls_ctrl_api.h:73
RTLS terminate link request.
Definition: rtls_ctrl_api.h:162
RTLS Configuration structure.
Definition: rtls_ctrl_api.h:121
uint8_t * pData
Pointer to request.
Definition: rtls_ctrl_api.h:135
void RTLSCtrl_dataSentEvt(uint16_t connHandle, uint8_t status)
RTLSCtrl_dataSentEvt.
rtlsCapabilities_e
Enumeration for RTLS Capabilities.
Definition: rtls_ctrl_api.h:106
uint8_t cmdOp
RTLS Application Command Opcode.
Definition: rtls_ctrl_api.h:142
void RTLSCtrl_scanResultEvt(rtlsStatus_e status, uint8_t *scanResult, uint8_t size)
RTLSCtrl_scanResultEvt.
void RTLSCtrl_sendDebugEvt(uint8_t *debug_string, uint32_t debug_value)
RTLSCtrl_sendDebugEvt.
void RTLSCtrl_connResultEvt(uint16_t connHandle, uint8_t status)
RTLSCtrl_connResultEvt.
void RTLSCtrl_rtlsPacketEvt(uint8_t *pPkt)
RTLSCtrl_rtlsPacketEvt.
void RTLSCtrl_connInfoEvt(uint8_t *connInfo, uint16_t connInfoLen)
RTLSCtrl_connInfoEvt.
void(* pfnRtlsAppCb)(uint8_t *cmd)
Application callback function.
Definition: rtls_ctrl_api.h:91
RTLS Enable Sync - This will tell the RTLS Application to start notifying RTLS Control about a specif...
Definition: rtls_ctrl_api.h:148
uint16_t payloadLen
Length.
Definition: rtls_ctrl_api.h:143
uint16_t connHandle
Connection handle.
Definition: rtls_ctrl_api.h:164
uint16_t revNum
Revision.
Definition: rtls_ctrl_api.h:125
void RTLSCtrl_aoaResultEvt(uint16_t connHandle, int8_t rssi, uint8_t channel, uint16_t numIqSamples, uint8_t sampleRate, uint8_t sampleSize, uint8_t sampleCtrl, uint8_t slotDuration, uint8_t numAnt, int8_t *pIQ)
RTLSCtrl_aoaResultEvt.
rtlsCapabilities_e rtlsCapab
RTLS Capabilities.
Definition: rtls_ctrl_api.h:123
uint8_t reqOp
Request Opcode.
Definition: rtls_ctrl_api.h:134
uint16_t connHandle
Connection handle.
Definition: rtls_ctrl_api.h:157
void RTLSCtrl_open(rtlsConfiguration_t *rtlsConfig)
RTLSCtrl_open.
RTLS Packet - Generic structure that will be translated to a specific command.
Definition: rtls_ctrl_api.h:139
pfnRtlsAppCb rtlsAppCb
Application callback function.
Definition: rtls_ctrl_api.h:128
rtlsStatus_e
Enumeration for RTLS Status.
Definition: rtls_ctrl_api.h:94
RTLS Get Active Connection Info - get the connection information for a specific handle.
Definition: rtls_ctrl_api.h:168
void RTLSCtrl_syncNotifyEvt(uint16_t connHandle, rtlsStatus_e status, uint32_t timeToNextEvent, int8_t rssi, uint8_t channel)
RTLSCtrl_syncNotifyEvt.
RTLS Control request.
Definition: rtls_ctrl_api.h:132
uint16_t connHandle
Connection handle.
Definition: rtls_ctrl_api.h:141
uint8_t maxNumConns
Maximum number of connections to support.
Definition: rtls_ctrl_api.h:127
RTLS update connection interval request.
Definition: rtls_ctrl_api.h:155
uint8_t devId
Device ID.
Definition: rtls_ctrl_api.h:126
uint16_t connInterval
Connection interval.
Definition: rtls_ctrl_api.h:158