NVSCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file NVSCC26XX.h
34  * @brief Non-Volatile Storage driver for CC13XX/CC26XX devices.
35  *
36  * ## Interrupt Latency During Flash Operations #
37  *
38  * When writing or erasing flash, interrupts must be disabled to avoid
39  * executing code in flash while the flash is being reprogrammed. This
40  * constraint is handled by the driver. Application code does not need
41  * to safeguard against this.
42  *
43  * Additionally, to avoid extremely large interrupt latencies that would be
44  * incurred if entire blocks were written with interrupts disabled, block
45  * writes to flash are broken into multiple smaller sizes.
46  *
47  * Even with this scheme in place, latencies of roughly 64 microseconds will
48  * be incurred while flash is being written to.
49  *
50  * A similar caveat applies to flash erase operations. Erasing an entire
51  * flash sector (the minimal amount that can be erased at a time) can take
52  * roughly 8 milliseconds. This entire operation must be performed with
53  * interrupts disabled. Here again, this requirement is met internally
54  * by the driver and flash region erases are performed one sector at a
55  * time to minimize this significant latency impact.
56  *
57  * Care must be taken by the user to not perform flash write or erase
58  * operations during latency critical phases of an application. See the
59  * NVS_lock() and NVS_unlock() API descriptions for more information.
60  *
61  * ## Maximum flash writes before erase #
62  *
63  * On CC13XX & CC26XX memory rows can be 128 or 256 bytes in length; refer to
64  * the device datasheet for the exact size. A maximum of 83 write operations
65  * can be performed on a memory row. Once the limit is reached, the row must
66  * be erased before it is written to again. It is the developer's
67  * responsibility to ensure that this limit is not exceeded in their
68  * applications. The developer may also opt to use the third party SPIFFS
69  * library implementation supported by TIRTOS which does track writes.
70  *
71  * \note The 83 write limit persists through device reset & power cycles.
72  * If 60 write operations were performed on a memory row & the device is
73  * reset; the page can still only be written to 23 more times before it must
74  * be erased.
75  *
76  * A write "Scoreboard" can be enabled in this driver; the scoreboard keeps
77  * track of how many times a page has been written to. It is provided as a
78  * debug tool to ensure the 83 write limit is not exceeded. If a page is
79  * written to more than 83 times, the NVSCC26XX driver will spin forever.
80  * Each byte in the scoreboard corresponds to a memory page in the NVS region.
81  * The byte is incremented when the memory is written to & set to 0 when
82  * erased.
83  *
84  * To enable the "scoreboard" the "NVSCC26XX_INSTRUMENTED" symbol must be
85  * defined when the driver is compiled. Three new fields are added to the
86  * #NVSCC26XX_HWAttrs structure:
87  * * scoreboard - a buffer provided by the application where each byte
88  * represents how many times a page has been written to.
89  * * scoreboardSize - number of bytes in the scoreboard.
90  * * flashPageSize - number of bytes in a flash page (i.e. 128 or 256)
91  *
92  * When configured correctly, the scoreboard can be viewed in a memory browser.
93  *
94  * \note The scoreboard will only keep track of writes to flash within a
95  * NVS region using a NVS driver. Writes performed outside the NVS
96  * region or without the NVS driver are untracked.
97  *
98  * \note The scoreboard is in RAM & will be lost on reset or power cycle.
99  *
100  *
101  * ============================================================================
102  */
103 
104 #ifndef ti_drivers_nvs_NVSCC26XX__include
105 #define ti_drivers_nvs_NVSCC26XX__include
106 
107 #include <stdint.h>
108 #include <stdbool.h>
109 
110 #if defined (__cplusplus)
111 extern "C" {
112 #endif
113 
120 #define NVSCC26XX_STATUS_LOW_VOLTAGE (NVS_STATUS_RESERVED - 1)
121 
154 extern const NVS_FxnTable NVSCC26XX_fxnTable;
155 
296 typedef struct
297 {
298  void *regionBase;
305  size_t regionSize;
316 #if defined(NVSCC26XX_INSTRUMENTED)
317  uint8_t *scoreboard;
318  size_t scoreboardSize;
319  uint32_t flashPageSize;
320 #endif
322 
323 /*
324  * @brief NVSCC26XX Object
325  *
326  * The application must not access any member variables of this structure!
327  */
328 typedef struct
329 {
330  bool opened; /* Has this region been opened */
332 
338 extern void NVSCC26XX_close(NVS_Handle handle);
339 extern int_fast16_t NVSCC26XX_control(NVS_Handle handle, uint_fast16_t cmd,
340  uintptr_t arg);
341 extern int_fast16_t NVSCC26XX_erase(NVS_Handle handle, size_t offset,
342  size_t size);
343 extern void NVSCC26XX_getAttrs(NVS_Handle handle, NVS_Attrs *attrs);
344 extern void NVSCC26XX_init();
345 extern int_fast16_t NVSCC26XX_lock(NVS_Handle handle, uint32_t timeout);
346 extern NVS_Handle NVSCC26XX_open(uint_least8_t index, NVS_Params *params);
347 extern int_fast16_t NVSCC26XX_read(NVS_Handle handle, size_t offset,
348  void *buffer, size_t bufferSize);
349 extern void NVSCC26XX_unlock(NVS_Handle handle);
350 extern int_fast16_t NVSCC26XX_write(NVS_Handle handle, size_t offset,
351  void *buffer, size_t bufferSize, uint_fast16_t flags);
354 #if defined (__cplusplus)
355 }
356 #endif /* defined (__cplusplus) */
357 
359 #endif /* ti_drivers_nvs_NVSCC26XX__include */
NVS attributes.
Definition: NVS.h:488
const NVS_FxnTable NVSCC26XX_fxnTable
void * regionBase
Definition: NVSCC26XX.h:298
NVS Parameters.
Definition: NVS.h:476
bool opened
Definition: NVSCC26XX.h:330
Definition: NVSCC26XX.h:328
size_t regionSize
Definition: NVSCC26XX.h:305
NVSCC26XX hardware attributes.
Definition: NVSCC26XX.h:296
NVS Global configuration.
Definition: NVS.h:618
The definition of an NVS function table that contains the required set of functions to control a spec...
Definition: NVS.h:574
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale