305 #ifndef ti_drivers_i2c_I2CCC26XX__include 306 #define ti_drivers_i2c_I2CCC26XX__include 315 #include <ti/drivers/dpl/HwiP.h> 316 #include <ti/drivers/dpl/SwiP.h> 317 #include <ti/drivers/dpl/SemaphoreP.h> 438 SemaphoreP_Struct mutex;
439 SemaphoreP_Struct transferComplete;
448 unsigned int writeCount;
450 unsigned int readCount;
uint8_t pinSDA
Definition: I2CCC26XX.h:348
int intNum
Definition: I2CCC26XX.h:397
I2CCC26XX Pin Configuration.
Definition: I2CCC26XX.h:347
I2CCC26XX Hardware attributes.
Definition: I2CCC26XX.h:391
I2C_TransferMode
Return behavior of I2C_Transfer() specified in the I2C_Params.
Definition: I2C.h:510
uint8_t sclPin
Definition: I2CCC26XX.h:421
The definition of an I2C function table that contains the required set of functions to control a spec...
Definition: I2C.h:656
unsigned long powerMngrId
Definition: I2CCC26XX.h:395
Device-specific pin & GPIO driver for CC26xx family [def].
Power notify object structure.
Definition: Power.h:443
const I2C_FxnTable I2CCC26XX_fxnTable
underlying data structure for type PIN_State
Definition: PIN.h:708
uint8_t pinSCL
Definition: I2CCC26XX.h:349
uint32_t baseAddr
Definition: I2CCC26XX.h:393
void(* I2C_CallbackFxn)(I2C_Handle handle, I2C_Transaction *transaction, bool transferStatus)
The definition of a callback function.
Definition: I2C.h:560
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
Definition: I2C.h:413
uint8_t sdaPin
Definition: I2CCC26XX.h:419
uint32_t swiPriority
I2C Swi priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: I2CCC26XX.h:417
Inter-Integrated Circuit (I2C) Driver.
uint8_t intPriority
I2C Peripheral's interrupt priority.
Definition: I2CCC26XX.h:411