TI-OpenThread 1.08.00.00 Release Notes

Table of Contents

Introduction

Texas Instrument’s Thread stack is an implementation based on OpenThread, an open-source implementation of Thread™ released by Nest and maintained on GitHub at https://github.com/openthread/openthread. The TI-OpenThread stack allows developers to create Thread 1.1.1 based products using the TI’s SimpleLink™ CC13x2 and CC26x2 family of wireless microcontrollers (MCUs). This software provides various examples which can be used as a framework to develop new end products; this allows you to quickly get started, reducing the time and cost of getting your product to market.

Documentation

What’s New

ID Summary
TIOP-883 Integrate CoreSDK GA for 2Q20
TIOP-882 Downstream public OpenThread 2Q20
TIOP-618 Enable support for CC1352P-4 LP + CC2652P device @ 10dBm

Fixed Issues

ID Summary
None None

Known Issues

ID Summary
TIOP-954 Thermostat attempts to promote to leader and form separate partition during reliability test
TIOP-953 IAR OAD image does not reboot upon a successful OAD transfer

Upgrade and Compatibility Information

The SimpleLink CC13x2 and CC26x2 4.20.00.xx SDK introduces changes that may impact existing projects. Refer to the included porting guide for migrating applications.

Operating System Support

The TI-OpenThread Stack is supported on the platforms supported by this SDK.

Dependencies

TI-OpenThread 1.08.00.00 was built and tested on a Windows host platform using the following Integrated Development Environments (IDEs), toolchains, and components. For supported tool and component version numbers, see the top level SDK release notes.

Note: Earlier IDE/toolchain versions are not supported and compatibility with newer versions of supported IDEs is not assured.

Device Support

See the top-level SDK release notes provided with this SDK for a list of supported devices.

Development Board Support

See the top-level SDK release notes provided with this SDK for a list of supported development boards.

Validation

The TI-OpenThread 1.08.00.00 stack is currently undergoing certification with the Thread Group. Stack certification status can be obtained from a Texas Instruments representative.

OpenThread Downstream

TI-OpenThread is merged with the public OpenThread repository from the following commit hash:

Technical Support and Product Updates