Go to the documentation of this file. 37 #ifndef _IEEE_MAILBOX_H 38 #define _IEEE_MAILBOX_H 46 #define IEEE_SUSPENDED 0x2001 47 #define IEEE_DONE_OK 0x2400 51 #define IEEE_DONE_BUSY 0x2401 52 #define IEEE_DONE_STOPPED 0x2402 53 #define IEEE_DONE_ACK 0x2403 54 #define IEEE_DONE_ACKPEND 0x2404 55 #define IEEE_DONE_TIMEOUT 0x2405 56 #define IEEE_DONE_BGEND 0x2406 57 #define IEEE_DONE_ABORT 0x2407 59 #define IEEE_ERROR_PAR 0x2800 63 #define IEEE_ERROR_NO_SETUP 0x2801 64 #define IEEE_ERROR_NO_FS 0x2802 65 #define IEEE_ERROR_SYNTH_PROG 0x2803 66 #define IEEE_ERROR_RXOVF 0x2804 67 #define IEEE_ERROR_TXUNF 0x2805
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale