649 #ifndef ti_drivers_rfcc26x2__include 650 #define ti_drivers_rfcc26x2__include 659 #include <ti/drivers/dpl/ClockP.h> 660 #include <ti/drivers/dpl/SemaphoreP.h> 661 #include <ti/drivers/utils/List.h> 663 #include <ti/devices/DeviceFamily.h> 664 #include DeviceFamily_constructPath(driverlib/rf_common_cmd.h) 665 #include DeviceFamily_constructPath(driverlib/rf_prop_cmd.h) 666 #include DeviceFamily_constructPath(driverlib/rf_ble_cmd.h) 679 #define RF_EventCmdDone (1 << 0) 680 #define RF_EventLastCmdDone (1 << 1) 681 #define RF_EventFGCmdDone (1 << 2) 682 #define RF_EventLastFGCmdDone (1 << 3) 683 #define RF_EventTxDone (1 << 4) 684 #define RF_EventTXAck (1 << 5) 685 #define RF_EventTxCtrl (1 << 6) 686 #define RF_EventTxCtrlAck (1 << 7) 687 #define RF_EventTxCtrlAckAck (1 << 8) 688 #define RF_EventTxRetrans (1 << 9) 689 #define RF_EventTxEntryDone (1 << 10) 690 #define RF_EventTxBufferChange (1 << 11) 691 #define RF_EventPaChanged (1 << 14) 692 #define RF_EventSamplesEntryDone (1 << 15) 693 #define RF_EventRxOk (1 << 16) 694 #define RF_EventRxNOk (1 << 17) 695 #define RF_EventRxIgnored (1 << 18) 696 #define RF_EventRxEmpty (1 << 19) 697 #define RF_EventRxCtrl (1 << 20) 698 #define RF_EventRxCtrlAck (1 << 21) 699 #define RF_EventRxBufFull (1 << 22) 700 #define RF_EventRxEntryDone (1 << 23) 701 #define RF_EventDataWritten (1 << 24) 702 #define RF_EventNDataWritten (1 << 25) 703 #define RF_EventRxAborted (1 << 26) 704 #define RF_EventRxCollisionDetected (1 << 27) 705 #define RF_EventModulesUnlocked (1 << 29) 706 #define RF_EventInternalError (uint32_t)(1 << 31) 707 #define RF_EventMdmSoft 0x0000002000000000 717 #define RF_EventCmdCancelled 0x1000000000000000 718 #define RF_EventCmdAborted 0x2000000000000000 719 #define RF_EventCmdStopped 0x4000000000000000 720 #define RF_EventRatCh 0x0800000000000000 721 #define RF_EventPowerUp 0x0400000000000000 722 #define RF_EventError 0x0200000000000000 723 #define RF_EventCmdPreempted 0x0100000000000000 742 #define RF_CTRL_SET_INACTIVITY_TIMEOUT 0 752 #define RF_CTRL_UPDATE_SETUP_CMD 1 758 #define RF_CTRL_SET_POWERUP_DURATION_MARGIN 2 766 #define RF_CTRL_SET_PHYSWITCHING_DURATION_MARGIN 3 774 #define RF_CTRL_SET_RAT_RTC_ERR_TOL_VAL 4 786 #define RF_CTRL_SET_POWER_MGMT 5 808 #define RF_CTRL_SET_HWI_PRIORITY 6 830 #define RF_CTRL_SET_SWI_PRIORITY 7 840 #define RF_CTRL_SET_AVAILABLE_RAT_CHANNELS_MASK 8 855 #define RF_CTRL_COEX_CONTROL 9 869 #define RF_TxPowerTable_MIN_DBM -128 877 #define RF_TxPowerTable_MAX_DBM 126 884 #define RF_TxPowerTable_INVALID_DBM 127 903 #define RF_TxPowerTable_INVALID_VALUE 0x3fffff 920 #define RF_TxPowerTable_TERMINATION_ENTRY \ 921 { .power = RF_TxPowerTable_INVALID_DBM, .value = { .rawValue = RF_TxPowerTable_INVALID_VALUE, .paType = RF_TxPowerTable_DefaultPA } } 929 #define RF_TxPowerTable_DEFAULT_PA_ENTRY(bias, gain, boost, coefficient) \ 930 { .rawValue = ((bias) << 0) | ((gain) << 6) | ((boost) << 8) | ((coefficient) << 9), .paType = RF_TxPowerTable_DefaultPA } 938 #define RF_TxPowerTable_HIGH_PA_ENTRY(bias, ibboost, boost, coefficient, ldotrim) \ 939 { .rawValue = ((bias) << 0) | ((ibboost) << 6) | ((boost) << 8) | ((coefficient) << 9) | ((ldotrim) << 16), .paType = RF_TxPowerTable_HighPA } 948 #define RF_GET_RSSI_ERROR_VAL (-128) 949 #define RF_CMDHANDLE_FLUSH_ALL (-1) 950 #define RF_ALLOC_ERROR (-2) 951 #define RF_SCHEDULE_CMD_ERROR (-3) 952 #define RF_ERROR_RAT_PROG (-255) 953 #define RF_ERROR_INVALID_RFMODE (-256) 954 #define RF_ERROR_CMDFS_SYNTH_PROG (-257) 956 #define RF_NUM_SCHEDULE_ACCESS_ENTRIES 2 957 #define RF_NUM_SCHEDULE_COMMAND_ENTRIES 8 958 #define RF_NUM_SCHEDULE_MAP_ENTRIES (RF_NUM_SCHEDULE_ACCESS_ENTRIES + RF_NUM_SCHEDULE_COMMAND_ENTRIES) 959 #define RF_SCH_MAP_CURRENT_CMD_OFFSET RF_NUM_SCHEDULE_ACCESS_ENTRIES 960 #define RF_SCH_MAP_PENDING_CMD_OFFSET (RF_SCH_MAP_CURRENT_CMD_OFFSET + 2) 962 #define RF_ABORT_PREEMPTION (1<<2) 963 #define RF_ABORT_GRACEFULLY (1<<0) 965 #define RF_SCH_CMD_EXECUTION_TIME_UNKNOWN 0 967 #define RF_RAT_ANY_CHANNEL (-1) 968 #define RF_RAT_TICKS_PER_US 4 970 #define RF_LODIVIDER_MASK 0x7F 979 #define RF_STACK_ID_DEFAULT 0x00000000 980 #define RF_STACK_ID_154 0x8000F154 981 #define RF_STACK_ID_BLE 0x8000FB1E 982 #define RF_STACK_ID_EASYLINK 0x8000FEA2 983 #define RF_STACK_ID_THREAD 0x8000FEAD 984 #define RF_STACK_ID_TOF 0x8000F00F 985 #define RF_STACK_ID_CUSTOM 0x0000FC00 991 #define RF_convertUsToRatTicks(microseconds) \ 992 ((microseconds) * (RF_RAT_TICKS_PER_US)) 997 #define RF_convertMsToRatTicks(milliseconds) \ 998 ((milliseconds) * 1000 * (RF_RAT_TICKS_PER_US)) 1003 #define RF_convertRatTicksToUs(ticks) \ 1004 ((ticks) / (RF_RAT_TICKS_PER_US)) 1009 #define RF_convertRatTicksToMs(ticks) \ 1010 ((ticks) / (1000 * (RF_RAT_TICKS_PER_US))) 1025 uint32_t rawValue:22;
1101 void (*cpePatchFxn)(void);
1102 void (*mcePatchFxn)(void);
1103 void (*rfePatchFxn)(void);
1395 typedef struct RF_ObjectMultiMode
RF_Object;
1400 struct RF_ObjectMultiMode{
1403 uint32_t nInactivityTimeout;
1406 uint32_t nPhySwitchingDuration;
1407 uint32_t nPowerUpDuration;
1408 bool bMeasurePowerUpDuration;
1410 uint16_t nPowerUpDurationMargin;
1413 void* pClientEventCb;
1414 RF_ClientEventMask nClientEventMask;
1415 uint16_t nPhySwitchingDurationMargin;
1423 SemaphoreP_Struct semSync;
1424 RF_EventMask
volatile eventSync;
1426 RF_EventMask unpendCause;
1427 ClockP_Struct clkReqAccess;
1473 RF_Handle pClientList[2];
1474 uint32_t phySwitchingTimeInUs[2];
1522 typedef void (*
RF_Callback)(RF_Handle h, RF_CmdHandle ch, RF_EventMask e);
1537 typedef void (*
RF_RatCallback)(RF_Handle h, RF_RatHandle rh, RF_EventMask e, uint32_t compareCaptureTime);
2137 extern RF_EventMask
RF_pendCmd(RF_Handle h, RF_CmdHandle ch, RF_EventMask bmEvent);
2208 extern RF_Stat
RF_cancelCmd(RF_Handle h, RF_CmdHandle ch, uint8_t mode);
2228 extern RF_Stat
RF_flushCmd(RF_Handle h, RF_CmdHandle ch, uint8_t mode);
2319 extern RF_Op*
RF_getCmdOp(RF_Handle h, RF_CmdHandle cmdHnd);
2464 extern RF_Stat
RF_control(RF_Handle h, int8_t ctrl,
void *args);
RF Hardware attributes.
Definition: RFCC26X2.h:1657
Definition: RFCC26X2.h:1621
uint32_t allowDelay
Definition: RFCC26X2.h:1752
RF_RatCaptureMode captureMode
Configuration of the mode of event to cause a capture event.
Definition: RFCC26X2.h:1876
Default PA.
Definition: RFCC26X2.h:1070
Generates a one-clock period width pulse.
Definition: RFCC26X2.h:1841
RF_CmdHandle ch
Command handle (RF_GET_CURR_CMD).
Definition: RFCC26X2.h:1470
RF_StartType startType
Definition: RFCC26X2.h:1642
Definition: RFCC26X2.h:1345
RF_EventMask RF_pendCmd(RF_Handle h, RF_CmdHandle ch, RF_EventMask bmEvent)
Synchronizes the calling task to an RF operation command ch and returns accumulated event flags...
Highest priority. Only use this for urgent commands.
Definition: RFCC26X2.h:1117
Configure RAT_CHANNEL[x] to interface with RAT_GPO[4].
Definition: RFCC26X2.h:1862
RF driver configuration parameters.
Definition: RFCC26X2.h:1579
rfc_CMD_RADIO_SETUP_PA_t common_pa
Radio setup command for BLE and IEEE modes with High Gain PA.
Definition: RFCC26X2.h:1220
RF_TxPowerTable_Value RF_TxPowerTable_findValue(RF_TxPowerTable_Entry table[], int8_t powerLevel)
Retrieves a power configuration value for a given power level in dBm.
uint32_t startTime
Start time window in RAT Time for radio access.
Definition: RFCC26X2.h:1770
RF_Callback volatile pCb
Definition: RFCC26X2.h:1632
RF_RatCallback callback
Callback function to be invoked upon a capture event (optional).
Definition: RFCC26X2.h:1885
Definition: RFCC26X2.h:1620
#define RF_NUM_SCHEDULE_ACCESS_ENTRIES
Number of access request entries.
Definition: RFCC26X2.h:956
Use RAT user channel 0.
Definition: RFCC26X2.h:1782
void RF_RatConfigOutput_init(RF_RatConfigOutput *ioConfig)
Initialize the configuration structure to be used to set up a RAT IO.
uint32_t RF_getCurrentTime(void)
Return current radio timer value.
Definition: RFCC26X2.h:1742
Function was called with an invalid parameter.
Definition: RFCC26X2.h:1190
void(* RF_GlobalCallback)(RF_Handle h, RF_GlobalEvent event, void *arg)
Handles global events as part of PHY configuration.
Definition: RFCC26X2.h:1569
uint16_t nPowerUpDurationMargin
Definition: RFCC26X2.h:1592
Definition: RFCC26X2.h:1798
RF_ExecuteHook executeHook
Function hook implements the runtime last second go-no-go execute decision.
Definition: RFCC26X2.h:1734
Frequency Synthesizer Programming Command.
Definition: rf_common_cmd.h:237
Create a bitmask showing available RAT channels.
Definition: RFCC26X2.h:1457
int8_t RF_getRssi(RF_Handle h)
Get RSSI value.
rfc_CMD_PROP_RADIO_SETUP_PA_t prop_pa
Radio setup command for PROPRIETARY mode on 2.4 GHz with High Gain PA.
Definition: RFCC26X2.h:1222
uint8_t rfMode
Specifies which PHY modes should be activated. Must be set to RF_MODE_MULTIPLE for dual-mode operatio...
Definition: RFCC26X2.h:1100
void RF_close(RF_Handle h)
Close client connection to RF driver.
Definition: RFCC26X2.h:1333
RF_AllowDelay
Controls the behavior of the RF_scheduleCmd() API.
Definition: RFCC26X2.h:1740
Coexistence override settings for BLE5 application scenarios.
Definition: RFCC26X2.h:1171
Definition: RFCC26X2.h:1741
Command finished with an error.
Definition: RFCC26X2.h:1189
RF_ClientEventMask nClientEventMask
Definition: RFCC26X2.h:1602
RF_EndType endType
Definition: RFCC26X2.h:1645
Free the channel after the first capture event.
Definition: RFCC26X2.h:1822
Configure RAT_CHANNEL[x] to interface with RAT_GPO[5].
Definition: RFCC26X2.h:1863
RF_ScheduleStatus
Describes the location within the pend queue where the new command was inserted by the scheduler...
Definition: RFCC26X2.h:1678
RF schedule map entry structure.
Definition: RFCC26X2.h:1481
RF_ExecuteAction
Controls the behavior of the state machine of the RF driver when a conflict is identified run-time be...
Definition: RFCC26X2.h:1669
Chose the first available channel.
Definition: RFCC26X2.h:1781
RF_EventMask RF_runCmd(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
Runs synchronously an RF operation command or a chain of commands and returns the termination reason...
void RF_ScheduleCmdParams_init(RF_ScheduleCmdParams *pSchParams)
Initialize the configuration structure to default values to be used with the RF_scheduleCmd() API...
RF_Stat RF_requestAccess(RF_Handle h, RF_AccessParams *pParams)
Request radio access.
uint32_t allowDelay
Definition: RFCC26X2.h:1643
Cmd is found in the pool but was already ended.
Definition: RFCC26X2.h:1191
Selects the RTC update signal source.
Definition: RFCC26X2.h:1793
Configure RAT_CHANNEL[x] to interface with RAT_GPO[2].
Definition: RFCC26X2.h:1860
RF_EventMask rfifg
Definition: RFCC26X2.h:1637
Definition: RFCC26X2.h:1630
Definition: RFCC26X2.h:1622
RF_RatHandle channel
RF_RatHandle identifies the channel to be allocated.
Definition: RFCC26X2.h:1874
RF_PriorityCoex priority
Priority level for coexistence priority signal.
Definition: RFCC26X2.h:1161
Low priority. Override default value configured by setup command.
Definition: RFCC26X2.h:1134
RF_Handle RF_open(RF_Object *pObj, RF_Mode *pRfMode, RF_RadioSetup *pRadioSetup, RF_Params *params)
Creates a a new client instance of the RF driver.
uint32_t nPowerUpDuration
Definition: RFCC26X2.h:1583
Retrieve a command handle of the current command.
Definition: RFCC26X2.h:1456
High priority. Override default value configured by setup command.
Definition: RFCC26X2.h:1135
Execute if no conflict, let current command finish if conflict.
Definition: RFCC26X2.h:1671
uint8_t swiPriority
Priority for SWIs belong to the RF driver.
Definition: RFCC26X2.h:1659
RF_ExecuteAction(* RF_ExecuteHook)(RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd)
Defines the execution and conflict resolution hook at runtime.
Definition: RFCC26X2.h:1725
Rising edge of the selected source will trigger a capture event.
Definition: RFCC26X2.h:1809
void RF_enableHPOSCTemperatureCompensation(void)
Enables temperature monitoring and temperature based drift compensation.
RF_Stat RF_setTxPower(RF_Handle h, RF_TxPowerTable_Value value)
Updates the transmit power configuration of the RF core.
Definition: RFCC26X2.h:1325
uint8_t volatile flags
Definition: RFCC26X2.h:1640
uint32_t duration
Duration in RAT Ticks for the radio command.
Definition: RFCC26X2.h:1758
rfc_CMD_PROP_RADIO_DIV_SETUP_t prop_div
Radio setup command for PROPRIETARY mode on Sub-1 Ghz.
Definition: RFCC26X2.h:1219
List_Elem _elem
Definition: RFCC26X2.h:1631
RF_GlobalEventMask globalEventMask
Event mask which the globalCallback is invoked upon.
Definition: RFCC26X2.h:1662
RF_RatOutputSelect
Selects GPO to be used with RF_ratCompare() or RF_ratCapture().
Definition: RFCC26X2.h:1858
RF_Op * RF_getCmdOp(RF_Handle h, RF_CmdHandle cmdHnd)
Get command structure pointer.
Stores output parameters for RF_getInfo().
Definition: RFCC26X2.h:1469
RF_Handle pClient
Pointer to client object.
Definition: RFCC26X2.h:1483
RF_CmdHandle RF_postCmd(RF_Handle h, RF_Op *pOp, RF_Priority ePri, RF_Callback pCb, RF_EventMask bmEvent)
Appends RF operation commands to the driver's command queue and returns a command handle...
RF_RatHandle RF_ratCapture(RF_Handle rfHandle, RF_RatConfigCapture *channelConfig, RF_RatConfigOutput *ioConfig)
Setup a Radio Timer (RAT) channel in capture mode.
Default priority. Use this in single-client applications.
Definition: RFCC26X2.h:1119
RF_CmdHandle ch
Definition: RFCC26X2.h:1638
Provide the client list.
Definition: RFCC26X2.h:1460
RF_Priority ePri
Definition: RFCC26X2.h:1639
RF_EndType endType
End type for the end time.
Definition: RFCC26X2.h:1757
RF_CoexOverride bleObserver
Definition: RFCC26X2.h:1175
Definition: rf_common_cmd.h:112
RF_RatOutputMode
Selects the mode of the RAT_GPO[x] for RF_ratCompare() or RF_ratCapture().
Definition: RFCC26X2.h:1840
RAT related IO parameter structure.
Definition: RFCC26X2.h:1895
High-power PA.
Definition: RFCC26X2.h:1071
RF_CmdHandle ch
Command handle.
Definition: RFCC26X2.h:1482
Inverts the polarity of the output.
Definition: RFCC26X2.h:1844
RF_RequestCoex request
Behavior for coexistence request signal.
Definition: RFCC26X2.h:1162
RF_InfoType
Selects the entry of interest in RF_getInfo().
Definition: RFCC26X2.h:1455
uint32_t startTime
Start time in RAT Ticks for the radio command.
Definition: RFCC26X2.h:1750
RF_Priority priority
Priority of the command or access request.
Definition: RFCC26X2.h:1486
Definition: RFCC26X2.h:1256
RF_Stat RF_flushCmd(RF_Handle h, RF_CmdHandle ch, uint8_t mode)
Abort/stop/cancel command and any subsequent commands in command queue.
RF_StartType
Controls the behavior of the RF_scheduleCmd() API.
Definition: RFCC26X2.h:1611
void RF_RatConfigCompare_init(RF_RatConfigCompare *channelConfig)
Initialize the configuration structure to be used to set up a RAT compare event.
Definition: RFCC26X2.h:1683
RF_ratCapture parameter structure.
Definition: RFCC26X2.h:1872
Definition: rf_prop_cmd.h:902
Runtime coexistence override parameters.
Definition: RFCC26X2.h:1160
Falling edge of the selected source will trigger a capture event.
Definition: RFCC26X2.h:1810
bool bRadioState
Current RF core power state (RF_GET_RADIO_STATE).
Definition: RFCC26X2.h:1472
RF_RatCaptureMode
Selects the mode of RF_ratCapture().
Definition: RFCC26X2.h:1808
RF_RatOutputSelect select
The signal which shall be connected to the GPO.
Definition: RFCC26X2.h:1897
RF_EndType
Controls the behavior of the RF_scheduleCmd() API.
Definition: RFCC26X2.h:1619
void(* RF_Callback)(RF_Handle h, RF_CmdHandle ch, RF_EventMask e)
Handles events related to RF command execution.
Definition: RFCC26X2.h:1522
RF_CmdHandle RF_scheduleCmd(RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
Schedule an RF operation (chain) to the command queue.
Proprietary Mode Radio Setup Command for 2.4 GHz.
Definition: rf_prop_cmd.h:455
#define RF_NUM_SCHEDULE_COMMAND_ENTRIES
Number of scheduled command entries.
Definition: RFCC26X2.h:957
Definition: rf_common_cmd.h:681
uint32_t endTime
Definition: RFCC26X2.h:1644
uint32_t activityInfo
Activity info provided by user.
Definition: RFCC26X2.h:1759
RF_ScheduleStatus RF_defaultSubmitPolicy(RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue)
Sorts and adds commands to the RF driver internal command queue.
uint32_t duration
Radio access duration in RAT Ticks requested by the client.
Definition: RFCC26X2.h:1769
Command successfully scheduled for execution.
Definition: RFCC26X2.h:1194
RF_RatCaptureSource source
Configuration of the event source to cause a capture event.
Definition: RFCC26X2.h:1875
Configure RAT_CHANNEL[x] to interface with RAT_GPO[6].
Definition: RFCC26X2.h:1864
Radio Setup Command for Pre-Defined Schemes.
Definition: rf_common_cmd.h:176
RF_RatCaptureRepetition repeat
Configuration of the channel to be used in single or repeated mode.
Definition: RFCC26X2.h:1877
Proprietary Mode Radio Setup Command for All Frequency Bands.
Definition: rf_prop_cmd.h:561
Command not executed because RF core is powered down.
Definition: RFCC26X2.h:1188
uint32_t startTime
Start time (in RAT tick) of the command or access request.
Definition: RFCC26X2.h:1484
Do not assert REQUEST in RX. Override default value configured by setup command.
Definition: RFCC26X2.h:1151
RF_GlobalCallback globalCallback
Pointer to a callback function serving client independent events listed in RF_GlobalEvent.
Definition: RFCC26X2.h:1661
RF_TxPowerTable_PAType
Selects a power amplifier path in a TX power value.
Definition: RFCC26X2.h:1069
RF_RequestCoex coexRequest
REQUEST line behavior to use for coexistence request.
Definition: RFCC26X2.h:1761
RF_CoexOverride bleBroadcaster
Definition: RFCC26X2.h:1174
RF_Stat RF_control(RF_Handle h, int8_t ctrl, void *args)
Set RF control parameters.
Definition: RFCC26X2.h:1612
Selects the Generic event of Event Fabric as source.
Definition: RFCC26X2.h:1794
void RF_yield(RF_Handle h)
Signal that radio client is not going to issue more commands in a while.
Definition: RFCC26X2.h:1749
Definition: RFCC26X2.h:1680
Definition: RFCC26X2.h:1682
The RF core has been powered up the radio setup has been finished.
Definition: RFCC26X2.h:1255
void(* RF_ClientCallback)(RF_Handle h, RF_ClientEvent event, void *arg)
Handles events related to a driver instance.
Definition: RFCC26X2.h:1554
Deprecated. Not supported.
Definition: RFCC26X2.h:1459
Signals the client that the RF driver is about to switch over from another client.
Definition: RFCC26X2.h:1260
RF_PriorityCoex coexPriority
Priority to use for coexistence request.
Definition: RFCC26X2.h:1760
RF_Callback pPowerCb
Definition: RFCC26X2.h:1587
RF_StartType startType
Start type for the start time.
Definition: RFCC26X2.h:1751
RF_Stat RF_getInfo(RF_Handle h, RF_InfoType type, RF_InfoVal *pValue)
Get value for some RF driver parameters.
rfc_radioOp_t RF_Op
Base type for all radio operation commands.
Definition: RFCC26X2.h:1088
High priority. Use this for time-critical commands in synchronous protocols.
Definition: RFCC26X2.h:1118
int16_t RF_CmdHandle
Command handle that is returned by RF_postCmd().
Definition: RFCC26X2.h:1373
General error specifier.
Definition: RFCC26X2.h:1192
Definition: RFCC26X2.h:1685
RF_ClientCallback pClientEventCb
Definition: RFCC26X2.h:1599
void RF_RatConfigCapture_init(RF_RatConfigCapture *channelConfig)
Initialize the configuration structure to be used to set up a RAT capture event.
RF_Stat RF_runDirectCmd(RF_Handle h, uint32_t cmd)
Send any Direct command.
Definition: RFCC26X2.h:1341
uint16_t availRatCh
Available RAT channels (RF_GET_AVAIL_RAT_CH).
Definition: RFCC26X2.h:1471
RF_GlobalEvent
Global RF driver events.
Definition: RFCC26X2.h:1324
RF_Object * RF_Handle
A handle that is returned by to RF_open().
Definition: RFCC26X2.h:1439
rfc_CMD_BLE5_RADIO_SETUP_PA_t ble5_pa
Radio setup command for BLE5 mode with High Gain PA.
Definition: RFCC26X2.h:1221
RF_Priority
Scheduling priority of RF operation commands.
Definition: RFCC26X2.h:1116
RF_PriorityCoex coexPriority
Definition: RFCC26X2.h:1648
Definition: RFCC26X2.h:1623
RF_Stat
Status codes for various RF driver functions.
Definition: RFCC26X2.h:1186
Definition: rf_ble_cmd.h:1516
Definition: RFCC26X2.h:1681
RF_Stat RF_cancelCmd(RF_Handle h, RF_CmdHandle ch, uint8_t mode)
Abort/stop/cancel single command in command queue.
Definition: RFCC26X2.h:1795
uint32_t timeout
Definition: RFCC26X2.h:1887
Definition: RFCC26X2.h:1337
uint32_t startTime
Definition: RFCC26X2.h:1641
uint32_t endTime
End time (in RAT tick) of the command or access request.
Definition: RFCC26X2.h:1485
Definition: rf_prop_cmd.h:1013
Use RAT user channel 1.
Definition: RFCC26X2.h:1783
RF_RatCaptureRepetition
Selects the repetition of RF_ratCapture().
Definition: RFCC26X2.h:1821
int8_t power
Definition: RFCC26X2.h:1056
RF_ClientEvent
Client-related RF driver events.
Definition: RFCC26X2.h:1254
RF_RatCaptureSource
Selects the source signal for RF_ratCapture().
Definition: RFCC26X2.h:1792
Provide the client to client switching times.
Definition: RFCC26X2.h:1461
RF request access parameter struct.
Definition: RFCC26X2.h:1768
Bluetooth 5 Radio Setup Command for all PHYs.
Definition: rf_ble_cmd.h:702
int8_t RF_RatHandle
RAT handle that is returned by RF_ratCompare() or RF_ratCapture().
Definition: RFCC26X2.h:1450
Use RAT user channel 2.
Definition: RFCC26X2.h:1784
RF_RatOutputMode mode
The mode the GPO should operate in.
Definition: RFCC26X2.h:1896
RF_CoexOverride bleConnected
Definition: RFCC26X2.h:1173
Default priority. Use value configured by setup command.
Definition: RFCC26X2.h:1133
uint32_t RF_ClientEventMask
Event mask for combining RF_ClientEvent event flags in RF_Params::nClientEventMask.
Definition: RFCC26X2.h:1354
RF_EventMask RF_runScheduleCmd(RF_Handle h, RF_Op *pOp, RF_ScheduleCmdParams *pSchParams, RF_Callback pCb, RF_EventMask bmEvent)
Runs synchronously a (chain of) RF operation(s) for dual or single-mode.
Configure RAT_CHANNEL[x] to interface with RAT_GPO[7].
Definition: RFCC26X2.h:1865
Definition: RFCC26X2.h:1329
Sets the output low independently of any RAT events.
Definition: RFCC26X2.h:1845
TX power configuration entry in a TX power table.
Definition: RFCC26X2.h:1054
Sets the output high independently of any RAT events.
Definition: RFCC26X2.h:1846
uint32_t activityInfo
Definition: RFCC26X2.h:1647
RF_Stat RF_runImmediateCmd(RF_Handle h, uint32_t *pCmdStruct)
Send any Immediate command.
A unified type for radio setup commands of different PHYs.
Definition: RFCC26X2.h:1213
void(* RF_RatCallback)(RF_Handle h, RF_RatHandle rh, RF_EventMask e, uint32_t compareCaptureTime)
Handles events related to the Radio Timer (RAT).
Definition: RFCC26X2.h:1537
RF_TxPowerTable_Value value
PA hardware configuration for that power level.
Definition: RFCC26X2.h:1059
RF_Op * pOp
Definition: RFCC26X2.h:1633
uint32_t nInactivityTimeout
Definition: RFCC26X2.h:1580
Abort the incoming command, letting the ongoing command finish.
Definition: RFCC26X2.h:1672
RF schedule map structure.
Definition: RFCC26X2.h:1492
RF_ScheduleStatus(* RF_SubmitHook)(RF_Cmd *pCmdNew, RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue)
Handles the queue sorting algorithm when a new command is submitted to the driver from any of the act...
Definition: RFCC26X2.h:1706
RF_ratCompare parameter structure.
Definition: RFCC26X2.h:1884
RF_EventMask pastifg
Definition: RFCC26X2.h:1636
RF_SubmitHook submitHook
Function hook implements the scheduling policy to be executed at the time of RF_scheduleCmd API call...
Definition: RFCC26X2.h:1733
Sets the output low on a RAT event.
Definition: RFCC26X2.h:1843
uint32_t duration
Definition: RFCC26X2.h:1646
Configure RAT_CHANNEL[x] to interface with RAT_GPO[3].
Definition: RFCC26X2.h:1861
RF_CoexOverride bleInitiator
Definition: RFCC26X2.h:1172
rfc_CMD_PROP_RADIO_DIV_SETUP_PA_t prop_div_pa
Radio setup command for PROPRIETARY mode on Sub-1 Ghz with High Gain PA.
Definition: RFCC26X2.h:1223
Assert REQUEST in RX. Override default value configured by setup command.
Definition: RFCC26X2.h:1150
RF_RequestCoex
Behavior for coexistence request signal.
Definition: RFCC26X2.h:1148
Command finished with success.
Definition: RFCC26X2.h:1193
Function finished with success.
Definition: RFCC26X2.h:1195
int8_t RF_TxPowerTable_findPowerLevel(RF_TxPowerTable_Entry table[], RF_TxPowerTable_Value value)
Retrieves a power level in dBm for a given power configuration value.
Definition: RFCC26X2.h:1811
RF_RatHandle RF_ratCompare(RF_Handle rfHandle, RF_RatConfigCompare *channelConfig, RF_RatConfigOutput *ioConfig)
Setup a Radio Timer (RAT) channel in compare mode.
RF_RatHandle channel
RF_RatHandle identifies the channel to be allocated.
Definition: RFCC26X2.h:1886
Abort the ongoing command and run dispatcher again.
Definition: RFCC26X2.h:1673
bool xoscHfAlwaysNeeded
Indicate that the XOSC HF should be turned on by the power driver.
Definition: RFCC26X2.h:1660
Rearm the channel after each capture events.
Definition: RFCC26X2.h:1823
Sets the output high on a RAT event.
Definition: RFCC26X2.h:1842
Configure RAT_CHANNEL[x] to interface with RAT_GPO[1].
Definition: RFCC26X2.h:1859
Show the current RF core power state. 0: Radio OFF, 1: Radio ON.
Definition: RFCC26X2.h:1458
RF_ExecuteAction RF_defaultExecutionPolicy(RF_Cmd *pCmdBg, RF_Cmd *pCmdFg, List_List *pPendQueue, List_List *pDoneQueue, bool bConflict, RF_Cmd *conflictCmd)
Makes a final decision before dispatching a scheduled command.
RF_RequestCoex coexRequest
Definition: RFCC26X2.h:1649
RF_RatSelectChannel
Select the preferred RAT channel through the configuration of RF_ratCompare() or RF_ratCapture().
Definition: RFCC26X2.h:1780
RF scheduler policy.
Definition: RFCC26X2.h:1732
void RF_Params_init(RF_Params *params)
Function to initialize the RF_Params struct to its defaults.
Definition: rf_common_cmd.h:122
Specifies a RF core firmware configuration.
Definition: RFCC26X2.h:1099
uint32_t nID
RF handle identifier.
Definition: RFCC26X2.h:1605
RF_Object * pClient
Definition: RFCC26X2.h:1634
rfc_command_t commandId
Definition: RFCC26X2.h:1214
Definition: RFCC26X2.h:1684
rfc_CMD_PROP_RADIO_SETUP_t prop
Radio setup command for PROPRIETARY mode on 2.4 GHz.
Definition: RFCC26X2.h:1218
rfc_CMD_BLE5_RADIO_SETUP_t ble5
Radio setup command for BLE5 mode.
Definition: RFCC26X2.h:1217
PA configuration value for a certain power level.
Definition: RFCC26X2.h:1024
RF_RatCallback callback
Callback function to be invoked upon a capture event (optional).
Definition: RFCC26X2.h:1873
Definition: RFCC26X2.h:1613
Command not executed because RF driver is busy.
Definition: RFCC26X2.h:1187
RF_Stat RF_ratDisableChannel(RF_Handle rfHandle, RF_RatHandle ratHandle)
Disable a RAT channel.
RF_Callback pErrCb
Definition: RFCC26X2.h:1590
uint8_t hwiPriority
Priority for HWIs belong to the RF driver.
Definition: RFCC26X2.h:1658
RF_TxPowerTable_Value RF_getTxPower(RF_Handle h)
Returns the currently configured transmit power configuration.
uint16_t nPhySwitchingDurationMargin
An additional safety margin to be used to calculate when conflicts shall be evaluated run-time...
Definition: RFCC26X2.h:1597
RF_EventMask bmEvent
Definition: RFCC26X2.h:1635
uint32_t RF_GlobalEventMask
Event mask for combining RF_GlobalEvent event flags in RFCC26XX_HWAttrsV2::globalEventMask.
Definition: RFCC26X2.h:1359
Stores the client's internal configuration and states.
RF_Priority priority
Access priority.
Definition: RFCC26X2.h:1771
uint64_t RF_EventMask
Data type for events during command execution.
Definition: RFCC26X2.h:1202
void * pScheduleMap
Deprecated. Not supported.
Definition: RFCC26X2.h:1475
RF_PriorityCoex
Priority level for coexistence priority signal.
Definition: RFCC26X2.h:1132
Default request line behavior. Use value configured by setup command.
Definition: RFCC26X2.h:1149