48 #if !defined ( GAP_BONDINGS_MAX ) 49 #define GAP_BONDINGS_MAX 10 53 #if !defined ( GAP_CHAR_CFG_MAX ) 54 #define GAP_CHAR_CFG_MAX 4 78 #define GAPBOND_PAIRING_MODE 0x400 89 #define GAPBOND_MITM_PROTECTION 0x402 100 #define GAPBOND_IO_CAPABILITIES 0x403 111 #define GAPBOND_OOB_ENABLED 0x404 123 #define GAPBOND_OOB_DATA 0x405 134 #define GAPBOND_BONDING_ENABLED 0x406 148 #define GAPBOND_KEY_DIST_LIST 0x407 155 #define GAPBOND_ERASE_ALLBONDS 0x409 158 #define GAPBOND_AUTO_FAIL_PAIRING 0x40A 159 #define GAPBOND_AUTO_FAIL_REASON 0x40B 171 #define GAPBOND_KEYSIZE 0x40C 186 #define GAPBOND_AUTO_SYNC_WL 0x40D 195 #define GAPBOND_BOND_COUNT 0x40E 207 #define GAPBOND_BOND_FAIL_ACTION 0x40F 218 #define GAPBOND_ERASE_SINGLEBOND 0x410 233 #define GAPBOND_SECURE_CONNECTION 0x411 253 #define GAPBOND_ECCKEY_REGEN_POLICY 0x412 276 #define GAPBOND_ECC_KEYS 0x413 287 #define GAPBOND_SC_HOST_DEBUG 0x414 302 #define GAPBOND_LRU_BOND_REPLACEMENT 0x418 312 #define GAPBOND_ERASE_LOCAL_INFO 0x41A 324 #define GAPBOND_PAIRING_MODE_NO_PAIRING 0x00 326 #define GAPBOND_PAIRING_MODE_WAIT_FOR_REQ 0x01 328 #define GAPBOND_PAIRING_MODE_INITIATE 0x02 336 #define GAPBOND_IO_CAP_DISPLAY_ONLY 0x00 338 #define GAPBOND_IO_CAP_DISPLAY_YES_NO 0x01 340 #define GAPBOND_IO_CAP_KEYBOARD_ONLY 0x02 342 #define GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT 0x03 344 #define GAPBOND_IO_CAP_KEYBOARD_DISPLAY 0x04 352 #define GAPBOND_KEYDIST_SENCKEY 0x01 354 #define GAPBOND_KEYDIST_SIDKEY 0x02 356 #define GAPBOND_KEYDIST_SSIGN 0x04 358 #define GAPBOND_KEYDIST_SLINK 0x08 360 #define GAPBOND_KEYDIST_MENCKEY 0x10 362 #define GAPBOND_KEYDIST_MIDKEY 0x20 364 #define GAPBOND_KEYDIST_MSIGN 0x40 366 #define GAPBOND_KEYDIST_MLINK 0x80 387 #define GAPBOND_PAIRING_STATE_STARTED 0x00 408 #define GAPBOND_PAIRING_STATE_COMPLETE 0x01 427 #define GAPBOND_PAIRING_STATE_ENCRYPTED 0x02 428 #define GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 430 #define GAPBOND_PAIRING_STATE_CAR_READ 0x04 432 #define GAPBOND_PAIRING_STATE_RPAO_READ 0x05 434 #define GAPBOND_GENERATE_ECC_DONE 0x06 451 #define SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED 0x01 452 #define SMP_PAIRING_FAILED_OOB_NOT_AVAIL 0x02 458 #define SMP_PAIRING_FAILED_AUTH_REQ 0x03 459 #define SMP_PAIRING_FAILED_CONFIRM_VALUE 0x04 461 #define SMP_PAIRING_FAILED_NOT_SUPPORTED 0x05 467 #define SMP_PAIRING_FAILED_ENC_KEY_SIZE 0x06 468 #define SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED 0x07 470 #define SMP_PAIRING_FAILED_UNSPECIFIED 0x08 476 #define SMP_PAIRING_FAILED_REPEATED_ATTEMPTS 0x09 481 #define SMP_PAIRING_FAILED_INVALID_PARAMETERS 0x0A 486 #define SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED 0x0B 491 #define SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED 0x0C 498 #define GAPBOND_FAIL_NO_ACTION 0x00 500 #define GAPBOND_FAIL_INITIATE_PAIRING 0x01 502 #define GAPBOND_FAIL_TERMINATE_LINK 0x02 508 #define GAPBOND_FAIL_TERMINATE_ERASE_BONDS 0x03 515 #define GAPBOND_SECURE_CONNECTION_NONE 0x00 517 #define GAPBOND_SECURE_CONNECTION_ALLOW 0x01 519 #define GAPBOND_SECURE_CONNECTION_ONLY 0x02 531 #define GAPBOND_REGENERATE_ALWAYS 0x00 533 #define GAPBOND_REGENERATE_NEVER 0xFF 537 #define ECC_KEYLEN 32 572 uint16_t connectionHandle,
575 uint32_t numComparison
591 uint16_t connectionHandle,
624 typedef struct gapBondOOBData
729 uint8_t *pIdentityAddr);
761 uint8_t status, uint32_t passcode);
775 extern bStatus_t GAPBondMgr_SCGetLocalOOBParameters(gapBondOOBData_t *localOobData);
791 extern bStatus_t GAPBondMgr_SCSetRemoteOOBParameters(gapBondOOBData_t *remoteOobData,
804 extern bStatus_t GAPBondMgr_GenerateEccKeys(
void );
GAP_Peer_Addr_Types_t
Address types used for specifying peer address type.
Definition: gap.h:598
Public and Private ECC Keys.
Definition: gapbondmgr.h:616
bStatus_t GAPBondMgr_Pair(uint16_t connHandle)
bStatus_t GAPBondMgr_GetParameter(uint16_t param, void *pValue)
bStatus_t GAPBondMgr_PasscodeRsp(uint16_t connectionHandle, uint8_t status, uint32_t passcode)
void(* pfnPairStateCB_t)(uint16_t connectionHandle, uint8_t state, uint8_t status)
Definition: gapbondmgr.h:590
pfnPasscodeCB_t passcodeCB
Passcode callback.
Definition: gapbondmgr.h:604
bStatus_t GAPBondMgr_FindAddr(uint8_t *pDevAddr, GAP_Peer_Addr_Types_t addrType, uint8_t *pIdx, GAP_Peer_Addr_Types_t *pIdentityAddrType, uint8_t *pIdentityAddr)
Search for an address in the bonding table. If the address is a random private resolvable address...
void GAPBondMgr_Register(gapBondCBs_t *pCB)
Definition: gapbondmgr.h:602
void(* pfnPasscodeCB_t)(uint8_t *deviceAddr, uint16_t connectionHandle, uint8_t uiInputs, uint8_t uiOutputs, uint32_t numComparison)
Definition: gapbondmgr.h:570
bStatus_t GAPBondMgr_ServiceChangeInd(uint16_t connectionHandle, uint8_t setParam)
bStatus_t GAPBondMgr_SetParameter(uint16_t param, uint8_t len, void *pValue)
Status_t bStatus_t
BLE Generic Status return.
Definition: bcomdef.h:246
#define ECC_KEYLEN
ECC Key Length: 256 bit keys.
Definition: gapbondmgr.h:538
#define KEYLEN
Default key length.
Definition: bcomdef.h:111
pfnPairStateCB_t pairStateCB
Pairing state callback.
Definition: gapbondmgr.h:605