![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.02.00
|
ATT layer interface.
Go to the source code of this file.
Data Structures | |
struct | attAttrBtType_t |
Attribute Type format (2-octet Bluetooth UUID). More... | |
struct | attAttrType_t |
Attribute Type format (2 or 16 octet UUID). More... | |
struct | attErrorRsp_t |
Error Response format. More... | |
struct | attExchangeMTUReq_t |
Exchange MTU Request format. More... | |
struct | attExchangeMTURsp_t |
Exchange MTU Response format. More... | |
struct | attExecuteWriteReq_t |
Execute Write Request format. More... | |
struct | attFindByTypeValueReq_t |
Find By Type Value Request format. More... | |
struct | attFindByTypeValueRsp_t |
Find By Type Value Response format. More... | |
struct | attFindInfoReq_t |
Find Information Request format. More... | |
struct | attFindInfoRsp_t |
Find Information Response format. More... | |
struct | attFlowCtrlViolatedEvt_t |
ATT Flow Control Violated Event message format. More... | |
struct | attHandleBtUUID_t |
Handle and its 16-bit Bluetooth UUIDs. More... | |
struct | attHandlesInfo_t |
Handles Information format. More... | |
struct | attHandleUUID_t |
Handle and its 128-bit UUID. More... | |
struct | attHandleValueInd_t |
Handle Value Indication format. More... | |
struct | attHandleValueNoti_t |
Handle Value Notification format. More... | |
union | attMsg_t |
ATT Message format. More... | |
struct | attMtuUpdatedEvt_t |
ATT MTU Updated Event message format. More... | |
struct | attPacket_t |
Attribute Protocol PDU format. More... | |
struct | attPrepareWriteReq_t |
Prepare Write Request format. More... | |
struct | attPrepareWriteRsp_t |
Prepare Write Response format. More... | |
struct | attReadBlobReq_t |
Read Blob Request format. More... | |
struct | attReadBlobRsp_t |
Read Blob Response format. More... | |
struct | attReadByGrpTypeReq_t |
Read By Group Type Request format. More... | |
struct | attReadByGrpTypeRsp_t |
Read By Group Type Response format. More... | |
struct | attReadByTypeReq_t |
Read By Type Request format. More... | |
struct | attReadByTypeRsp_t |
Read By Type Response format. More... | |
struct | attReadMultiReq_t |
Read Multiple Request format. More... | |
struct | attReadMultiRsp_t |
Read Multiple Response format. More... | |
struct | attReadReq_t |
Read Request. More... | |
struct | attReadRsp_t |
Read Response. More... | |
struct | attWriteReq_t |
Write Request format. More... | |
Macros | |
#define | ATT_AUTHEN_SIG_FLAG_BIT 0x80 |
Authentication Signature Flag (bit 7) | |
#define | ATT_AUTHEN_SIG_LEN 12 |
Length of Authentication Signature field. | |
#define | ATT_BT_UUID_SIZE 2 |
Size of 16-bit Bluetooth UUID. | |
#define | ATT_CANCEL_PREPARED_WRITES 0x00 |
Cancel all prepared writes. | |
#define | ATT_CMD_FLAG_BIT 0x40 |
Command Flag (bit 6) | |
#define | ATT_ERR_ATTR_NOT_FOUND 0x0a |
No attribute found within the given attribute handle range. | |
#define | ATT_ERR_ATTR_NOT_LONG 0x0b |
Attribute cannot be read or written using the Read Blob Request or Prepare Write Request. | |
#define | ATT_ERR_INSUFFICIENT_AUTHEN 0x05 |
The attribute requires authentication before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_AUTHOR 0x08 |
The attribute requires an authorization before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_ENCRYPT 0x0f |
The attribute requires encryption before it can be read or written. | |
#define | ATT_ERR_INSUFFICIENT_KEY_SIZE 0x0c |
The Encryption Key Size used for encrypting this link is insufficient. | |
#define | ATT_ERR_INSUFFICIENT_RESOURCES 0x11 |
Insufficient Resources to complete the request. | |
#define | ATT_ERR_INVALID_HANDLE 0x01 |
Attribute handle value given was not valid on this attribute server. | |
#define | ATT_ERR_INVALID_OFFSET 0x07 |
Offset specified was past the end of the attribute. | |
#define | ATT_ERR_INVALID_PDU 0x04 |
The attribute PDU was invalid. | |
#define | ATT_ERR_INVALID_VALUE 0x80 |
The attribute value is invalid for the operation. | |
#define | ATT_ERR_INVALID_VALUE_SIZE 0x0d |
The attribute value length is invalid for the operation. | |
#define | ATT_ERR_PREPARE_QUEUE_FULL 0x09 |
Too many prepare writes have been queued. | |
#define | ATT_ERR_READ_NOT_PERMITTED 0x02 |
Attribute cannot be read. | |
#define | ATT_ERR_UNLIKELY 0x0e |
The attribute request that was requested has encountered an error that was very unlikely, and therefore could not be completed as requested. | |
#define | ATT_ERR_UNSUPPORTED_GRP_TYPE 0x10 |
The attribute type is not a supported grouping attribute as defined by a higher layer specification. | |
#define | ATT_ERR_UNSUPPORTED_REQ 0x06 |
Attribute server doesn't support the request received from the attribute client. | |
#define | ATT_ERR_WRITE_NOT_PERMITTED 0x03 |
Attribute cannot be written. | |
#define | ATT_ERROR_RSP 0x01 |
ATT Error Response. This method is passed as a gattMsgEvent_t defined as attErrorRsp_t. | |
#define | ATT_ERROR_RSP_SIZE 4 |
Length of Error Response: Command opcode in error (1) + Attribute handle in error (2) + Status code (1) | |
#define | ATT_EXCHANGE_MTU_REQ 0x02 |
ATT Exchange MTU Request. This method is passed as a GATT message defined as attExchangeMTUReq_t. | |
#define | ATT_EXCHANGE_MTU_REQ_SIZE 2 |
Length of Exchange MTU Request: client receive MTU size (2) | |
#define | ATT_EXCHANGE_MTU_RSP 0x03 |
ATT Exchange MTU Response. This method is passed as a GATT message defined as attExchangeMTURsp_t. | |
#define | ATT_EXCHANGE_MTU_RSP_SIZE 2 |
Length of Exchange MTU Response: server receive MTU size (2) | |
#define | ATT_EXECUTE_WRITE_REQ 0x18 |
ATT Execute Write Request. This method is passed as a GATT message defined as attExecuteWriteReq_t. | |
#define | ATT_EXECUTE_WRITE_REQ_SIZE 1 |
Length of Execute Write Request: Flags (1) | |
#define | ATT_EXECUTE_WRITE_RSP 0x19 |
ATT Execute Write Response. This method is passed as a GATT message defines as attHandleValueNoti_t. | |
#define | ATT_FIND_BY_TYPE_VALUE_REQ 0x06 |
ATT Find By Type Value Request. This method is passed as a GATT message defined as attFindByTypeValueReq_t. | |
#define | ATT_FIND_BY_TYPE_VALUE_REQ_FIXED_SIZE 6 |
Length of Find By Type Value Request's fixed fields: Start handle (2) + End handle (2) + Type (2) | |
#define | ATT_FIND_BY_TYPE_VALUE_REQ_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_FIND_BY_TYPE_VALUE_REQ_FIXED_SIZE ) |
Length of Find By Type Value Request's Header. | |
#define | ATT_FIND_BY_TYPE_VALUE_RSP 0x07 |
ATT Find By Type Value Response. This method is passed as a GATT message defined as attFindByTypeValueRsp_t. | |
#define | ATT_FIND_INFO_REQ 0x04 |
ATT Find Information Request. This method is passed as a GATT message defined as attFindInfoReq_t. | |
#define | ATT_FIND_INFO_REQ_FIXED_SIZE 4 |
Length of Find Information Request's fixed fields: First handle number (2) + Last handle number (2) | |
#define | ATT_FIND_INFO_RSP 0x05 |
ATT Find Information Response. This method is passed as a GATT message defined as attFindInfoRsp_t. | |
#define | ATT_FIND_INFO_RSP_FIXED_SIZE 1 |
Length of Find Information Response's fixed field: Format (1) | |
#define | ATT_FIND_INFO_RSP_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_FIND_INFO_RSP_FIXED_SIZE ) |
Length of Find Information Response's Header. | |
#define | ATT_FLOW_CTRL_VIOLATED_EVENT 0x7E |
Sent when ATT flow control is violated on a connection. This event is sent as an OSAL message defined as attFlowCtrlViolatedEvt_t. | |
#define | ATT_HANDLE_BT_UUID_TYPE 0x01 |
Handle and 16-bit Bluetooth UUID. | |
#define | ATT_HANDLE_UUID_TYPE 0x02 |
Handle and 128-bit UUID. | |
#define | ATT_HANDLE_VALUE_CFM 0x1e |
ATT Handle Value Confirmation. This method is passed as a GATT message. | |
#define | ATT_HANDLE_VALUE_IND 0x1d |
ATT Handle Value Indication. This method is passed as a GATT message defined as attHandleValueInd_t. | |
#define | ATT_HANDLE_VALUE_IND_FIXED_SIZE 2 |
Length of Handle Value Indication's fixed size: Attribute Handle (2) | |
#define | ATT_HANDLE_VALUE_IND_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_HANDLE_VALUE_IND_FIXED_SIZE ) |
Size of Indication header. | |
#define | ATT_HANDLE_VALUE_NOTI 0x1b |
ATT Handle Value Notification. This method is passed as a GATT message defined as attErrorRsp_t. | |
#define | ATT_MAX_MTU_SIZE (255-L2CAP_HDR_SIZE) |
Maximum ATT MTU size. | |
#define | ATT_METHOD_BITS 0x3f |
Method (bits 5-0) | |
#define | ATT_MIN_NUM_HANDLES 2 |
Minimum number of handles in a single Read Multiple Request. | |
#define | ATT_MSG_TIMEOUT 30 |
ATT Response or Confirmation timeout. | |
#define | ATT_MTU_SIZE L2CAP_MTU_SIZE |
Minimum ATT MTU size. | |
#define | ATT_MTU_UPDATED_EVENT 0x7F |
Sent when MTU is updated for a connection. This event is sent as an OSAL message defined as attMtuUpdatedEvt_t. | |
#define | ATT_OPCODE_SIZE 1 |
Length of opcode field: Opcode (1) | |
#define | ATT_PREPARE_WRITE_REQ 0x16 |
ATT Prepare Write Request. This method is passed as a GATT message defined as attPrepareWriteReq_t. | |
#define | ATT_PREPARE_WRITE_REQ_FIXED_SIZE 4 |
Length of Prepare Write Request's fixed fields: Attribute Handle (2) + Value Offset (2) | |
#define | ATT_PREPARE_WRITE_REQ_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_PREPARE_WRITE_REQ_FIXED_SIZE ) |
Size of Prepare Write Request Header. | |
#define | ATT_PREPARE_WRITE_RSP 0x17 |
ATT Prepare Write Response. This method is passed as a GATT message defined as attPrepareWriteRsp_t. | |
#define | ATT_PREPARE_WRITE_RSP_FIXED_SIZE 4 |
Length of Prepare Write Response's fixed size: Attribute Handle (2) + Value Offset (2) | |
#define | ATT_READ_BLOB_REQ 0x0c |
ATT Read Blob Request. This method is passed as a GATT message defined as attReadBlobReq_t. | |
#define | ATT_READ_BLOB_REQ_SIZE 4 |
Length of Read Blob Request: Attribute Handle (2) + Value Offset (2) | |
#define | ATT_READ_BLOB_RSP 0x0d |
ATT Read Blob Response. This method is passed as a GATT message defined as attReadBlobRsp_t. | |
#define | ATT_READ_BY_GRP_TYPE_REQ 0x10 |
ATT Read By Group Type Request. This method is passed as a GATT message defined as attReadByGrpTypeReq_t. | |
#define | ATT_READ_BY_GRP_TYPE_RSP 0x11 |
ATT Read By Group Type Response. This method is passed as a GATT message defined as attReadByGrpTypeRsp_t. | |
#define | ATT_READ_BY_GRP_TYPE_RSP_FIXED_SIZE 1 |
Length of Read By Type Response's fixed fields: Length (1) | |
#define | ATT_READ_BY_GRP_TYPE_RSP_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_READ_BY_GRP_TYPE_RSP_FIXED_SIZE ) |
Size of Read by Group Type Response Header. | |
#define | ATT_READ_BY_TYPE_REQ 0x08 |
ATT Read By Type Request. This method is passed as a GATT message defined as attReadByTypeReq_t. | |
#define | ATT_READ_BY_TYPE_REQ_FIXED_SIZE 4 |
Length of Read By Type Request's fixed fields: First handle number (2) + Last handle number (2) | |
#define | ATT_READ_BY_TYPE_REQ_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_READ_BY_TYPE_REQ_FIXED_SIZE ) |
Size of Read by Type Request Header. | |
#define | ATT_READ_BY_TYPE_RSP 0x09 |
ATT Read By Type Response. This method is passed as a GATT message defined as attReadByTypeRsp_t. | |
#define | ATT_READ_BY_TYPE_RSP_FIXED_SIZE 1 |
Length of Read By Type Response's fixed fields: Length (1) | |
#define | ATT_READ_BY_TYPE_RSP_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_READ_BY_TYPE_RSP_FIXED_SIZE ) |
Size of Read by Type Response Header. | |
#define | ATT_READ_MULTI_REQ 0x0e |
ATT Read Multiple Request. This method is passed as a GATT message defined as attReadMultiReq_t. | |
#define | ATT_READ_MULTI_RSP 0x0f |
ATT Read Multiple Response. This method is passed as a GATT message defined as attReadMultiRsp_t. | |
#define | ATT_READ_REQ 0x0a |
ATT Read Request. This method is passed as a GATT message defined as attReadReq_t. | |
#define | ATT_READ_REQ_SIZE 2 |
Length of Read Request: Attribute Handle (2) | |
#define | ATT_READ_RSP 0x0b |
ATT Read Response. This method is passed as a GATT message defined as attReadRsp_t. | |
#define | ATT_SIG_INVALID 0x02 |
Included signature not valid. | |
#define | ATT_SIG_NOT_INCLUDED 0x00 |
Signature not included. | |
#define | ATT_SIG_VALID 0x01 |
Included signature valid. | |
#define | ATT_SIGNED_WRITE_CMD 0xD2 |
ATT Signed Write Command. | |
#define | ATT_TRANSACTION_READY_EVENT 0x7D |
ATT transaction ready on the specified connection handle. This event is sent as an OSAL message defined as attTransactionReadyEvt_t. | |
#define | ATT_UNSUPPORTED_METHOD 0x20 |
Garbage ATT opcode used for negative testing. | |
#define | ATT_UUID_SIZE 16 |
Size of 128-bit UUID. | |
#define | ATT_WRITE_CMD 0x52 |
ATT Write Command. | |
#define | ATT_WRITE_COMMAND(method, cmd) ( ( (method) == ATT_WRITE_REQ ) && ( (cmd) == TRUE ) ) |
ATT Write Command. | |
#define | ATT_WRITE_PREPARED_VALUES 0x01 |
Immediately write all pending prepared values. | |
#define | ATT_WRITE_REQ 0x12 |
ATT Write Request. This method is passed as a GATT message defined as attWriteReq_t. | |
#define | ATT_WRITE_REQ_FIXED_SIZE 2 |
Length of Write Request's fixed field: Attribute Handle (2) | |
#define | ATT_WRITE_REQ_FIXED_SIZE 2 |
Length of Write Request's fixed field: Attribute Handle (2) | |
#define | ATT_WRITE_REQ_HDR_SIZE ( ATT_OPCODE_SIZE + ATT_WRITE_REQ_FIXED_SIZE ) |
Size of Write Request Header. | |
#define | ATT_WRITE_RSP 0x13 |
ATT Write Response. This method is passed as a GATT message. | |
Functions | |
bStatus_t | ATT_ErrorRsp (uint16 connHandle, attErrorRsp_t *pRsp) |
Send Error Response. More... | |
bStatus_t | ATT_ExchangeMTUReq (uint16 connHandle, attExchangeMTUReq_t *pReq) |
Send Exchange MTU Request. More... | |
bStatus_t | ATT_ExchangeMTURsp (uint16 connHandle, attExchangeMTURsp_t *pRsp) |
Send Exchange MTU Response. More... | |
bStatus_t | ATT_ExecuteWriteReq (uint16 connHandle, attExecuteWriteReq_t *pReq) |
Send Execute Write Request. More... | |
bStatus_t | ATT_ExecuteWriteRsp (uint16 connHandle) |
Send Execute Write Response. More... | |
bStatus_t | ATT_FindByTypeValueReq (uint16 connHandle, attFindByTypeValueReq_t *pReq) |
Send Find By Type Value Request. More... | |
bStatus_t | ATT_FindByTypeValueRsp (uint16 connHandle, attFindByTypeValueRsp_t *pRsp) |
Send Find By Type Value Response. More... | |
bStatus_t | ATT_FindInfoReq (uint16 connHandle, attFindInfoReq_t *pReq) |
Send Find Information Request. More... | |
bStatus_t | ATT_FindInfoRsp (uint16 connHandle, attFindInfoRsp_t *pRsp) |
Send Find Information Response. More... | |
uint16 | ATT_GetMTU (uint16 connHandle) |
This function is used to get the MTU size of a connection. More... | |
uint16 | ATT_GetParamValue (void) |
Get a ATT Parameter value. More... | |
bStatus_t | ATT_HandleValueCfm (uint16 connHandle) |
Send Handle Value Confirmation. More... | |
bStatus_t | ATT_HandleValueInd (uint16 connHandle, attHandleValueInd_t *pInd) |
Send Handle Value Indication. More... | |
bStatus_t | ATT_HandleValueNoti (uint16 connHandle, attHandleValueNoti_t *pNoti) |
Send Handle Value Notification. More... | |
bStatus_t | ATT_PrepareWriteReq (uint16 connHandle, attPrepareWriteReq_t *pReq) |
Send Prepare Write Request. More... | |
bStatus_t | ATT_PrepareWriteRsp (uint16 connHandle, attPrepareWriteRsp_t *pRsp) |
Send Prepare Write Response. More... | |
bStatus_t | ATT_ReadBlobReq (uint16 connHandle, attReadBlobReq_t *pReq) |
Send Read Blob Request. More... | |
bStatus_t | ATT_ReadBlobRsp (uint16 connHandle, attReadBlobRsp_t *pRsp) |
Send Read Blob Response. More... | |
bStatus_t | ATT_ReadByGrpTypeReq (uint16 connHandle, attReadByGrpTypeReq_t *pReq) |
Send Read By Group Type Request. More... | |
bStatus_t | ATT_ReadByGrpTypeRsp (uint16 connHandle, attReadByGrpTypeRsp_t *pRsp) |
Send Read By Group Type Respond. More... | |
bStatus_t | ATT_ReadByTypeReq (uint16 connHandle, attReadByTypeReq_t *pReq) |
Send Read By Type Request. More... | |
bStatus_t | ATT_ReadByTypeRsp (uint16 connHandle, attReadByTypeRsp_t *pRsp) |
Send Read By Type Respond. More... | |
bStatus_t | ATT_ReadMultiReq (uint16 connHandle, attReadMultiReq_t *pReq) |
Send Read Multiple Request. More... | |
bStatus_t | ATT_ReadMultiRsp (uint16 connHandle, attReadMultiRsp_t *pRsp) |
Send Read Multiple Response. More... | |
bStatus_t | ATT_ReadReq (uint16 connHandle, attReadReq_t *pReq) |
Send Read Request. More... | |
bStatus_t | ATT_ReadRsp (uint16 connHandle, attReadRsp_t *pRsp) |
Send Read Response. More... | |
void | ATT_RegisterClient (attNotifyTxCB_t pfnNotifyTx) |
Register the client's notify Tx function with the ATT layer. More... | |
void | ATT_RegisterServer (attNotifyTxCB_t pfnNotifyTx) |
Register the server's notify Tx function with the ATT layer. More... | |
void | ATT_SetParamValue (uint16 value) |
Set a ATT Parameter value. Use this function to change the default ATT parameter values. More... | |
uint8 | ATT_UpdateMTU (uint16 connHandle, uint16 MTU) |
This function is used to update the MTU size of a connection. More... | |
bStatus_t | ATT_WriteReq (uint16 connHandle, attWriteReq_t *pReq) |
Send Write Request. More... | |
bStatus_t | ATT_WriteRsp (uint16 connHandle) |
Send Write Response. More... | |